Open Core Interface - MLPI
MLPI-MotionLogicProgrammingInterface(mlpi4COM)  1.26.2
IGroupInfo Interface Reference

Inherits IDispatch.

Collaboration diagram for IGroupInfo:
Collaboration graph

Public Member Functions

HRESULT MovePoint ([in, out] IRobotPoint *point)
 
HRESULT SetPerformanceEnable ([in] enum RobotPerformance type)
 
HRESULT GetPerformanceResult ([out, retval] SAFEARRAY(struct RobotPerformanceResult)*performanceResult)
 
HRESULT GetMechanicData ([in] BOOL updateOnly, [out, retval] SAFEARRAY(struct RobotMechanicData)*mechanicData)
 
HRESULT GetActualPosition ([in] enum RobotCoordinateSystem cs, [out, retval] IRobotPoint **position)
 
HRESULT GetName ([out, retval] BSTR *name)
 
HRESULT GetType ([out, retval] enum RobotTypes *type)
 
HRESULT GetTransform ([in] enum RobotCoordinateSystem coordSys, [out] struct RobotTrafoParameter *trafoParam)
 
HRESULT GetBeltConfiguration ([in] struct AxisRef belt, [out] struct RobotBeltConfigValues *beltValues)
 
HRESULT GetBeltErrorReaction ([in] struct AxisRef belt, [out] struct RobotBeltErrorReactionValues *beltErrorReactParam)
 
HRESULT GetKinematicValues ([out, retval] struct KinematicsValues *kinematicsValues)
 
HRESULT GetKinematicUnits ([out, retval] struct KinematicsUnits *kinematicsUnits)
 
HRESULT GetDiagnosisText ([out, retval] BSTR *diagnosisText)
 
HRESULT TransformPoint ([in] enum RobotCoordinateSystem csOut, [in, out] IRobotPoint *point)
 

Detailed Description

Definition of the IGroupInfo interface used to access information of a group.

Use the IGroupInfo interface to get information about a group.

Definition at line 70 of file IGroupInfo.idl.

Member Function Documentation

HRESULT IGroupInfo::MovePoint ( [in, out] IRobotPoint *  point)

This function returns the current position of the given point. You can use this function to track a point on a belt. If the point is not on a belt, the coordinates of the point will not be changed.

Parameters
[in,out]pointPoint to determine the current position
Returns
Return value indicating success (>=0) or error (<0).
Example C#:
//return current position of myPoint on a belt
connection.Robot.Groups[1].Information.MovePoint(myPoint);
Note:
This method maps to the mlpiCore function mlpiRobotMovePoint, where you can find further documentation.
HRESULT IGroupInfo::SetPerformanceEnable ( [in] enum RobotPerformance  type)

This function sets the IRobot::RobotPerformance of the Group. You can enable the performance measurement using RobotPerformance.ROBOT_PERFORMANCE_ENABLE. During the enable performance measurement, old values are cleared. To disable performance measurement, use RobotPerformance.ROBOT_PERFORMANCE_DISABLE.

Parameters
[in]typeIRobot::RobotPerformance of the group.
Returns
Return value indicating success (>=0) or error (<0).
Example C#:
//enable performance measurement
connection.Robot.Groups[1].Information.SetPerformanceEnable(RobotPerformance.ROBOT_PERFORMANCE_ENABLE);
//disable performance measurement
connection.Robot.Groups[1].Information.SetPerformanceEnable(RobotPerformance.ROBOT_PERFORMANCE_DISABLE);
Note:
This method maps to the mlpiCore function mlpiRobotSetPerformanceEnable, where you can find further documentation.
HRESULT IGroupInfo::GetPerformanceResult ( [out, retval] SAFEARRAY(struct RobotPerformanceResult)*  performanceResult)

This function returns an array of IRobot::RobotPerformanceResult of the Group.

Parameters
[out]performanceResultIRobot::RobotPerformanceResult of the group.
Returns
Return value indicating success (>=0) or error (<0).
Example C#:
RobotPerformanceResult[] groupPerformance = (RobotPerformanceResult[])connection.Robot.Groups[1].Information.GetPerformanceResult();
foreach (RobotPerformanceResult item in groupPerformance)
{
// do something with the values
}
Note:
This method maps to the mlpiCore function mlpiRobotGetPerfomanceResult, where you can find further documentation.
HRESULT IGroupInfo::GetMechanicData ( [in] BOOL  updateOnly,
[out, retval] SAFEARRAY(struct RobotMechanicData)*  mechanicData 
)

This function returns an array of IRobot::RobotMechanicData of the Group.

Parameters
[in]updateOnlyUpdates of mechanic data only
[out]mechanicDataIRobot::RobotMechanicData of the group.
Returns
Return value indicating success (>=0) or error (<0).
Example C#:
RobotMechanicData[] mechanicData = (RobotMechanicData[])connection.Robot.Groups[1].Information.GetMechanicData(false);
foreach (RobotMechanicData item in mechanicData)
{
// do something with the values
}
Note:
This method maps to the mlpiCore function mlpiRobotGetMechanicData, where you can find further documentation.
HRESULT IGroupInfo::GetActualPosition ( [in] enum RobotCoordinateSystem  cs,
[out, retval] IRobotPoint **  position 
)

This function returns the current position of the group in the given coordinate system.

Parameters
[in]csIRobot::RobotCoordinateSystem to read the position from the group
[out]positionCurrent position of the group.
Returns
Return value indicating success (>=0) or error (<0).
Example C#:
//get current position of the group in MCS and write it to actPos
RobotPoint actPos = connection.Robot.Groups[1].Information.GetActualPosition(RobotCoordinateSystem.ROBOT_CS_MCS);
Example VBA:
Note:
This method maps to the mlpiCore function mlpiRobotReadPos, where you can find further documentation.
HRESULT IGroupInfo::GetName ( [out, retval] BSTR *  name)

This function returns the name of the Group.

Parameters
[out]nameName of the group.
Returns
Return value indicating success (>=0) or error (<0).
Example C#:
connection.Robot.Groups["Delta"].Information.GetName(); // returns "Delta"
Note:
This method maps to the mlpiCore function mlpiParameterReadDataString and reads parameter K-0-0002.
HRESULT IGroupInfo::GetType ( [out, retval] enum RobotTypes *  type)

This function returns the IRobot::RobotTypes of the Group.

Parameters
[in]typeIRobot::RobotTypes of the group.
Returns
Return value indicating success (>=0) or error (<0).
Example C#:
//return the RobotTypes of the given group
connection.Robot.Groups[1].Information.GetType();
Note:
This method maps to the mlpiCore function mlpiParameterReadDataUlong and reads parameter K-0-0019.
HRESULT IGroupInfo::GetTransform ( [in] enum RobotCoordinateSystem  coordSys,
[out] struct RobotTrafoParameter *  trafoParam 
)

This function returns the transformation values of a selected coordinate system.

Parameters
[in]coordSysIRobot::RobotCoordinateSystem struct defines the type of performance measurement.
[out]trafoParamSaves the values in a IRobot::RobotTrafoParameter struct.
Returns
Return value indicating success (>=0) or error (<0).
Example C#:
//save the trafo parameter to "trafoparam"
RobotTrafoParameter trafoparam;
connection.Robot.Groups[1].Information.GetTransform(ROBOT_CS_BCS, trafoparam)
Note:
This method maps to the mlpiCore function mlpiRobotGetTransform, where you can find further documentation.
HRESULT IGroupInfo::GetBeltConfiguration ( [in] struct AxisRef  belt,
[out] struct RobotBeltConfigValues *  beltValues 
)

This function returns the values of a belt configuration.

Parameters
[in]beltSaves the values in a IRobot::RobotBeltConfigValues
[out]beltValuesIMotion::AxisRef defines the axis through the definition of control and axis number
Returns
Return value indicating success (>=0) or error (<0).
Example C#:
//save the belt configuration to beltValues.
AxisRef belt;
RobotBeltConfigValues *beltValues;
connection.Robot.Groups[1].Information.GetBeltConfiguration(belt, beltValues);
Note:
This method maps to the mlpiCore function mlpiRobotGetBeltConfiguration, where you can find further documentation.
HRESULT IGroupInfo::GetBeltErrorReaction ( [in] struct AxisRef  belt,
[out] struct RobotBeltErrorReactionValues *  beltErrorReactParam 
)

This function returns the values of a configured belt error reaction.

Parameters
[out]beltErrorReactParamSaves the values in a IRobot::RobotBeltErrorReactionValues
[in]beltIMotion::AxisRef defines the axis through the definition of control and axis number
Returns
Return value indicating success (>=0) or error (<0).
Example C#:
//save the configured belt error reaction to beltErrorReactParam.
AxisRef belt;
RobotBeltErrorReactionValues *beltErrorReactParam;
connection.Robot.Groups[1].Information.GetBeltErrorReaction(belt, beltValues);
Note:
This method maps to the mlpiCore function mlpiRobotGetBeltErrorReaction, where you can find further documentation.
HRESULT IGroupInfo::GetKinematicValues ( [out, retval] struct KinematicsValues *  kinematicsValues)

This function fills an array of KinematicValues.

Parameters
[in,out]kinematicsValuesReturns a struct with the current operation information about the kinematic.
Returns
Return value indicating success (>=0) or error (<0).
Note
Elements of the struct that can not be read will be set to 0.
Example C#:
//save the configured kinematic values to kinematicsValues.
KinematicsValues *kinematicsValues;
connection.Robot.Groups[1].Information.GetKinematicValues(kinematicsValues);
Note:
This method maps to the mlpiCore function mlpiRobotGetKinematicsValues, where you can find further documentation.
HRESULT IGroupInfo::GetKinematicUnits ( [out, retval] struct KinematicsUnits *  kinematicsUnits)

This function fills an array of KinematicUnits with information about the units of the kinematic.

Parameters
[out]kinematicsUnitsReturns a struct with the current unit information about kinematics.
Returns
Return value indicating success (>=0) or error (<0).
Example C#:
//save the configured kinematic units to kinematicsUnits.
KinematicsUnits *kinematicsUnits;
connection.Robot.Groups[1].Information.GetKinematicUnits(kinematicsUnits);
Note:
This method maps to the mlpiCore function mlpiRobotGetKinematicsUnits, where you can find further documentation.
HRESULT IGroupInfo::GetDiagnosisText ( [out, retval] BSTR *  diagnosisText)

This function reads the current diagnosis text of the kinematic.

Parameters
[out]diagnosisTextReturns the current diagnosis text as string.
Returns
Return value indicating success (>=0) or error (<0).
Example C#:
//save the DiagnosisText to diagnosisText.
BSTR *diagnosisText;
connection.Robot.Groups[1].Information.GetDiagnosisText(diagnosisText);
Note:
This method maps to the mlpiCore function mlpiRobotGetDiagnosisText, where you can find further documentation.
HRESULT IGroupInfo::TransformPoint ( [in] enum RobotCoordinateSystem  csOut,
[in, out] IRobotPoint *  point 
)

This function transforms the current position of the given point into the given coordinate system. Transforms point from csIn to csOut.

Parameters
[in]csOutIRobot::RobotCoordinateSystem to transform the point into.
[in,out]pointPoint which gets transformed.
Returns
Return value indicating success (>=0) or error (<0).
Example C#:
//transform point "mypoint" into the coordinate system "myCoordSysOut".
connection.Robot.Groups[1].Information.TransformPoint(myCoordSysOut, myPoint);
Note:
This method maps to the mlpiCore function mlpiRobotTransformPoint, where you can find further documentation.

The documentation for this interface was generated from the following file: