Open Core Interface - MLPI
MLPI-MotionLogicProgrammingInterface(mlpi4COM)  1.26.2
IMlpiConnection Interface Reference

Inherits IDispatch.

Collaboration diagram for IMlpiConnection:
Collaboration graph

Public Types

typedef struct IMlpiConnection::Version Version
 
typedef struct IMlpiConnection::ConnectionInfo ConnectionInfo
 

Public Member Functions

HRESULT Connect ([in] BSTR address)
 
HRESULT Disconnect (void)
 
HRESULT TestConnection ([in] LONG payload, [in] LONG numMeasurements, [out, retval] struct ConnectionInfo *connectInfo)
 
HRESULT Delay ([in] LONG delayMilliseconds)
 
HRESULT GetClientCoreVersion ([out, retval] struct Version *versionInfo)
 
HRESULT GetServerCoreVersion ([out, retval] struct Version *versionInfo)
 

Properties

VARIANT_BOOL IsConnected [get]
 
ISystem System [get]
 
IMotion Motion [get]
 
ILogic Logic [get]
 
IParameter Parameter [get]
 
IWatchdog Watchdog [get]
 
IIo Io [get]
 
ITrace Trace [get]
 
IContainer Container [get]
 
IRobot Robot [get]
 

Detailed Description

Definition of the IMlpiConnection interface which is the root object of a connection to a MLPI Device.

The IMlpiConnection class is the root object of the MLPI object hierarchy. It represents a single connection to a device that supports the MLPI. The MlpiConnection class contains properties and subobjects which contain further MLPI methods.

Definition at line 76 of file IMlpiConnection.idl.

Member Typedef Documentation

IMlpiConnection::Version

Describes the API version information. The build number counts continuously within a major release, all other elements count at the beginning, if a higher element will be incremented.

Elements of struct Version

Type Element Description
LONG major Major release, changes of interfaces, behavior or significant changes of code may occur.
LONG minor Minor release, new features or a significant set of bug fixes may occur.
LONG bugfix Bug fixes of existing features.
LONG patch Patch of an existing release.
LONG build Build number.
IMlpiConnection::ConnectionInfo

This structure is used by the function TestConnection to return the results of the timing measurements.

Elements of struct ConnectionInfo

Type Element Description
DOUBLE minimum Minimum time duration of all measurements.
DOUBLE maximum Maximum time duration of all measurements.
DOUBLE average Average time duration of all measurements.
DOUBLE variance Variance of all measurements.
DOUBLE standardDeviation Standard deviation of all measurements.

Member Enumeration Documentation

This enumeration defines the basic types of as used by the MLPI.

Enumerator
TYPE_INVALID 

invalid or not supported type

TYPE_CHAR 

1 byte signed integer

TYPE_UCHAR 

1 byte unsigned integer

TYPE_SHORT 

2 byte signed integer

TYPE_USHORT 

2 byte unsigned integer

TYPE_LONG 

4 byte signed integer

TYPE_ULONG 

4 byte unsigned integer

TYPE_LLONG 

8 byte signed integer

TYPE_ULLONG 

8 byte unsigned integer

TYPE_FLOAT 

4 byte floating point

TYPE_DOUBLE 

4 byte floating point

TYPE_CHAR_ARRAY 

1 byte signed integer array

TYPE_UCHAR_ARRAY 

1 byte unsigned integer array

TYPE_SHORT_ARRAY 

2 byte signed integer array

TYPE_USHORT_ARRAY 

2 byte unsigned integer array

TYPE_LONG_ARRAY 

4 byte signed integer array

TYPE_ULONG_ARRAY 

4 byte unsigned integer array

TYPE_LLONG_ARRAY 

8 byte signed integer array

TYPE_ULLONG_ARRAY 

8 byte unsigned integer array

TYPE_FLOAT_ARRAY 

4 byte floating point array

TYPE_DOUBLE_ARRAY 

4 byte floating point array

TYPE_BOOL8 

1 byte boolean

TYPE_BOOL8_ARRAY 

1 byte boolean array

TYPE_CHAR_UTF8 

string with 1 byte per character

TYPE_CHAR_UTF16 

string with 2 bytes per character

TYPE_CHAR_UTF8_ARRAY 

string array with 1 byte per character

TYPE_CHAR_UTF16_ARRAY 

string array with 2 bytes per character

Definition at line 81 of file IMlpiConnection.idl.

Member Function Documentation

HRESULT IMlpiConnection::Connect ( [in] BSTR  address)

This function connects the user application with a MLPI Device. The first argument is used to specify the target device to which you want to connect. This can either be a control running on the same physical device as your application or a control that is connected via a network, for example, by TCP/IP. In this case, you have to give the IP or host name of the target.

It is also possible to set additional options in the connect string as an argument list.

  • address=value IP or URL path of connection.
  • timeout_connect=value Timeout used for connecting in milliseconds.
  • timeout_send=value Timeout used for sending data to target in milliseconds.
  • timeout_receive=value Timeout used for receiving data from target in milliseconds.
  • auto_reconnect=value If set to 1 or 'true', then the MLPI will try to reconnect with each new call of any MLPI function after connection was lost. For connecting, the same timeout settings are used as given for the first connect.
  • user=value Login name of user. See Permission and user management for more information about user and permission system.
  • password=value Password of user.

A timeout value of 0 means that the timeout value should be chosen automatically by the operating system.

Parameters
[in]addressAddress identifying the control. Use an IP address to connect over Ethernet to another control.
Returns
Return value indicating success (>=0) or error (<0).
Example C#:
try
{
MlpiConnection connection = new MlpiConnection();
// connect to control with ip address 192.168.0.17
connection.Connect("192.168.0.17");
// read current diagnosis text of the target device
Console.WriteLine("Diagnosis Text: " + connection.System.GetDisplayedDiagnosis().text);
// disconnect from control
connection.Disconnect();
}
catch (System.Exception ex)
{
Console.WriteLine("Error: " + ex.Message);
}
Example VBA:
Dim connection As MlpiConnection
Set connection = New MlpiConnection
' connect to device with ip address
connection.Connect "192.168.0.17"
' retrieve and show the name of the device
MsgBox connection.System.GetName
' disconnect from control
connection.Disconnect
Note:
This method maps to the mlpiCore function mlpiApiConnect, where you can find further documentation.
HRESULT IMlpiConnection::Disconnect ( void  )

This function disconnects the user application from the MlpiConnection. After closing the MLPI connection, no more method calls to the MLPI device can be made.

Returns
Return value indicating success (>=0) or error (<0).
Note:
This method maps to the mlpiCore function mlpiApiDisconnect, where you can find further documentation.
HRESULT IMlpiConnection::TestConnection ( [in] LONG  payload,
[in] LONG  numMeasurements,
[out, retval] struct ConnectionInfo *  connectInfo 
)

This function performs a benchmark on the MLPI communication mechanism. Use it to measure the duration of a MLPI function call with the given payload in bytes. The resulting timing values are the durations which are necessary to marshal the payload, send the payload to the MLPI server, unmarshal it on the MLPI server, perform the remote procedure call, marshal the results, send them back to the MLPI client unmarshal them again and return them to the client thread program. These are the basic costs needed for nearly every MLPI call.

Parameters
[in]payloadPayload in number of bytes that is used for the MLPI communication to be measured.
[in]numMeasurementsNumber of measurements to do for calculating the average resulting timing values.
[out]connectInfoPointer to structure which receives the calculated timing values.
Returns
Return value indicating success (>=0) or error (<0).
Example C#:
try
{
// run 50 iterations with 100 byte payload to measure the connection speed
ConnectionInfo info = connection.TestConnection(100, 50);
// print info to console
Console.WriteLine("Average: " + info.average * 0.001 + " ms");
Console.WriteLine("Minimum: " + info.minimum * 0.001 + " ms");
Console.WriteLine("Maximum: " + info.maximum * 0.001 + " ms");
Console.WriteLine("Variance: " + info.variance * 0.001 * 0.001 + " ms^2");
Console.WriteLine("Standard Deviation: " + info.standardDeviation * 0.001 + " ms");
}
catch (System.Exception ex)
{
Console.WriteLine("Error: " + ex.Message);
}
Note:
This method maps to the mlpiCore function mlpiApiTestConnection, where you can find further documentation.
HRESULT IMlpiConnection::Delay ( [in] LONG  delayMilliseconds)

This function does a simple delay on the server side. All this function performs is a blocking delay on the server side in the given amount of milliseconds. Use it during development or debugging of your application to simulate high traffic on your network. This way, you can test the behavior of your client application when MLPI communication slows down. The delay has no impact on the performance of the control.

Parameters
[in]delayMillisecondsDelay in milliseconds to block.
Returns
Return value indicating success (>=0) or error (<0).
Example C#:
try
{
// block on server side for 1 second
connection.Delay(1000);
}
catch (System.Exception ex)
{
Console.WriteLine("Error: " + ex.Message);
}
Note:
This method maps to the mlpiCore function mlpiApiDelay, where you can find further documentation.
HRESULT IMlpiConnection::GetClientCoreVersion ( [out, retval] struct Version *  versionInfo)

This function returns the version info of the MLPI client library. No connection to the server is needed to execute this method.

Parameters
[out]versionInfoPointer to struct receiving the version info.
Returns
Return value indicating success (>=0) or error (<0).
Example C#:
try
{
// read the version info. Client Version can be called without established connection
commlpiLib.Version version = connection.GetClientCoreVersion();
// print to console
Console.WriteLine("Major: " + version.major);
Console.WriteLine("Minor: " + version.minor);
Console.WriteLine("Bugfix: " + version.bugfix);
Console.WriteLine("Patch: " + version.patch);
Console.WriteLine("Build: " + version.build);
}
catch (System.Exception ex)
{
Console.WriteLine("Error: " + ex.Message);
}
Note:
This method maps to the mlpiCore function mlpiApiGetClientCoreVersion, where you can find further documentation.
HRESULT IMlpiConnection::GetServerCoreVersion ( [out, retval] struct Version *  versionInfo)

This function returns the version info of the MLPI server library.

Parameters
[out]versionInfoPointer to struct receiving the version info.
Returns
Return value indicating success (>=0) or error (<0).
Example C#:
try
{
// read the version info.
commlpiLib.Version version = connection.GetServerCoreVersion();
// print to console
Console.WriteLine("Major: " + version.major);
Console.WriteLine("Minor: " + version.minor);
Console.WriteLine("Bugfix: " + version.bugfix);
Console.WriteLine("Patch: " + version.patch);
Console.WriteLine("Build: " + version.build);
}
catch (System.Exception ex)
{
Console.WriteLine("Error: " + ex.Message);
}
Note:
This method maps to the mlpiCore function mlpiApiGetServerCoreVersion, where you can find further documentation.

Property Documentation

VARIANT_BOOL IMlpiConnection::IsConnected
getproperty

This function returns the current state of the MLPI connection. If FALSE is returned, then the connection is either not yet established or closed due to a communication error or because Disconnect has been called. In all cases, a reconnect using Connect has to be made to make new MLPI method calls. If connection has been lost for an unknown reason, try increasing the connection timeout using Connect.

Parameters
[out]pConnectedReturns TRUE if a connection has been established and FALSE if disconnected.
Returns
Return value indicating success (>=0) or error (<0).
Example C#:
MlpiConnection connection = new MlpiConnection();
// show connection status when not connected yet --> False
Console.WriteLine(connection.IsConnected.ToString());
// show connection status when connected --> True
connection.Connect ("192.168.0.17");
Console.WriteLine(connection.IsConnected.ToString());
// show connection status when disconnected again --> False
connection.Disconnect();
Console.WriteLine(connection.IsConnected.ToString());
Example VBA:
Dim connection As MlpiConnection
Set connection = New MlpiConnection
' show connection status when not connected yet --> False
MsgBox connection.IsConnected
' show connection status when connected --> True
connection.Connect "192.168.0.17"
MsgBox connection.IsConnected
' show connection status when disconnected again --> False
connection.Disconnect
MsgBox connection.IsConnected
Note:
This method maps to the mlpiCore function mlpiApiIsConnected, where you can find further documentation.
ISystem IMlpiConnection::System
getproperty

Property to access the System methods of the MLPI device by providing access to the ISystem interface.

Parameters
[out]pValReturns the System object.
Returns
Return value indicating success (>=0) or error (<0).
IMotion IMlpiConnection::Motion
getproperty

Property to access the Motion methods of the MLPI device by providing access to the IMotion interface.

Parameters
[out]pValReturns the Motion object.
Returns
Return value indicating success (>=0) or error (<0).
ILogic IMlpiConnection::Logic
getproperty

Property to access the Logic methods of the MLPI device by providing access to the ILogic interface.

Parameters
[out]pValReturns the Logic object.
Returns
Return value indicating success (>=0) or error (<0).
IParameter IMlpiConnection::Parameter
getproperty

Property to access the Parameter methods of the MLPI device by providing access to the IParameter interface.

Parameters
[out]pValReturns the IParameter object.
Returns
Return value indicating success (>=0) or error (<0).
IWatchdog IMlpiConnection::Watchdog
getproperty

Property to access the Watchdog methods of the MLPI device by providing access to the IWatchdog interface.

Parameters
[out]pValReturns the Watchdog object.
Returns
Return value indicating success (>=0) or error (<0).
IIo IMlpiConnection::Io
getproperty

Property to access the Input/Output methods of the MLPI device by providing access to the IIo interface.

Parameters
[out]pValReturns the IO object.
Returns
Return value indicating success (>=0) or error (<0).
ITrace IMlpiConnection::Trace
getproperty

Property to access the Trace methods of the MLPI device by providing access to the ITrace interface.

Parameters
[out]pValReturns the Trace object.
Returns
Return value indicating success (>=0) or error (<0).
IContainer IMlpiConnection::Container
getproperty

Property to access the Container methods of the MLPI device by providing access to the IContainer interface.

Parameters
[out]pValReturns the Trace object.
Returns
Return value indicating success (>=0) or error (<0).
IRobot IMlpiConnection::Robot
getproperty

Property to access the Robot methods of the MLPI device by providing access to the IRobot interface.

Parameters
[out]pValReturns the Trace object.
Returns
Return value indicating success (>=0) or error (<0).

The documentation for this interface was generated from the following file: