Open Core Interface - MLPI
MLPI-MotionLogicProgrammingInterface(mlpiCore)  1.26.2
MlpiAxisStateDecoder Struct Reference
Collaboration diagram for MlpiAxisStateDecoder:
Collaboration graph

Public Member Functions

 MLPI_MOTION_BIT_ACCESS (CamTab_0, 0)
 
 MLPI_MOTION_BIT_ACCESS (CamTab_1, 1)
 
 MLPI_MOTION_BIT_ACCESS (CamTab_2, 2)
 
 MLPI_MOTION_BIT_ACCESS (CamSwitching, 3)
 
 MLPI_MOTION_BIT_ACCESS (InVelocity, 4)
 
 MLPI_MOTION_BIT_ACCESS (Standstill, 5)
 
 MLPI_MOTION_BIT_ACCESS (InPosition, 6)
 
 MLPI_MOTION_BIT_ACCESS (InSynchron, 7)
 
 MLPI_MOTION_BIT_ACCESS (Warning, 8)
 
 MLPI_MOTION_BIT_ACCESS (Error, 9)
 
 MLPI_MOTION_BIT_ACCESS (Homed, 10)
 
 MLPI_MOTION_BIT_ACCESS (InTorque, 11)
 
 MLPI_MOTION_BIT_ACCESS (OperationMode, 12)
 
 MLPI_MOTION_BIT_ACCESS (Inbb, 13)
 
 MLPI_MOTION_BIT_ACCESS (InAb, 14)
 
 MLPI_MOTION_BIT_ACCESS (Power, 15)
 
 MLPI_MOTION_BIT_ACCESS (CmdActive, 16)
 
 MLPI_MOTION_BIT_ACCESS (ErrInProgress, 17)
 
 MLPI_MOTION_BIT_ACCESS (CyclicPosChannelActive, 18)
 
 MLPI_MOTION_BIT_ACCESS (InMasterPhaseOffset, 19)
 
 MLPI_MOTION_BIT_ACCESS (CyclicTrqChannelActive, 20)
 
 MLPI_MOTION_BIT_ACCESS (CyclicVelChannelActive, 21)
 
 MLPI_MOTION_BIT_ACCESS (CyclicAnaChannelActive, 22)
 
 MLPI_MOTION_BIT_ACCESS (NRTActive, 23)
 
 MLPI_MOTION_BIT_ACCESS (Interrupted, 24)
 
 MLPI_MOTION_BIT_ACCESS (Modulo, 28)
 
 MLPI_MOTION_BIT_ACCESS (Rotatory, 29)
 
 MLPI_MOTION_BIT_ACCESS (Valid, 30)
 
 MLPI_MOTION_BIT_ACCESS (Decoupled, 31)
 

Detailed Description

The following struct helps to decode the axis state as given by mlpiMotionGetAxisState or mlpiMotionGetAxisValues.

Example:
See mlpiMotionGetState

Definition at line 207 of file mlpiMotionHelper.h.

Member Function Documentation

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( CamTab_0  ,
0   
)

Bit0 of active CAM table of CamIn command.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( CamTab_1  ,
1   
)

Bit1 of active CAM table of CamIn command.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( CamTab_2  ,
2   
)

Bit2 of active CAM table of CamIn command.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( CamSwitching  ,
3   
)

Returns the active CAM table of CamIn command.

Cam is waiting for switching position.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( InVelocity  ,
4   
)

Axis is in velocity.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( Standstill  ,
5   
)

Axis is in standstill.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( InPosition  ,
6   
)

Axis is in position.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( InSynchron  ,
7   
)

Axis is synchronous to another axis.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( Warning  ,
8   
)

Axis has warning.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( Error  ,
9   
)

Axis has an error.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( Homed  ,
10   
)

Axis is homed.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( InTorque  ,
11   
)

Axis is in torque.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( OperationMode  ,
12   
)

Axis is in P4.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( Inbb  ,
13   
)

Axis is ready for power.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( InAb  ,
14   
)

Axis is ready for operation.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( Power  ,
15   
)

Axis has power.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( CmdActive  ,
16   
)

Axis has a active sercos command.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( ErrInProgress  ,
17   
)

Error reaction of axis is in progress.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( CyclicPosChannelActive  ,
18   
)

Cyclic position channel is active.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( InMasterPhaseOffset  ,
19   
)

Axis has reached the master phase offset.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( CyclicTrqChannelActive  ,
20   
)

Cyclic torque channel is active.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( CyclicVelChannelActive  ,
21   
)

Cyclic velocity channel is active.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( CyclicAnaChannelActive  ,
22   
)

Cyclic analog channel is active.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( NRTActive  ,
23   
)

NRT channel for axis is connected.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( Interrupted  ,
24   
)

Axis did not follow control.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( Modulo  ,
28   
)

Axis is in Modulo format.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( Rotatory  ,
29   
)

Axis is rotatory.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( Valid  ,
30   
)

Actual data of axis is valid.

MlpiAxisStateDecoder::MLPI_MOTION_BIT_ACCESS ( Decoupled  ,
31   
)

Axis is decoupled from commanded position of control.


The documentation for this struct was generated from the following file: