Inherits IDispatch.
|
| HRESULT | AddAllAxisToGroup (void) |
| |
| HRESULT | RemAllAxisFromGroup (void) |
| |
| HRESULT | SetCartesianTransform ([in] enum RobotCoordinateSystem coordSys, [in] DOUBLE posX, [in] DOUBLE posY, [in] DOUBLE posZ, [in] DOUBLE rotA, [in] DOUBLE rotB, [in] DOUBLE rotC) |
| |
| HRESULT | SetCylindricTransform ([in] enum RobotCoordinateSystem coordSys, [in] DOUBLE posX, [in] DOUBLE posY, [in] DOUBLE posZ, [in] DOUBLE rotA, [in] DOUBLE rotB, [in] DOUBLE rotC) |
| |
| HRESULT | SetBeltConfiguration ([in] AxisRef *beltAxis, [in] DOUBLE posX, [in] DOUBLE posY, [in] DOUBLE posZ, [in] DOUBLE rotA, [in] DOUBLE rotB, [in] DOUBLE rotC, [in] DOUBLE beginLength, [in] DOUBLE totalLength) |
| |
| HRESULT | SetRotaryTableConfiguration ([in] AxisRef *beltAxis, [in] DOUBLE posX, [in] DOUBLE posY, [in] DOUBLE posZ, [in] DOUBLE rotA, [in] DOUBLE rotB, [in] DOUBLE rotC, [in] DOUBLE beginLength, [in] DOUBLE totalLength) |
| |
| HRESULT | SetBeltErrorReaction ([in] AxisRef *beltAxis, [in] enum RobotSyncErrorReactionMode errorType, [in] DOUBLE time, [in] DOUBLE deceleration, [in] DOUBLE jerk) |
| |
| HRESULT | SetName ([in] BSTR name) |
| |
| HRESULT | SetAxisConfiguration ([in] SAFEARRAY(struct RobotAxisConfiguration) axisConfig) |
| |
| HRESULT | SetKinematicType ([in]LONG type) |
| |
| HRESULT | Reset () |
| |
| HRESULT | SetSafeZone ([in]SHORT zoneNumber, [in]enum RobotSafeZoneType zoneType, [in]DOUBLE maxPosX, [in]DOUBLE maxPosY, [in]DOUBLE maxPosZ, [in]DOUBLE minPosX, [in]DOUBLE minPosY, [in]DOUBLE minPosZ) |
| |
Definition of the IGroupConfig interface used to access motion commands to move an group.
Use the IGroupConfig interface to physically move or control a group by using various motion commands.
Definition at line 70 of file IGroupConfig.idl.
| HRESULT IGroupConfig::AddAllAxisToGroup |
( |
void |
| ) |
|
This function adds all configured axis to the group.
- Returns
- Return value indicating success (>=0) or error (<0).
- Example C#:
connection.Robot.Robots[1].Configuration.AddAllAxisToGroup;
- Note:
- This method maps to the mlpiCore function
mlpiRobotAddAllAxisToGroup, where you can find further documentation.
| HRESULT IGroupConfig::RemAllAxisFromGroup |
( |
void |
| ) |
|
This function removes all configured axes from the group.
- Returns
- Return value indicating success (>=0) or error (<0).
- Example C#:
connection.Robot.Robots[1].Configuration.RemAllAxisFromGroup;
- Note:
- This method maps to the mlpiCore function
mlpiRobotRemAllAxisFromGroup, where you can find further documentation.
| HRESULT IGroupConfig::SetCartesianTransform |
( |
[in] enum RobotCoordinateSystem |
coordSys, |
|
|
[in] DOUBLE |
posX, |
|
|
[in] DOUBLE |
posY, |
|
|
[in] DOUBLE |
posZ, |
|
|
[in] DOUBLE |
rotA, |
|
|
[in] DOUBLE |
rotB, |
|
|
[in] DOUBLE |
rotC |
|
) |
| |
This function sets a Cartesian transformation for PCS to WCS within the kinematic.
- Parameters
-
| [in] | coordSys | specifies the coordinate system, where the transformation will be set |
| [in] | posX | deferral in X |
| [in] | posY | deferral in Y |
| [in] | posZ | deferral in Z |
| [in] | rotA | twisting around X |
| [in] | rotB | twisting around Y |
| [in] | rotC | twisting around Z |
- Returns
- Return value indicating success (>=0) or error (<0).
- Example C#:
myGroup.Configuration.SetCartesianTransform(ROBOT_CS_PCS1, 10, 10, 10, 0, 0, 0);
- Example VBA:
- Note:
- This method maps to the mlpiCore function
mlpiRobotSetCartesianTransform, where you can find further documentation.
| HRESULT IGroupConfig::SetCylindricTransform |
( |
[in] enum RobotCoordinateSystem |
coordSys, |
|
|
[in] DOUBLE |
posX, |
|
|
[in] DOUBLE |
posY, |
|
|
[in] DOUBLE |
posZ, |
|
|
[in] DOUBLE |
rotA, |
|
|
[in] DOUBLE |
rotB, |
|
|
[in] DOUBLE |
rotC |
|
) |
| |
This function sets a cylindric transformation for PCS to WCS within the kinematic.
- Parameters
-
| [in] | coordSys | specifies the coordinate system, where the transformation will be set |
| [in] | posX | deferral in X |
| [in] | posY | deferral in Y |
| [in] | posZ | deferral in Z |
| [in] | rotA | twisting around X |
| [in] | rotB | twisting around Y |
| [in] | rotC | twisting around Z |
- Returns
- Return value indicating success (>=0) or error (<0).
- Example C#:
myGroup.Configuration.SetCylindricTransform(ROBOT_CS_PCS1, 10, 10, 10, 0, 0, 0);
- Example VBA:
- Note:
- This method maps to the mlpiCore function
mlpiRobotSetCylindricTransform, where you can find further documentation.
| HRESULT IGroupConfig::SetBeltConfiguration |
( |
[in] AxisRef * |
beltAxis, |
|
|
[in] DOUBLE |
posX, |
|
|
[in] DOUBLE |
posY, |
|
|
[in] DOUBLE |
posZ, |
|
|
[in] DOUBLE |
rotA, |
|
|
[in] DOUBLE |
rotB, |
|
|
[in] DOUBLE |
rotC, |
|
|
[in] DOUBLE |
beginLength, |
|
|
[in] DOUBLE |
totalLength |
|
) |
| |
This function sets a Cartesian transformation for PCS to WCS within the kinematic and configures a belt for belt synchronous moves.
- Parameters
-
| [in] | beltAxis | specifies the belt, which should be configured |
| [in] | posX | deferral in X |
| [in] | posY | deferral in Y |
| [in] | posZ | deferral in Z |
| [in] | rotA | twisting around X |
| [in] | rotB | twisting around Y |
| [in] | rotC | twisting around Z |
| [in] | beginLength | the synchronization to belt must be started until beginLength exceeded |
| [in] | totalLength | total length of belt synchronous working area |
- Returns
- Return value indicating success (>=0) or error (<0).
- Example C#:
myGroup.Configuration.SetBeltConfiguration(beltAxis1, 10, 10, 10, 0, 0, 0, 1000, 2000);
- Example VBA:
- Note:
- This method maps to the mlpiCore function
mlpiRobotSetBeltConfiguration, where you can find further documentation.
| HRESULT IGroupConfig::SetRotaryTableConfiguration |
( |
[in] AxisRef * |
beltAxis, |
|
|
[in] DOUBLE |
posX, |
|
|
[in] DOUBLE |
posY, |
|
|
[in] DOUBLE |
posZ, |
|
|
[in] DOUBLE |
rotA, |
|
|
[in] DOUBLE |
rotB, |
|
|
[in] DOUBLE |
rotC, |
|
|
[in] DOUBLE |
beginLength, |
|
|
[in] DOUBLE |
totalLength |
|
) |
| |
This function sets a cylindric transformation for PCS to WCS within the kinematic and configures a belt for belt synchronous moves on a rotary table.
- Parameters
-
| [in] | beltAxis | specifies the belt, which should be configured |
| [in] | posX | deferral in X |
| [in] | posY | deferral in Y |
| [in] | posZ | deferral in Z |
| [in] | rotA | twisting around X |
| [in] | rotB | twisting around Y |
| [in] | rotC | twisting around Z |
| [in] | beginLength | the synchronization to belt must be started until beginLength exceeded. In this case, the angle around Z |
| [in] | totalLength | total length of belt synchronous working area. In this case, the angle around Z |
- Returns
- Return value indicating success (>=0) or error (<0).
- Example C#:
myGroup.Configuration.SetRotaryTableConfiguration(beltAxis1, 10, 10, 10, 0, 0, 0, 100, 270);
- Example VBA:
- Note:
- This method maps to the mlpiCore function
mlpiRobotSetRotaryTableConfiguration, where you can find further documentation.
| HRESULT IGroupConfig::SetBeltErrorReaction |
( |
[in] AxisRef * |
beltAxis, |
|
|
[in] enum RobotSyncErrorReactionMode |
errorType, |
|
|
[in] DOUBLE |
time, |
|
|
[in] DOUBLE |
deceleration, |
|
|
[in] DOUBLE |
jerk |
|
) |
| |
This function configures a error reaction for a kinematic and belt synchronous moves.
- Parameters
-
| [in] | beltAxis | specifies the belt, which should be configured |
| [in] | errorType | specifies the type of error reaction |
| [in] | time | time in s for desynchronization in case of an error |
| [in] | deceleration | deceleration desynchronization in case of an error |
| [in] | jerk | jerk desynchronization in case of an error |
- Returns
- Return value indicating success (>=0) or error (<0).
- Example C#:
myGroup.Configuration.SetBeltErrorReaction(beltAxis1, ROBOT_BELT_ERROR_DESYNC_OVER_TIME, 1, 0, 0);
- Example VBA:
- Note:
- This method maps to the mlpiCore function
mlpiRobotSetBeltErrorReaction, where you can find further documentation.
| HRESULT IGroupConfig::SetName |
( |
[in] BSTR |
name | ) |
|
This function sets the name of the Group.
- Parameters
-
| [in] | name | New name of the group. |
- Returns
- Return value indicating success (>=0) or error (<0).
- Example C#:
connection.Robot.Groups[1].Configuration.SetName("Delta1);
connection.Robot.Groups[1].Information.GetName(); // returns "Delta1"
- Note:
- This method maps to the mlpiCore function
mlpiParameterWriteDataString and writes parameter K-0-0002.
| HRESULT IGroupConfig::SetAxisConfiguration |
( |
[in] SAFEARRAY(struct RobotAxisConfiguration) |
axisConfig | ) |
|
This function sets the axis configuration of the group.
- Parameters
-
| [in] | axisConfig | New axis configuration of the group. |
- Returns
- Return value indicating success (>=0) or error (<0).
- Example C#:
GroupAxisConfiguration[] axisConfig = new GroupAxisConfiguration[3];
axisConfig[0].axisConfiguration = 8;
axisConfig[0].controlNumber = 0;
axisConfig[0].axisNumber = 1;
axisConfig[1].axisConfiguration = 8;
axisConfig[1].controlNumber = 0;
axisConfig[1].axisNumber = 2;
axisConfig[2].axisConfiguration = 8;
axisConfig[2].controlNumber = 0;
axisConfig[2].axisNumber = 3;
myGroup.Configuration.SetAxisConfiguration(axisConfig);
- Example VBA:
- Note:
- This method maps to the mlpiCore function
mlpiParameterWriteDataArrayUshort and writes parameter K-0-0008.
| HRESULT IGroupConfig::SetKinematicType |
( |
[in] LONG |
type | ) |
|
This function sets the kinematic type (transformation scheme) of the robot.
- Parameters
-
| [in] | type | New transformation scheme of the robot |
- Returns
- Return value indicating success (>=0) or error (<0).
- Example C#:
myGroup.Configuration.SetKinematicType(20);
- Example VBA:
- Note:
- This method maps to the mlpiCore function
mlpiParameterWriteDataArrayUshort and writes parameter K-0-0031.
| HRESULT IGroupConfig::Reset |
( |
| ) |
|
This function resets the kinematic.
- Returns
- Return value indicating success (>=0) or error (<0).
- Example C#:
myGroup.Configuration.Reset();
- Example VBA:
- Note:
- This method maps to the mlpiCore function
mlpiRobotReset, where you can find further documentation.
| HRESULT IGroupConfig::SetSafeZone |
( |
[in] SHORT |
zoneNumber, |
|
|
[in] enum RobotSafeZoneType |
zoneType, |
|
|
[in] DOUBLE |
maxPosX, |
|
|
[in] DOUBLE |
maxPosY, |
|
|
[in] DOUBLE |
maxPosZ, |
|
|
[in] DOUBLE |
minPosX, |
|
|
[in] DOUBLE |
minPosY, |
|
|
[in] DOUBLE |
minPosZ |
|
) |
| |
This function configures a safe zone of the robot.
- Parameters
-
| [in] | zoneNumber | Zone number to configure |
| [in] | zoneType | New type of the zone |
| [in] | maxPosX | New positive x-position limit of the zone |
| [in] | maxPosY | New positive y-position limit of the zone |
| [in] | maxPosZ | New positive z-position limit of the zone |
| [in] | minPosX | New negative x-position limit of the zone |
| [in] | minPosY | New negative y-position limit of the zone |
| [in] | minPosZ | New negative z-position limit of the zone |
- Returns
- Return value indicating success (>=0) or error (<0).
- Example C#:
- Example VBA:
- Note:
- This method maps to the mlpiCore function
mlpiRobotSetSafeZone
The documentation for this interface was generated from the following file: