Open Core Interface - MLPI
MLPI-MotionLogicProgrammingInterface(mlpiCore)  1.26.2
All Classes Files Functions Variables Typedefs Enumerations Enumerator Macros Modules Pages
MlpiAxisScalingVelocity Struct Reference
Collaboration diagram for MlpiAxisScalingVelocity:
Collaboration graph

Detailed Description

The following struct helps to encode or decode the velocity scaling settings of the axis given or set by mlpiMotionGetVelocityScaling or mlpiMotionSetVelocityScaling.

Example:
See mlpiMotionGetVelocityScaling mlpiMotionSetVelocityScaling

Definition at line 617 of file mlpiMotionHelper.h.


The documentation for this struct was generated from the following file: