|
The following functions provide the possibility of using customized C/C++ extension within the IEC61131-3 environment IndraWorks / IndraLogic.
With these functions, you can integrate your customized C/C++ functionality into the IEC61131-3 environment IndraWorks / IndraLogic as a IEC 61131-3 function, function block, method or property. The C/C++ functions must be implemented in a user-defined real-time extension. For more information about customized, a user-defined real-time extension and the Bosch Rexroth Workbench OEM ; please refer to the respective documents (Creating a new Downloadable Kernel Module (DKM) Project using Wind River Workbench 3.3).