|
This library contains functions to control and manage the logic runtime system on the target device. Furthermore, this library provides the symbolic read and write access to logic variables and the possibility to read and write memory areas such as the input area (like "%IB0" or "%QB0").
The table shows the PLC data types within the IEC61131 environment 'IndraLogic' and the corresponding data types within the C/C++ environment (e.g. 'Workbench OEM') of the MLPI. On reading or writing variables by symbols or memory areas, on default, you use the functions below named after the MLPI data type like mlpiLogicWriteVariableBySymbolUshort. If you include the header mlpiLogicHelper.h, you can also use the equivalent functions named after the IEC61131 data types like mlpiLogicWriteVariableBySymbolWord or like mlpiLogicWriteVariableBySymbolUint.
| Number of Bits | Data types of PLC | Data types of MLPI |
|---|---|---|
| 8 | BOOL | BOOL8 |
| 8 | SINT | CHAR |
| 16 | INT | SHORT |
| 32 | DINT | LONG |
| 64 | LINT | LLONG |
| 8 | USINT | UCHAR |
| 16 | UINT | USHORT |
| 32 | UDINT | ULONG |
| 64 | ULINT | ULLONG |
| 8 | BYTE | UCHAR |
| 16 | WORD | USHORT |
| 32 | DWORD | ULONG |
| 64 | LWORD | ULLONG |
| 32 | REAL | FLOAT |
| 64 | LREAL | DOUBLE |
| 8n | STRING | WCHAR16 |
| 16n | WSTRING | WCHAR16 |
| 16 | TIME | ULONG |
| 16 | DATE | ULONG |
| 16 | DATE_AND_TIME | ULONG |
| 16 | TIME_OF_DAY | ULONG |
| 8 | Enumerator | SHORT |