Open Core Interface - MLPI
MLPI-MotionLogicProgrammingInterface(mlpiCore)  1.26.2
Write memory area
Collaboration diagram for Write memory area:

Functions

MLPIRESULT mlpiLogicWriteMemoryAreaBool8 (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG bitOffset, const BOOL8 data)
 
MLPIRESULT mlpiLogicWriteMemoryAreaChar (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, const CHAR data)
 
MLPIRESULT mlpiLogicWriteMemoryAreaUchar (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, const UCHAR data)
 
MLPIRESULT mlpiLogicWriteMemoryAreaShort (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, const SHORT data)
 
MLPIRESULT mlpiLogicWriteMemoryAreaUshort (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, const USHORT data)
 
MLPIRESULT mlpiLogicWriteMemoryAreaLong (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, const LONG data)
 
MLPIRESULT mlpiLogicWriteMemoryAreaUlong (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, const ULONG data)
 
MLPIRESULT mlpiLogicWriteMemoryAreaLlong (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, const LLONG data)
 
MLPIRESULT mlpiLogicWriteMemoryAreaUllong (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, const ULLONG data)
 
MLPIRESULT mlpiLogicWriteMemoryAreaFloat (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, const FLOAT data)
 
MLPIRESULT mlpiLogicWriteMemoryAreaDouble (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, const DOUBLE data)
 
MLPIRESULT mlpiLogicWriteMemoryAreaArrayChar (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, const CHAR *data, const ULONG numElements)
 
MLPIRESULT mlpiLogicWriteMemoryAreaArrayUchar (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, const UCHAR *data, const ULONG numElements)
 
MLPIRESULT mlpiLogicWriteMemoryAreaArrayShort (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, const SHORT *data, const ULONG numElements)
 
MLPIRESULT mlpiLogicWriteMemoryAreaArrayUshort (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, const USHORT *data, const ULONG numElements)
 
MLPIRESULT mlpiLogicWriteMemoryAreaArrayLong (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, const LONG *data, const ULONG numElements)
 
MLPIRESULT mlpiLogicWriteMemoryAreaArrayUlong (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, const ULONG *data, const ULONG numElements)
 
MLPIRESULT mlpiLogicWriteMemoryAreaArrayLlong (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, const LLONG *data, const ULONG numElements)
 
MLPIRESULT mlpiLogicWriteMemoryAreaArrayUllong (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, const ULLONG *data, const ULONG numElements)
 
MLPIRESULT mlpiLogicWriteMemoryAreaArrayFloat (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, const FLOAT *data, const ULONG numElements)
 
MLPIRESULT mlpiLogicWriteMemoryAreaArrayDouble (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, const DOUBLE *data, const ULONG numElements)
 

Detailed Description

These functions write the following memory areas: "%Ix" (Input), "%Qx" (Output) and "%Mx" (Marker)

The table shows the PLC data types within the IEC61131 environment 'IndraLogic' and the corresponding data types within the C/C++ environment (e.g. 'Workbench OEM') of the MLPI. On writing to memory areas, on default, you use the functions below named after the MLPI data type like mlpiLogicWriteMemoryAreaUllong. If you include the header mlpiLogicHelper.h, you can also use the equivalent functions named after the IEC61131 data types like mlpiLogicWriteMemoryAreaLword or like mlpiLogicWriteMemoryAreaUlint.

Note
Reading on outputs and writing on inputs is not supported yet.
Number of Bits Data types of PLC Data types of MLPI
8 BOOL BOOL8
8 SINT CHAR
16 INT SHORT
32 DINT LONG
64 LINT LLONG
8 USINT UCHAR
16 UINT USHORT
32 UDINT ULONG
64 ULINT ULLONG
8 BYTE UCHAR
16 WORD USHORT
32 DWORD ULONG
64 LWORD ULLONG
32 REAL FLOAT
64 LREAL DOUBLE
8n STRING WCHAR16
16n WSTRING WCHAR16

Function Documentation

MLPIRESULT mlpiLogicWriteMemoryAreaBool8 ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  bitOffset,
const BOOL8  data 
)

This function writes a Boolean value e.g. a bit (BOOL8, MlpiLogicType) to the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]bitOffsetBit offset based on zero (e.g. QX0.0).
[in]dataVariable which contains the value that should be written.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Writes the data value to the memory area %QX1.5.
2 BOOL8 data = TRUE;
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicWriteMemoryAreaBool8(connection, application, MLPI_MEMORY_AREA_OUTPUT, 13, data);

Referenced by utilLogicGetSymbolListExtended().

Here is the caller graph for this function:

MLPIRESULT mlpiLogicWriteMemoryAreaChar ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
const CHAR  data 
)

This function writes the 8-bit signed data value (SINT, MlpiLogicType) to the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. QB0).
[in]dataVariable which contains the value that should be written.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Writes the data value to the memory area %QB42.
2 CHAR data = -1;
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicWriteMemoryAreaChar(connection, application, MLPI_MEMORY_AREA_OUTPUT, 42, data);

Referenced by utilLogicGetSymbolListExtended().

Here is the caller graph for this function:

MLPIRESULT mlpiLogicWriteMemoryAreaUchar ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
const UCHAR  data 
)

This function writes the 8-bit unsigned data value (BYTE, USINT, MlpiLogicType) to the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. QB0).
[in]dataVariable which contains the value that should be written.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Writes the data value to the memory area %QB42.
2 UCHAR data = 1;
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicWriteMemoryAreaUchar(connection, application, MLPI_MEMORY_AREA_OUTPUT, 42, data);

Referenced by utilLogicGetSymbolListExtended().

Here is the caller graph for this function:

MLPIRESULT mlpiLogicWriteMemoryAreaShort ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
const SHORT  data 
)

This function writes the 16-bit signed data value (INT, MlpiLogicType) to the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. QB0).
[in]dataVariable which contains the value that should be written.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Writes the data value to the memory area %QW42.
2 SHORT data = -18;
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicWriteMemoryAreaShort(connection, application, MLPI_MEMORY_AREA_OUTPUT, 42, data);

Referenced by utilLogicGetSymbolListExtended().

Here is the caller graph for this function:

MLPIRESULT mlpiLogicWriteMemoryAreaUshort ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
const USHORT  data 
)

This function writes the 16-bit unsigned data value (WORD, UINT, MlpiLogicType) to the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. QB0).
[in]dataVariable which contains the value that should be written.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Writes the data value to the memory area %QW42.
2 USHORT data = 18;
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicWriteMemoryAreaUshort(connection, application, MLPI_MEMORY_AREA_OUTPUT, 42, data);

Referenced by utilLogicGetSymbolListExtended().

Here is the caller graph for this function:

MLPIRESULT mlpiLogicWriteMemoryAreaLong ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
const LONG  data 
)

This function writes the 32-bit signed data value (DINT, MlpiLogicType) to the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. QB0).
[in]dataVariable which contains the value that should be written.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Writes the data value to the memory area %QD42.
2 LONG data = -42;
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicWriteMemoryAreaLong(connection, application, MLPI_MEMORY_AREA_OUTPUT, 42, data);

Referenced by utilLogicGetSymbolListExtended().

Here is the caller graph for this function:

MLPIRESULT mlpiLogicWriteMemoryAreaUlong ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
const ULONG  data 
)

This function writes the 32-bit unsigned data value (DWORD, UDINT, MlpiLogicType) to the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. QB0).
[in]dataVariable which contains the value that should be written.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Writes the data value to the memory area %QD42.
2 ULONG data = 42;
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicWriteMemoryAreaUlong(connection, application, MLPI_MEMORY_AREA_OUTPUT, 42, data);

Referenced by utilLogicGetSymbolListExtended().

Here is the caller graph for this function:

MLPIRESULT mlpiLogicWriteMemoryAreaLlong ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
const LLONG  data 
)

This function writes the 64-bit signed data value (LINT, MlpiLogicType) to the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. QB0).
[in]dataVariable which contains the value that should be written.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Writes the data value to the memory area %QL42.
2 LLONG data = -13;
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicWriteMemoryAreaLlong(connection, application, MLPI_MEMORY_AREA_OUTPUT, 42, data);

Referenced by utilLogicGetSymbolListExtended().

Here is the caller graph for this function:

MLPIRESULT mlpiLogicWriteMemoryAreaUllong ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
const ULLONG  data 
)

This function writes the 64-bit unsigned data value (LWORD, ULINT, MlpiLogicType) to the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. QB0).
[in]dataVariable which contains the value that should be written.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Writes the data value to the memory area %QL42.
2 ULLONG data = 13;
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicWriteMemoryAreaUllong(connection, application, MLPI_MEMORY_AREA_OUTPUT, 42, data);

Referenced by utilLogicGetSymbolListExtended().

Here is the caller graph for this function:

MLPIRESULT mlpiLogicWriteMemoryAreaFloat ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
const FLOAT  data 
)

This function writes the 32-bit floating point data value (single precision, REAL, MlpiLogicType) to the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. QB0).
[in]dataVariable which contains the value that should be written.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Writes the data value to the memory area %QD42.
2 FLOAT data = 1.234;
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicWriteMemoryAreaFloat(connection, application, MLPI_MEMORY_AREA_OUTPUT, 42, data);

Referenced by utilLogicGetSymbolListExtended().

Here is the caller graph for this function:

MLPIRESULT mlpiLogicWriteMemoryAreaDouble ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
const DOUBLE  data 
)

This function writes the 64-bit floating point data value (double precision, LREAL, MlpiLogicType) to the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. QB0).
[in]dataVariable which contains the value that should be written.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Writes the data value to the memory area %QL42.
2 DOUBLE data = 1.23456789;
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicWriteMemoryAreaDouble(connection, application, MLPI_MEMORY_AREA_OUTPUT, 42, data);

Referenced by utilLogicGetSymbolListExtended().

Here is the caller graph for this function:

MLPIRESULT mlpiLogicWriteMemoryAreaArrayChar ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
const CHAR *  data,
const ULONG  numElements 
)

This function writes an array of 8-bit signed data values (SINT, MlpiLogicType) to the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. QB0).
[in]dataPointer to variable which contains the values that should be written.
[in]numElementsNumber of CHAR elements in 'data*' available to write.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Writes the data values to the memory area %IB0 to %IB1.
2 CHAR data[] = {-1, 2};
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicWriteMemoryAreaArrayChar(connection, application, MLPI_MEMORY_AREA_OUTPUT, 0, data, _countof(data));

Referenced by utilLogicGetSymbolListExtended().

Here is the caller graph for this function:

MLPIRESULT mlpiLogicWriteMemoryAreaArrayUchar ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
const UCHAR *  data,
const ULONG  numElements 
)

This function writes an array of 8-bit unsigned data values (BYTE, USINT, MlpiLogicType) to the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. QB0).
[in]dataPointer to variable which contains the values that should be written.
[in]numElementsNumber of UCHAR elements in 'data' available to write.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Writes the data values to the memory area %IB0 to %IB1.
2 UCHAR data[] = {1, 85};
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicWriteMemoryAreaArrayUchar(connection, application, MLPI_MEMORY_AREA_OUTPUT, 0, data, _countof(data));

Referenced by utilLogicGetSymbolListExtended().

Here is the caller graph for this function:

MLPIRESULT mlpiLogicWriteMemoryAreaArrayShort ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
const SHORT *  data,
const ULONG  numElements 
)

This function writes an array of 16-bit signed data values (INT, MlpiLogicType) to the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. QB0).
[in]dataPointer to variable which contains the values that should be written.
[in]numElementsNumber of SHORT elements in 'data' available to write.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Writes the data values to the memory area %IW0 to %IW2.
2 SHORT data[] = {-18, 65};
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicWriteMemoryAreaArrayShort(connection, application, MLPI_MEMORY_AREA_OUTPUT, 0, data, _countof(data));

Referenced by utilLogicGetSymbolListExtended().

Here is the caller graph for this function:

MLPIRESULT mlpiLogicWriteMemoryAreaArrayUshort ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
const USHORT *  data,
const ULONG  numElements 
)

This function writes an array of 16-bit unsigned data values (WORD, UINT, MlpiLogicType) to the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. QB0).
[in]dataPointer to variable which contains the values that should be written.
[in]numElementsNumber of USHORT elements in 'data' available to write.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Writes the data values to the memory area %IW0 to %IW2.
2 USHORT data[] = {18, 33};
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicWriteMemoryAreaArrayUshort(connection, application, MLPI_MEMORY_AREA_OUTPUT, 0, data, _countof(data));

Referenced by utilLogicGetSymbolListExtended().

Here is the caller graph for this function:

MLPIRESULT mlpiLogicWriteMemoryAreaArrayLong ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
const LONG *  data,
const ULONG  numElements 
)

This function writes an array of 32-bit signed data values (DINT, MlpiLogicType) to the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. QB0).
[in]dataPointer to variable which contains the values that should be written.
[in]numElementsNumber of LONG elements in 'data' available to write.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Writes the data values to the memory area %ID0 to %ID4.
2 LONG data[] = {-42, 99};
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicWriteMemoryAreaArrayLong(connection, application, MLPI_MEMORY_AREA_OUTPUT, 0, data, _countof(data));

Referenced by utilLogicGetSymbolListExtended().

Here is the caller graph for this function:

MLPIRESULT mlpiLogicWriteMemoryAreaArrayUlong ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
const ULONG *  data,
const ULONG  numElements 
)

This function writes an array of 32-bit unsigned data values (DWORD, UDINT, MlpiLogicType) to the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. QB0).
[in]dataPointer to variable which contains the values that should be written.
[in]numElementsNumber of ULONG elements in 'data' available to write.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Writes the data values to the memory area %ID0 to %ID4.
2 ULONG data[] = {42, 55};
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicWriteMemoryAreaArrayUlong(connection, application, MLPI_MEMORY_AREA_OUTPUT, 0, data, _countof(data));

Referenced by utilLogicGetSymbolListExtended().

Here is the caller graph for this function:

MLPIRESULT mlpiLogicWriteMemoryAreaArrayLlong ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
const LLONG *  data,
const ULONG  numElements 
)

This function writes an array of 64-bit signed data values (LINT, MlpiLogicType) to the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. QB0).
[in]dataPointer to variable which contains the values that should be written.
[in]numElementsNumber of LLONG elements in 'data' available to write.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Writes the data values to the memory area %IL0 to %IL8.
2 LLONG data[] = {-13, 44};
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicWriteMemoryAreaArrayLlong(connection, application, MLPI_MEMORY_AREA_OUTPUT, 0, data, _countof(data));

Referenced by utilLogicGetSymbolListExtended().

Here is the caller graph for this function:

MLPIRESULT mlpiLogicWriteMemoryAreaArrayUllong ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
const ULLONG *  data,
const ULONG  numElements 
)

This function writes an array of 64-bit unsigned data values (LWORD, ULINT, MlpiLogicType) to the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. QB0).
[in]dataPointer to variable which contains the values that should be written.
[in]numElementsNumber of ULLONG elements in 'data' available to write.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Writes the data values to the memory area %IL0 to %IL8.
2 ULLONG data[] = {13, 77};
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicWriteMemoryAreaArrayUllong(connection, application, MLPI_MEMORY_AREA_OUTPUT, 0, data, _countof(data));

Referenced by utilLogicGetSymbolListExtended().

Here is the caller graph for this function:

MLPIRESULT mlpiLogicWriteMemoryAreaArrayFloat ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
const FLOAT *  data,
const ULONG  numElements 
)

This function writes an array of 32-bit floating point data values (single precision, REAL, MlpiLogicType) to the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. QB0).
[in]dataPointer to variable which contains the values that should be written.
[in]numElementsNumber of FLOAT elements in 'data' available to write.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Writes the data values to the memory area %ID0 to %ID4.
2 FLOAT data[] = {1.234, 9.907};
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicWriteMemoryAreaArrayFloat(connection, application, MLPI_MEMORY_AREA_OUTPUT, 0, data, _countof(data));

Referenced by utilLogicGetSymbolListExtended().

Here is the caller graph for this function:

MLPIRESULT mlpiLogicWriteMemoryAreaArrayDouble ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
const DOUBLE *  data,
const ULONG  numElements 
)

This function writes an array of 64-bit floating point data values (double precision, LREAL, MlpiLogicType) to the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. QB0).
[in]dataPointer to variable which contains the values that should be written.
[in]numElementsNumber of DOUBLE elements in 'data' available to write.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Writes the data values to the memory area %IL0 to %IL8.
2 DOUBLE data[] = {1.23456789, 9.87654321};
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicWriteMemoryAreaArrayDouble(connection, application, MLPI_MEMORY_AREA_OUTPUT, 0, data, _countof(data));

Referenced by utilLogicGetSymbolListExtended().

Here is the caller graph for this function: