Open Core Interface - MLPI
MLPI-MotionLogicProgrammingInterface(mlpiCore)  1.26.2
Control Tasking
Collaboration diagram for Control Tasking:

Functions

MLPIRESULT mlpiTaskWaitForEvent (const MLPIHANDLE connection, const MlpiTaskEvent taskEvent, const ULONG timeout)
 
MLPIRESULT mlpiTaskSetSystemPriority (const MLPIHANDLE connection, const MlpiSystemTask task, const ULONG priority)
 
MLPIRESULT mlpiTaskGetSystemPriority (const MLPIHANDLE connection, const MlpiSystemTask task, ULONG *priority)
 
MLPIRESULT mlpiTaskSetCurrentPriority (const MLPIHANDLE connection, const ULONG priority)
 
MLPIRESULT mlpiTaskGetCurrentPriority (const MLPIHANDLE connection, ULONG *priority)
 
MLPIRESULT mlpiTaskSetTriggerSetup (const MLPIHANDLE connection, const MlpiTaskTriggerSetup *triggerSetup, const ULONG numElements)
 
MLPIRESULT mlpiTaskGetTriggerSetup (const MLPIHANDLE connection, MlpiTaskTriggerSetup *triggerSetup, const ULONG numElements, ULONG *numElementsRet)
 
MLPIRESULT mlpiTaskSetTrigger (const MLPIHANDLE connection, const MlpiTaskTrigger *taskTrigger, const ULONG numElements)
 
MLPIRESULT mlpiTaskGetTrigger (const MLPIHANDLE connection, MlpiTaskTrigger *taskTrigger, const ULONG numElements, BOOL8 *cmdActive, ULONG *numElementsRet)
 

Detailed Description

The following functions are used for controlling task and schedule behavior.

Function Documentation

MLPIRESULT mlpiTaskWaitForEvent ( const MLPIHANDLE  connection,
const MlpiTaskEvent  taskEvent,
const ULONG  timeout 
)

This function pends the calling task until the given event occurs. You can use it to synchronize a task to a system event. This way, you can get for example a task which is activated every time data arrives from the sercos bus. Of course, your task needs to have a priority which is high enough to be activated immediately. Otherwise the time between the event and this function to return is not deterministic.

Parameters
[in]connectionHandle for multiple connections.
[in]taskEventThe event to wait for.
[in]timeoutThe timeout after which the function should return an error if the event did not raise. Use MLPI_INFINITE to wait forever.
Returns
Return value indicating success (>=0) or error (<0).
Example:
See TaskLib
MLPIRESULT mlpiTaskSetSystemPriority ( const MLPIHANDLE  connection,
const MlpiSystemTask  task,
const ULONG  priority 
)

This function sets the priority of tasks inside the system. For example, you can set the priority of the MotionKernel(MOK) here.

Parameters
[in]connectionHandle for multiple connections.
[in]taskEnum identifying the internal task.
[in]priorityThe desired priority of the task. This has to be between MLPI_PRIORITY_HIGH_MAX and MLPI_PRIORITY_HIGH_MIN.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 MLPIRESULT result = mlpiTaskSetSystemPriority(connection, MLPI_TASK_MOTIONKERNEL, MLPI_PRIORITY_HIGH_MAX);
2 if (MLPI_FAILED(result)) {
3  printf("\ncall of MLPI function failed with 0x%08x!", (unsigned)result);
4  return result;
5 }
MLPIRESULT mlpiTaskGetSystemPriority ( const MLPIHANDLE  connection,
const MlpiSystemTask  task,
ULONG *  priority 
)

This function reads back the priority of a task inside the system. For example, you can get the priority of the MotionKernel(MOK) here.

Parameters
[in]connectionHandle for multiple connections.
[in]taskEnum identifying the internal task.
[out]priorityPointer to a variable which will receive the priority of the task.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 ULONG priority = 0;
2 MLPIRESULT result = mlpiTaskGetSystemPriority(connection, MLPI_TASK_MOTIONKERNEL, &priority);
3 if (MLPI_FAILED(result)) {
4  printf("\ncall of MLPI function failed with 0x%08x!", (unsigned)result);
5  return result;
6 }
7 
8 printf("\nPriority of MotionTask is %d", priority);
MLPIRESULT mlpiTaskSetCurrentPriority ( const MLPIHANDLE  connection,
const ULONG  priority 
)

This function sets the priority of the calling task. Use this to set the priority of your own user C/C++ task to a higher level.

Parameters
[in]connectionHandle for multiple connections.
[in]priorityThe desired priority of the task. This has to be between MLPI_PRIORITY_HIGH_MAX and MLPI_PRIORITY_HIGH_MIN for real-time tasks and MLPI_PRIORITY_BACKGROUND for background tasks.
Returns
Return value indicating success (>=0) or error (<0).
Example:
See TaskLib
MLPIRESULT mlpiTaskGetCurrentPriority ( const MLPIHANDLE  connection,
ULONG *  priority 
)

Read back the priority of the calling task.

Parameters
[in]connectionHandle for multiple connections.
[out]priorityPointer to a variable receiving the current task priority of the calling task.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 ULONG priority = 0;
2 MLPIRESULT result = mlpiTaskGetCurrentPriority(connection, &priority);
3 if (MLPI_FAILED(result)) {
4  printf("\ncall of MLPI function failed with 0x%08x!", (unsigned)result);
5  return result;
6 }
7 
8 printf("\nPriority of current task is %d", priority);
MLPIRESULT mlpiTaskSetTriggerSetup ( const MLPIHANDLE  connection,
const MlpiTaskTriggerSetup *  triggerSetup,
const ULONG  numElements 
)

This function sets the configuration of the external trigger. Use this function to deactivate cyclic events and configure the behaviour of the external trigger function.
Use the options 'MLPI_TASK_TRIG_OPT_NO_CYCLIC_MOTION' and 'MLPI_TASK_TRIG_OPT_NO_CYCLIC_SERCOS' to activate or deactivate cyclic execution of the events. It is only possible to decouple events if all axis are in standstill. Events are triggered synchronous to theirs specific cycles. To change this behaviour set the option 'MLPI_TASK_TRIG_OPT_IMMEDIATE_EXECUTION'. In this case all events are executed immediately one after the other and not within their cycles.
A warning is set as long as an event is decoupled from cyclic execution. To suppress this warning set the option 'MLPI_TASK_TRIG_OPT_NO_WARNING'. If an fatal error occurs all decoupled events will be reset and coupled again, so that an error reaction can be performed. To deactivate the reset of events set the option 'MLPI_TASK_TRIG_OPT_NO_ERROR_REACTION'. The call of the function 'mlpiTaskSetTrigger' is asynchronous and will return immediately. Set the option 'MLPI_TASK_TRIG_OPT_SYNCHRONOUS' to call the function synchronous. In this case the function will return after all triggers are done.

Parameters
[in]connectionHandle for multiple connections.
[in]triggerSetupPointer to array of structures to activate and deactivate options.
[in]numElementsNumber of MlpiTaskTriggerSetup elements available in 'triggerSetup' for writing.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 //decouple motion from cyclic execution and set option synchronous
2 MlpiTaskTriggerSetup triggerSetup[2];
3 triggerSetup[0].triggerOption = MLPI_TASK_TRIG_OPT_NO_CYCLIC_MOTION;
4 triggerSetup[0].active = TRUE;
5 triggerSetup[1].triggerOption = MLPI_TASK_TRIG_OPT_SYNCHRONOUS;
6 triggerSetup[1].active = TRUE;
7 MLPIRESULT result = mlpiTaskSetTriggerSetup(connection, triggerSetup, _countof(triggerSetup));
8 if (MLPI_FAILED(result))
9 {
10  printf("\ncall of MLPI function failed with 0x%08x", (unsigned)result);
11  return result;
12 }
MLPIRESULT mlpiTaskGetTriggerSetup ( const MLPIHANDLE  connection,
MlpiTaskTriggerSetup *  triggerSetup,
const ULONG  numElements,
ULONG *  numElementsRet 
)

This function gets the configuration of the external trigger.

Parameters
[in]connectionHandle for multiple connections.
[in,out]triggerSetupPointer to array of structures to store the actual configured options.
The triggerOption is an input parameter. It defines which option is requested.
Active is an output parameter. It says if the option is activated or not.
[in]numElementsNumber of MlpiTaskTriggerSetup elements available in 'triggerSetup' for reading.
[out]numElementsRetNumber of elements used.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // get configuration of option 'MLPI_TASK_TRIG_OPT_NO_CYCLIC_MOTION'
2 ULONG numElementsRet = 0;
3 MlpiTaskTriggerSetup triggerSetup;
4 triggerSetup.triggerOption = MLPI_TASK_TRIG_OPT_NO_CYCLIC_MOTION;
5 MLPIRESULT result = mlpiTaskGetTriggerSetup(connection, &triggerSetup, 1, &numElementsRet);
6 if (MLPI_FAILED(result))
7 {
8  printf("\ncall of MLPI function failed with 0x%08x", (unsigned)result);
9  return result;
10 }
11 
12 printf("\nOption 'MLPI_TASK_TRIG_OPT_NO_CYCLIC_MOTION' is %s", (triggerSetup.active?"active":"not active"));
MLPIRESULT mlpiTaskSetTrigger ( const MLPIHANDLE  connection,
const MlpiTaskTrigger *  taskTrigger,
const ULONG  numElements 
)

This function executes the external trigger. To trigger an event it has to be decoupled from the cyclic execution. Use the 'mlpiTaskSetTriggerSetup' function to decouple the events and to configure the behavior of execution. It is not possible to execute a new trigger if an execution is still active. To check if an execution is active use the 'mlpiTaskGetTrigger' function.

Parameters
[in]connectionHandle for multiple connections.
[in]taskTriggerPointer to array of structures to activate and deactivate events.
Use the parameter numTriggers to define how often an activated events should be triggered.
[in]numElementsNumber of MlpiTaskTrigger elements available in 'taskTrigger' for writing.
Returns
Return value indicating success (>=0) or error (<0).
Attention
According to the operation mode of the real drive connected to the axis, an movement may continue once triggered. If the drive is e.g. in the velocity control mode and the event motion is triggered, the drive keeps this velocity until interrupted by a new command. Error on real drives can not be recognized if motion isn't triggered. So no error reaction can occur.
This function should be used for simulation and not on real machines.
Example:
1 // execute motion event 20 times
2 MlpiTaskTrigger taskTrigger;
3 taskTrigger.triggerEvent = MLPI_TASK_TRIG_EVT_MOTION;
4 taskTrigger.active = TRUE;
5 taskTrigger.numTriggers = 20;
6 MLPIRESULT result = mlpiTaskSetTrigger(connection, &taskTrigger, 1);
7 if (MLPI_FAILED(result))
8 {
9  printf("\ncall of MLPI function failed with 0x%08x", (unsigned)result);
10  return result;
11 }
MLPIRESULT mlpiTaskGetTrigger ( const MLPIHANDLE  connection,
MlpiTaskTrigger *  taskTrigger,
const ULONG  numElements,
BOOL8 *  cmdActive,
ULONG *  numElementsRet 
)

This function gets the configuration of the events of external trigger functionality.

Parameters
[in]connectionHandle for multiple connections.
[in,out]taskTriggerPointer to array of structures to store configuration of the events.
The triggerEvent is an input parameter. It defines which event is requested.
The parameter active defines if an event is actual active or not and numTriggers defines how many triggers are left for this event.
[in]numElementsNumber of MlpiTaskTrigger elements available in 'taskTrigger' for reading.
[out]cmdActiveTrue if an execution of an external trigger is active.
[out]numElementsRetNumber of elements used.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // get the configuration of the event 'MLPI_TASK_TRIG_EVT_MOTION' without checking of active execution
2 ULONG numElementsRet = 0;
3 MlpiTaskTrigger taskTrigger;
4 taskTrigger.triggerEvent = MLPI_TASK_TRIG_EVT_MOTION;
5 MLPIRESULT result = mlpiTaskGetTrigger(connection, &taskTrigger, 1, NULL, &numElementsRet);
6 if (MLPI_FAILED(result))
7 {
8  printf("\ncall of MLPI function failed with 0x%08x", (unsigned)result);
9  return result;
10 }
11 printf("\nThe event 'MLPI_TASK_TRIG_EVT_MOTION' is %s; number of triggers: %u", (taskTrigger.active?"active":"not active"), taskTrigger.numTriggers);
12 
13 // just check if exection of external tigger is active
14 BOOL8 cmdActive = FALSE;
15 result = mlpiTaskGetTrigger(connection, NULL, 0, &cmdActive, NULL);
16 if (MLPI_FAILED(result))
17 {
18  printf("\ncall of MLPI function failed with 0x%08x", (unsigned)result);
19  return result;
20 }
21 printf("\nThe execution of external trigger is %s", (cmdActive?"active":"not active"));