|
Macros | |
| #define | MLPI_SIDN_TYPE_DRIVE_S (0x0000000000ULL) |
| #define | MLPI_SIDN_TYPE_DRIVE_P (0x0000008000ULL) |
| #define | MLPI_SIDN_TYPE_AXIS (0x0100000000ULL) |
| #define | MLPI_SIDN_TYPE_CONTROL (0x0200000000ULL) |
| #define | MLPI_SIDN_TYPE_KINEMATIC (0x2B00000000ULL) |
| #define | MLPI_SIDN_TYPE_PROBE (0x2D00000000ULL) |
| #define | MLPI_SIDN_TYPE_POSLIMSWITCH (0x2E00000000ULL) |
| #define | MLPI_SIDN_TYPE_OSCILLOSCOPE (0x2F00000000ULL) |
| #define | MLPI_SIDN_INSTANCE_MASK (0xFF00000000000000ULL) |
| #define | MLPI_SIDN_TYPE_MASK (0xFF00008000ULL) |
| #define | MLPI_SIDN_SET_MASK (0x00007000) |
| #define | MLPI_SIDN_BLOCK_MASK (0x00000FFF) |
| #define | MLPI_SIDN_SE_MASK (0x00FF0000) |
| #define | MLPI_SIDN_SI_MASK (0xFF000000) |
| #define | MLPI_ADDRESS_MODE_LOGICAL (0x0000000000000000ULL) |
| #define | MLPI_ADDRESS_MODE_PHYSICAL (0x0000000000000001ULL) |
| #define | MLPI_ADDRESS_MODE_TOPOLOGICAL (0x0000000000000002ULL) |
| #define | MLPI_ADDRESS_MODE_LOGICAL_NATIVE (0x0000000000000003ULL) |
| #define | MLPI_ADDRESS_SLAVE_MASK (0x000000000000FFFFULL) |
| #define | MLPI_ADDRESS_MASTER_MASK (0x00000000FFFF0000ULL) |
| #define | MLPI_ADDRESS_MODE_MASK (0x000000FF00000000ULL) |
| #define | MLPI_SIDN(type, set, block, si, se) |
| #define | MLPI_SIDN_A(block) (MLPI_SIDN(MLPI_SIDN_TYPE_AXIS, 0, block, 0, 0)) |
| #define | MLPI_SIDN_C(block) (MLPI_SIDN(MLPI_SIDN_TYPE_CONTROL, 0, block,0, 0)) |
| #define | MLPI_SIDN_K(block) (MLPI_SIDN(MLPI_SIDN_TYPE_KINEMATIC, 0, block, 0, 0)) |
| #define | MLPI_SIDN_M(block) (MLPI_SIDN(MLPI_SIDN_TYPE_PROBE, 0, block, 0, 0)) |
| #define | MLPI_SIDN_N(block) (MLPI_SIDN(MLPI_SIDN_TYPE_POSLIMSWITCH, 0, block, 0, 0)) |
| #define | MLPI_SIDN_O(block) (MLPI_SIDN(MLPI_SIDN_TYPE_OSCILLOSCOPE, 0, block, 0, 0)) |
| #define | MLPI_SIDN_S(block) (MLPI_SIDN(MLPI_SIDN_TYPE_DRIVE_S, 0, block, 0, 0)) |
| #define | MLPI_SIDN_P(block) (MLPI_SIDN(MLPI_SIDN_TYPE_DRIVE_P, 0, block, 0, 0)) |
| #define | MLPI_SIDN_INST(sidn) ( (UCHAR) ((sidn & MLPI_SIDN_INSTANCE_MASK ) >> 56 ) ) |
| #define | MLPI_SIDN_TYPE(sidn) ( (ULLONG) ((sidn & MLPI_SIDN_TYPE_MASK ) ) ) |
| #define | MLPI_SIDN_SET(sidn) ( (UCHAR) ((sidn & MLPI_SIDN_SET_MASK ) >> 12 ) ) |
| #define | MLPI_SIDN_BLOCK(sidn) ( (USHORT) ((sidn & MLPI_SIDN_BLOCK_MASK) ) ) |
| #define | MLPI_SIDN_SI(sidn) ( (UCHAR) ((sidn & MLPI_SIDN_SI_MASK ) >> 24 ) ) |
| #define | MLPI_SIDN_SE(sidn) ( (UCHAR) ((sidn & MLPI_SIDN_SE_MASK ) >> 16 ) ) |
| #define | MLPI_ADDRESS(mode, master, slave) |
| #define | MLPI_PARAMETER_EIDN_MAX_LENGTH_OF_NAME ( 60) |
| #define | MLPI_PARAMETER_EIDN_MAX_LENGTH_OF_UNIT ( 12) |
| #define | MLPI_PARAMETER_EIDN_MAX_LENGTH_OF_DATA (65532) |
Typedefs | |
| typedef struct MlpiSidnError | MlpiSidnError |
| typedef struct MlpiReadEverything | MlpiReadEverything |
| typedef struct MlpiParamProcessStatus | MlpiParamProcessStatus |
| typedef struct MlpiParamWriteAccess | MlpiParamWriteAccess |
Enumerations |
List of used types, enumerations, structures and more...
| #define MLPI_SIDN_TYPE_DRIVE_S (0x0000000000ULL) |
This definition represents the valid type of an S parameter ident.
Definition at line 440 of file mlpiParameterLib.h.
| #define MLPI_SIDN_TYPE_DRIVE_P (0x0000008000ULL) |
This definition represents the valid type of a P parameter ident.
Definition at line 443 of file mlpiParameterLib.h.
| #define MLPI_SIDN_TYPE_AXIS (0x0100000000ULL) |
This definition represents the valid type of an A parameter ident.
Definition at line 446 of file mlpiParameterLib.h.
| #define MLPI_SIDN_TYPE_CONTROL (0x0200000000ULL) |
This definition represents the valid type of a C parameter ident.
Definition at line 449 of file mlpiParameterLib.h.
| #define MLPI_SIDN_TYPE_KINEMATIC (0x2B00000000ULL) |
This definition represents the valid type of a K parameter ident.
Definition at line 452 of file mlpiParameterLib.h.
| #define MLPI_SIDN_TYPE_PROBE (0x2D00000000ULL) |
This definition represents the valid type of an M parameter ident.
Definition at line 455 of file mlpiParameterLib.h.
| #define MLPI_SIDN_TYPE_POSLIMSWITCH (0x2E00000000ULL) |
This definition represents the valid type of an N parameter ident.
Definition at line 458 of file mlpiParameterLib.h.
| #define MLPI_SIDN_TYPE_OSCILLOSCOPE (0x2F00000000ULL) |
This definition represents the valid type of an O parameter ident.
Definition at line 461 of file mlpiParameterLib.h.
| #define MLPI_SIDN_INSTANCE_MASK (0xFF00000000000000ULL) |
This definition masks the instance address of a parameter ident.
Definition at line 464 of file mlpiParameterLib.h.
| #define MLPI_SIDN_TYPE_MASK (0xFF00008000ULL) |
This definition masks the element type of a parameter ident.
Definition at line 467 of file mlpiParameterLib.h.
| #define MLPI_SIDN_SET_MASK (0x00007000) |
This definition masks the element set of a parameter ident.
Definition at line 470 of file mlpiParameterLib.h.
| #define MLPI_SIDN_BLOCK_MASK (0x00000FFF) |
This definition masks the element block of a parameter ident.
Definition at line 473 of file mlpiParameterLib.h.
| #define MLPI_SIDN_SE_MASK (0x00FF0000) |
This definition masks the element SE of a parameter ident.
Definition at line 476 of file mlpiParameterLib.h.
| #define MLPI_SIDN_SI_MASK (0xFF000000) |
This definition masks the element SI of a parameter ident.
Definition at line 479 of file mlpiParameterLib.h.
| #define MLPI_ADDRESS_MODE_LOGICAL (0x0000000000000000ULL) |
Address the object by its logical address given in the lower 4 bytes.
Definition at line 498 of file mlpiParameterLib.h.
| #define MLPI_ADDRESS_MODE_PHYSICAL (0x0000000000000001ULL) |
Address the object by its physical address(sercos device address) given in the lower 4 bytes.
Definition at line 501 of file mlpiParameterLib.h.
| #define MLPI_ADDRESS_MODE_TOPOLOGICAL (0x0000000000000002ULL) |
Address the object by its topological address(position in the ring) given in the lower 4 bytes.
Definition at line 504 of file mlpiParameterLib.h.
| #define MLPI_ADDRESS_MODE_LOGICAL_NATIVE (0x0000000000000003ULL) |
Address the object by its logical address given in the lower 4 bytes, but don't convert value and attribute. Using this address mode within any other parameter access than S or P parameter will be handled like using the logical addressing mode MLPI_ADDRESS_MODE_LOGICAL.
Definition at line 509 of file mlpiParameterLib.h.
| #define MLPI_ADDRESS_SLAVE_MASK (0x000000000000FFFFULL) |
This definition masks the slave address of an address ident.
Definition at line 513 of file mlpiParameterLib.h.
| #define MLPI_ADDRESS_MASTER_MASK (0x00000000FFFF0000ULL) |
This definition masks the master address of an address ident.
Definition at line 516 of file mlpiParameterLib.h.
| #define MLPI_ADDRESS_MODE_MASK (0x000000FF00000000ULL) |
This definition masks the address mode of an address ident.
Definition at line 519 of file mlpiParameterLib.h.
| #define MLPI_SIDN | ( | type, | |
| set, | |||
| block, | |||
| si, | |||
| se | |||
| ) |
This macro creates the 64-bit value of an EIDN like <TYPE-SET-BLOCK>.<SI>.<SE> using all elements of parameter ident number.
| type | Type of parameter such as A, C, ... . Use definitions MLPI_SIDN_TYPE_AXIS, MLPI_SIDN_TYPE_CONTROL, ... to set it. |
| set | Set of parameter (value: 0..7). |
| block | Block of parameter (value: 0..4095). |
| si | SI |
| se | SE |
Definition at line 539 of file mlpiParameterLib.h.
| #define MLPI_SIDN_A | ( | block | ) | (MLPI_SIDN(MLPI_SIDN_TYPE_AXIS, 0, block, 0, 0)) |
This easy-to-use macro creates the 64-bit value of an A parameter EIDN like <TYPE-SET-BLOCK>.<SI>.<SE> using the block value.
| block | Block of parameter (value: 0..4095). |
Definition at line 550 of file mlpiParameterLib.h.
| #define MLPI_SIDN_C | ( | block | ) | (MLPI_SIDN(MLPI_SIDN_TYPE_CONTROL, 0, block,0, 0)) |
This easy-to-use macro creates the 64-bit value of an C parameter EIDN like <TYPE-SET-BLOCK>.<SI>.<SE> using the block value.
| block | Block of parameter (value: 0..4095). |
Definition at line 556 of file mlpiParameterLib.h.
| #define MLPI_SIDN_K | ( | block | ) | (MLPI_SIDN(MLPI_SIDN_TYPE_KINEMATIC, 0, block, 0, 0)) |
This easy-to-use macro creates the 64-bit value of a K parameter EIDN like <TYPE-SET-BLOCK>.<SI>.<SE> using the block value.
| block | Block of parameter (value: 0..4095). |
Definition at line 562 of file mlpiParameterLib.h.
| #define MLPI_SIDN_M | ( | block | ) | (MLPI_SIDN(MLPI_SIDN_TYPE_PROBE, 0, block, 0, 0)) |
This easy-to-use macro creates the 64-bit value of an M parameter EIDN like <TYPE-SET-BLOCK>.<SI>.<SE> using the block value.
| block | Block of parameter (value: 0..4095). |
Definition at line 568 of file mlpiParameterLib.h.
| #define MLPI_SIDN_N | ( | block | ) | (MLPI_SIDN(MLPI_SIDN_TYPE_POSLIMSWITCH, 0, block, 0, 0)) |
This easy-to-use macro creates the 64-bit value of an N parameter EIDN like <TYPE-SET-BLOCK>.<SI>.<SE> using the block value.
| block | Block of parameter (value: 0..4095). |
Definition at line 574 of file mlpiParameterLib.h.
| #define MLPI_SIDN_O | ( | block | ) | (MLPI_SIDN(MLPI_SIDN_TYPE_OSCILLOSCOPE, 0, block, 0, 0)) |
This easy-to-use macro creates the 64-bit value of an O parameter EIDN like <TYPE-SET-BLOCK>.<SI>.<SE> using the block value.
| block | Block of parameter (value: 0..4095). |
Definition at line 580 of file mlpiParameterLib.h.
| #define MLPI_SIDN_S | ( | block | ) | (MLPI_SIDN(MLPI_SIDN_TYPE_DRIVE_S, 0, block, 0, 0)) |
This easy-to-use macro creates the 64-bit value of an S parameter EIDN like <TYPE-SET-BLOCK>.<SI>.<SE> using the block value.
| block | Block of parameter (value: 0..4095). |
Definition at line 586 of file mlpiParameterLib.h.
| #define MLPI_SIDN_P | ( | block | ) | (MLPI_SIDN(MLPI_SIDN_TYPE_DRIVE_P, 0, block, 0, 0)) |
This easy-to-use macro creates the 64-bit value of a P parameter EIDN like <TYPE-SET-BLOCK>.<SI>.<SE> using the block value.
| block | Block of parameter (value: 0..4095). |
Definition at line 592 of file mlpiParameterLib.h.
| #define MLPI_SIDN_INST | ( | sidn | ) | ( (UCHAR) ((sidn & MLPI_SIDN_INSTANCE_MASK ) >> 56 ) ) |
This macro splits an EIDN address like <INSTANCE>:<TYPE-SET-BLOCK>.<SI>.<SE>
| sidn | 64-bit parameter ident number |
Definition at line 597 of file mlpiParameterLib.h.
| #define MLPI_SIDN_TYPE | ( | sidn | ) | ( (ULLONG) ((sidn & MLPI_SIDN_TYPE_MASK ) ) ) |
This macro splits an EIDN type like <TYPE-SET-BLOCK>.<SI>.<SE>
| sidn | 64-bit parameter ident number |
Definition at line 602 of file mlpiParameterLib.h.
| #define MLPI_SIDN_SET | ( | sidn | ) | ( (UCHAR) ((sidn & MLPI_SIDN_SET_MASK ) >> 12 ) ) |
This macro splits an EIDN set like <TYPE-SET-BLOCK>.<SI>.<SE>
| sidn | 64-bit parameter ident number |
Definition at line 607 of file mlpiParameterLib.h.
| #define MLPI_SIDN_BLOCK | ( | sidn | ) | ( (USHORT) ((sidn & MLPI_SIDN_BLOCK_MASK) ) ) |
This macro splits an EIDN block like <TYPE-SET-BLOCK>.<SI>.<SE>
| sidn | 64-bit parameter ident number |
Definition at line 612 of file mlpiParameterLib.h.
| #define MLPI_SIDN_SI | ( | sidn | ) | ( (UCHAR) ((sidn & MLPI_SIDN_SI_MASK ) >> 24 ) ) |
This macro splits an EIDN SI like <TYPE-SET-BLOCK>.<SI>.<SE>
| sidn | 64-bit parameter ident number |
Definition at line 617 of file mlpiParameterLib.h.
| #define MLPI_SIDN_SE | ( | sidn | ) | ( (UCHAR) ((sidn & MLPI_SIDN_SE_MASK ) >> 16 ) ) |
This macro splits an EIDN SE like <TYPE-SET-BLOCK>.<SI>.<SE>
| sidn | 64-bit parameter ident number |
Definition at line 622 of file mlpiParameterLib.h.
| #define MLPI_ADDRESS | ( | mode, | |
| master, | |||
| slave | |||
| ) |
This macro creates the 64-bit address identifier.
| mode | Type of address (logical, physical, topological). The slave element of this address identifier is interpreted based on this selection. Use the definitions MLPI_ADDRESS_MODE_LOGICAL, MLPI_ADDRESS_MODE_PHYSICAL, MLPI_ADDRESS_MODE_TOPOLOGICAL or MLPI_ADDRESS_MODE_LOGICAL_NATIVE to set it. |
| master | Master address. |
| slave | Slave address. |
Definition at line 636 of file mlpiParameterLib.h.
| #define MLPI_PARAMETER_EIDN_MAX_LENGTH_OF_NAME ( 60) |
This definition represents the maximum number of characters of the sercos parameter element 'name'.
Definition at line 651 of file mlpiParameterLib.h.
| #define MLPI_PARAMETER_EIDN_MAX_LENGTH_OF_UNIT ( 12) |
This definition represents the maximum number of characters of the sercos parameter element 'unit'.
Definition at line 654 of file mlpiParameterLib.h.
| #define MLPI_PARAMETER_EIDN_MAX_LENGTH_OF_DATA (65532) |
This definition represents the maximum number of bytes of the sercos parameter element 'data'.
Definition at line 657 of file mlpiParameterLib.h.
| MlpiSidnError |
This structure defines the information returned in case an error occurred during parameter import or export.
Elements of struct MlpiSidnError
| Type | Element | Description |
|---|---|---|
| ULLONG | parameterNumber | SIDN of parameter which has an error during import or export. |
| ULONG | errorCode | Error code of occurred error. |
| MlpiReadEverything |
This structure defines the information returned using mlpiParameterReadEverything.
Elements of struct MlpiReadEverything
| Type | Direction | Element | Description |
|---|---|---|---|
| ULLONG | [in] | address | Address identifying the object to access. Use macro MLPI_ADDRESS_x to generate an address field. |
| ULLONG | [in] | sidn | ID of parameter to be accessed. Use macro MLPI_SIDN_x to get the desired ID. |
| ULONG | [out] | validElements | Bitmask of elements, which are valid in this response invalid length elements are set to nil. |
| ULONG | [out] | dataStatus | Data status of the parameter (Parameter structure, sercos element 1). |
| ULONG | [out] | nameOffset | Offset in the buffer where the name of the parameter stands. The name is an null-terminated WCHAR16 string (Parameter structure, sercos element 2). |
| ULONG | [out] | attribute | Attribute of the parameter (Parameter structure, sercos element 3). |
| ULONG | [out] | unitOffset | Offset in the buffer where the unit of the parameter stands. The unit is an null-terminated WCHAR16 string (Parameter structure, sercos element 4). |
| ULONG | [out] | minOffset | Offset in the buffer where the minimum value of the parameter stands. (Parameter structure, sercos element 5). |
| ULONG | [out] | maxOffset | Offset in the buffer where the maximum value of the parameter stands. (Parameter structure, sercos element 6). |
| ULONG | [out] | dataLength | Length of minimum, maximum and data in octets. Length of one list element if parameter is a list. |
| ULONG | [out] | dataOffset | Offset in the buffer where the data value of the parameter stands (Parameter structure, sercos element 7) |
| ULONG | [out] | dataSize | Length of data in octets. |
| ULONG | [out] | maxDataSize | Maximum length of data in octets. Valid if parameter is a list. |
| MLPIRESULT | [out] | result | Return value indicating success (>=0) or error (<0). |
| MlpiParamProcessStatus |
This structure defines the information about a parameter process status.
Elements of struct MlpiParamProcessStatus
| Type | Element | Description |
|---|---|---|
| MlpiParameterProcessType | processType | Type of parameter process (import or export). |
| MlpiProcessState | processStatus | Status of process. |
| MLPIRESULT | processResult | Return value of asynchron function. |
| MlpiParamWriteAccess |
This structure defines the information of an parameter used by function mlpiParameterWriteAccessSetup and mlpiParameterWriteAccessStatus.
Elements of struct MlpiParamWriteAccess
| Type | Element | Description |
|---|---|---|
| ULLONG | address | Address identifying the object to access. Use macro MLPI_ADDRESS_x to generate an address field. |
| ULLONG | sidn | ID of parameter to be accessed. Use macro MLPI_SIDN_x to get the desired ID. |
This enumeration defines the type of the parameter process.
| Enumerator | |
|---|---|
| MLPI_PARAMETER_PROCESSTYPE_IMPORT |
Import. |
| MLPI_PARAMETER_PROCESSTYPE_EXPORT |
Export. |
Definition at line 667 of file mlpiParameterLib.h.
This enumeration defines the status of a command execution using mlpiParameterReadCommandStatus.
Definition at line 675 of file mlpiParameterLib.h.