Learn how to set up a simple VS2005 project which runs on the BoschRexroth VEP WinCE6.0 platform and how to access the MLP firmware using MLPI function calls.
Start Visual Studio 2005 and create a new project: ( From Menu: File->New->Project ).
Select 'Console Application' and finish the project wizard by clicking 'Finish'. You have now an empty WinCE project and may want to start developing with the MLPI-API library.
Add the MLPI-COM reference to the VB Project ( From Menu: Project->Add Reference...)
Setting Build Configuration for x86 platform ( From Menu: Build->Configuration Manager->Active Solution Platform )
You have to include the MLPI library to the project properties (Right click: Project->Properties->References) by activating it.
You are now able to use MLPI functions. Here is some example code showing how to connect to a MLC/MLP/XLC control and to read the current control firmware version. Don't forget to replace the IP address of your control in the example code.
Build your project by selecting Build->Build Solution from the Visual Studio menu.