Every MLPI function call returns an integer value of type MLPIRESULT which indicates if the function has succeeded(>=0) or not(<0). The return value is positive or zero if the call has succeeded and negative if the function call has failed. You may want to use either the MLPI_FAILED or the MLPI_SUCCEEDED macro for quick evaluation of the return value.
In most cases, the return value not only holds information about success or failure, but also information about the cause of a failure. In the mlpi header mlpiGlobal.h, there is a list of definitions with some generic and most likely error codes.
| Define | Value | Description |
|---|---|---|
| MLPI_S_OK | 0x00360000 | Return code "everything okay". |
| MLPI_E_FAIL | 0xF0360001 | General error during function call. |
| MLPI_E_NOTSUPPORTED | 0xF0360002 | The given function is not supported yet. |
| MLPI_E_INVALIDARG | 0xF0360003 | Invalid argument given to method. |
| MLPI_E_OUTOFMEMORY | 0xF0360004 | Out of memory. |
| MLPI_E_TIMEOUT | 0xF0360005 | Timeout during function call. |
| MLPI_E_SERVEREXCEPTION | 0xF0360006 | System exception on control side. |
| MLPI_E_CONNECTFAILED | 0xF0360007 | Connection failed. |
| MLPI_E_CREATEERROR | 0xF0360008 | Error creating the resource. |
| MLPI_E_SYSTEMERROR | 0xF0360009 | System error during execution. |
| MLPI_E_BUFFERTOOSHORT | 0xF036000A | Given buffer is too short. |
| MLPI_E_INVALIDSIGNATURE | 0xF036000B | Invalid signature. |
| MLPI_E_STARTERROR | 0xF036000C | Error during start of functionality. |
| MLPI_E_WATCHDOGWARNING | 0xF036000D | Watchdog warning occurred. |
| MLPI_E_WATCHDOGERROR | 0xF536000E | Watchdog error occurred. |
| MLPI_E_UNIMPLEMENTED | 0xF036000F | The given function is not implemented on this specific device. |
| MLPI_E_LIMIT_MIN | 0xF0360010 | The minimum of a limitation is exceeded. |
| MLPI_E_LIMIT_MAX | 0xF0360011 | The maximum of a limitation is exceeded. |
| MLPI_E_VERSION | 0xF0360012 | Version conflict. |
| MLPI_E_DEPRECATED | 0xF0360013 | Deprecated. The lib or function is no longer supported. |
| MLPI_E_PERMISSION | 0xF0360014 | Request declined due to missing permission rights. |
| MLPI_E_TYPE_MISSMATCH | 0xF0360015 | Type mismatch, present type doesn't match requested type. |
| MLPI_E_SIZE_MISSMATCH | 0xF0360016 | Size mismatch, present size doesn't match requested size. |
| MLPI_E_INVALID_HANDLE | 0xF0360017 | Invalid handle argument or NULL pointer argument. |
| MLPI_E_NOCONNECTION | 0xF0360018 | The connection is not established, no longer established or has been quit by peer. |
| MLPI_E_RD_WR_PROTECTION | 0xF0360019 | Request declined due to read or write protection. |
| MLPI_E_INVALID_FLOATINGPOINT | 0xF036001A | Invalid floating point numer given to method. |
| MLPI_E_NOTINITIALIZED | 0xF036001B | Object not initialized yet. |
| MLPI_E_STREAM_OUT_OF_SYNC | 0xF036001C | Send / Receive stream out of synchronization. |
| MSL_E_INVALID_PRIVATEKEY_FILE | 0xF036001D | The given private key file is broken or not existing. |
| MSL_E_INVALID_CERTIFICATE_FILE | 0xF036001E | The given certificate key file is broken or not existing. |
| MSL_E_KEYPAIR_MISSMATCH | 0xF036001F | The given certificate does not match the given private key. |
| MSL_E_TLS_HANDSHAKE_FAILED | 0xF0360020 | The TLS handshake was not successful. |
| MLPI_E_GENERAL_AC_ERROR | 0xF0360021 | General Access Control Error. |
| MLPI_E_POLICY_VIOLATION_AC | 0xF0360022 | A violation in the user policies occurred. |
| MLPI_E_USER_ALREADY_EXISTS | 0xF0360023 | The given username is already in use. |
| MLPI_E_GROUP_ALREADY_EXISTS | 0xF0360024 | The given groupname is already in use. |
| MLPI_E_MEMBERSHIP_ALREADY_EXISTS | 0xF0360025 | The given user is already member of the given group. |
| MLPI_E_USER_NOT_EXISTING | 0xF0360026 | The given user does not exist on the control. |
| MLPI_E_GROUP_NOT_EXISTING | 0xF0360027 | The given group does not exist on the control. |
| MLPI_E_MEMBERSHIP_NOT_EXISTING | 0xF0360028 | The given user is not member of the given group. |
Please note that this is not a complete list of all possible return values a MLPI function might return. Besides these common error codes, there are also many device specific error codes. These error codes are specific to the facility (for example, Motion, Logic, sercos, drive...) of the connected device and not directly part of the MLPI. Still, all these error codes are unique and based on the idea that a failure message is a negative value (0xFxxxxxxx) and a success message is a positive value (0x0xxxxxxx). The difference to the errors listed above is that you won't find the description of the error code within this documentation, but within the documentation of the MLPI device you are connected to. For example, if you are connected to a XLC/MLC device, you will probably find more help on the error code by looking into the XLC/MLC diagnostics documentation which is not directly part of the MLPI SDK. In most cases, you will find the documentation included in an IndraWorks installation or you may want to download an up-to-date version from the http://www.boschrexroth.com homepage.
Running this program and having no device with address 99 will result in the following output:
For more insight into debugging and the system, you may want to have a look at TraceLib and its usage.
Each functionality on the client side needs a related functionality on the server side, meaning on the control. The following table shows the implemented server version of the MLPI at a certain firmware version of the control. You can find out the MLPI server version of your control by mlpiApiGetServerCoreVersion. You can read out the firmware version of your control by mlpiSystemGetVersionInfo.
| Server version of MLPI | Firmware version of control |
|---|---|
| 1.0.16.0 | 13V02 |
| 1.0.20.0 | 13V04 |
| 1.3.2.0 | 13V06 |
| 1.3.2.0 | 13V08 |
| 1.3.2.1 | 13V08 Patch 4 |
| 1.4.0.0 | 13V10 |
| 1.6.5.0 | 13V12 Patch 1 |
| 1.6.5.0 | 13V14 |
| 1.11.3.0 | 14V06 |
| 1.17.0.0 | 14V18 |
| 1.20.0.0 | 14V20 |
The Motion Logic Programming Interface (MLPI) supports a wide range of programming languages and environments. Starting at version 1.17.0, the SDK supports data integrity during communication and management of security services located at the target device. Integrity of the communication data is supported by MLPIS. Management of security services consists of two MLPI libraries named SecurityLib and AccessControlLib.
The following symbols specify the availability of MLPI and MLPIS Communication (see Security in MLPI) and SecurityLib and AccessControlLib.
| Library | Location | Library | Communication | Libraries | ||
|---|---|---|---|---|---|---|
| MLPI | MLPIS | SecurityLib | AccessControlLib | |||
| mlpiCoreClient | mlpiCoreClient\lib | win_pharlap-vs2005 | ||||
| wince-vs2005sp1-x86 | ||||||
| win-vs2005sp1-x86 | ||||||
| win-vs2005sp1-x64 | ||||||
| vxw69-gcc-ATOMgnu_RTP | ||||||
| android-ndk_gcc-armv7 | ||||||
| macosx-xcode-x86_64_i386 | ||||||
| ios-xcode-arm64_armv7 | ||||||
| ios-xcode-x86_64_i386 | ||||||
| ios-xcode-x86_64_i386_arm64_armv7 | ||||||
| mlpiCoreClient\bin | win_pharlap-vs2005sp1-x86 | |||||
| win_pharlap-vs2005sp1-x64 | ||||||
| wince-vs2005sp1-x86 | ||||||
| win-vs2005sp1-x86 | ||||||
| win-vs2005sp1-x64 | ||||||
| vxw69-gcc-ATOMgnu_RTP | ||||||
| win-vs2012-x86 | ||||||
| win-vs2012-x64 | ||||||
| linux-lvrt2014_gcc-x64 | ||||||
| linux-lvrt2014_gcc-armv7 | ||||||
| linux-gcc-x86 | ||||||
| linux-gcc-x64 | ||||||
| linux-gcc-armv7hf | ||||||
| linux-gcc-armv7 | ||||||
| mlpi4Java | mlpi4Java\bin | win-vs2005sp1-x86 | ||||
| win-vs2005sp1-x64 | ||||||
| win-vs2012-x86 | ||||||
| win-vs2012-x64 | ||||||
| linux-gcc-x86 | ||||||
| linux-gcc-x64 | ||||||
| linux-gcc-armv7hf | ||||||
| linux-gcc-armv7 | ||||||
| android-ndk_gcc-armv7 | ||||||
| mlpi4Lua | mlpi4Lua\bin | win_luadist-any-x86 | ||||
| win-any-x86 | ||||||
| win-any-x64 | ||||||
| mlpi4COM | mlpi4COM\bin | wince-vs2005sp1-x86 | ||||
| win-vs2005sp1-x86 | ||||||
| win-vs2005sp1-x64 | ||||||
| mlpi4LabVIEW | mlpi4LabVIEW\bin\win-labview2016-any\mlpi4LabVIEW_NativeInterface | win_pharlap-vs2005sp1-x86 | ||||
| win-vs2005sp1-x86 | ||||||
| win-vs2005sp1-x64 | ||||||
| win-vs2012-x86 | ||||||
| win-vs2012-x64 | ||||||
| linux-lvrt2014_gcc-x64 | ||||||
| linux-lvrt2014_gcc-ARMv7 | ||||||
| mlpi4MATLAB | mlpi4MATLAB\bin | dllmlpiwin32.dll | ||||
| mlpi4Modelica | mlpi4Modelica\lib\mlpi4Modelica\Resources\Library | win32 | ||||
| win64 | ||||||
| Symbol | Definition |
|---|---|
| X | Supported |
| - | Unsupported |