|
Modules | |
| UtilApiHelper | |
| UtilGlobalHelper | |
| UtilLogicHelper | |
| UtilIoHelper | |
| UtilMotionHelper | |
| UtilParameterHelper | |
| UtilWchar16 | |
This collection of utilities is helpful for using the MLPI.
Please note that this piece of source code is not directly part of the MLPI. You do not need this file to program against the MLPI. Nevertheless, at least parts of this file have been considered to be somewhat useful when using or learning to use MLPI functionality. It is therefore included without any support, but to act as sample code and source of inspiration.