|
Modules | |
| Movement functions | |
| Configuration functions | |
| Robot information | |
| Robot TeachIn | |
| Version and Permission | |
| Structs, types, ... | |
This robot library provides functionality for defining a robot, commanding motion and getting robot information.
The following functions all deal with the motion of a robot. In general, "robot" is used to address a robot. Each motion command usually uses a structure to pass on the information about a particular move. The command will be executed in the control and returns a handle. This handle must be used in future requests for getting status information. The handle and the robot reference a particular motion command. One robot can have multiple active commands (for example, MoveLinearAbs is one and a MoveLinearRel is commanded). A previous commanded move will not be interrupted by a currently executed move. All moves will be executed consecutively.