Open Core Interface - MLPI
MLPI-MotionLogicProgrammingInterface(mlpi4LabVIEW)  1.26.2
Trace modules
Collaboration diagram for Trace modules:

Functions

MLPIRESULT mlpiTraceActivateModule (const MLPIHANDLE connection, const WCHAR16 *moduleName)
 
MLPIRESULT mlpiTraceDeactivateModule (const MLPIHANDLE connection, const WCHAR16 *moduleName)
 
MLPIRESULT mlpiTraceActivateAllModules (const MLPIHANDLE connection)
 
MLPIRESULT mlpiTraceDeactivateAllModules (const MLPIHANDLE connection)
 
MLPIRESULT mlpiTraceGetNumberOfModules (const MLPIHANDLE connection, ULONG *numberOfModules)
 
MLPIRESULT mlpiTraceGetModuleList (const MLPIHANDLE connection, MlpiTraceModuleInformation *moduleInfo, const ULONG numElements, ULONG *numElementsRet=0)
 

Detailed Description

Use the following functions to activate, deactivate and read information about the trace modules.

Function Documentation

MLPIRESULT mlpiTraceActivateModule ( const MLPIHANDLE  connection,
const WCHAR16 *  moduleName 
)

This function activates a trace module. Trace messages to modules which are not activated will not be written to the trace buffer. This means, that you have to activate a module to trace its messages. Available Module names can be retrieved with the function mlpiTraceGetModuleList. It is highly recommended to use the macro MLPI_TRACE_MODULE_USER for your code.

Note
Enabling trace modules might cost some CPU performance.
Parameters
[in]connectionHandle for multiple connections.
[out]moduleNamePointer to module name string.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Activate only the module 'MLPI_TRACE_MODULE_USER'
2 MLPIRESULT result = mlpiTraceActivateModule(connection, MLPI_TRACE_MODULE_USER);
3 if (MLPI_FAILED(result)) {
4  printf("\ncall of MLPI function failed with 0x%08x!", result);
5  return result;
6 }
MLPIRESULT mlpiTraceDeactivateModule ( const MLPIHANDLE  connection,
const WCHAR16 *  moduleName 
)

This function deactivates a trace module. Messages to a deactivated trace module are ignored by the tracing system and thus will not appear in the trace buffer. Available Module names can be retrieved with the function mlpiTraceGetModuleList.

Parameters
[in]connectionHandle for multiple connections.
[out]moduleNamePointer to module name string.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Deactivate only the module 'MLPI_TRACE_MODULE_USER'
2 MLPIRESULT result = mlpiTraceDeactivateModule(connection, MLPI_TRACE_MODULE_USER);
3 if (MLPI_FAILED(result)) {
4  printf("\ncall of MLPI function failed with 0x%08x!", result);
5  return result;
6 }
MLPIRESULT mlpiTraceActivateAllModules ( const MLPIHANDLE  connection)

This function activates all available trace modules.

Note
Enabling all trace modules might result in a performance drop, as tracing costs CPU time. It is not recommended to enable all trace modules on a productive machine. Try activating only the modules of interest, or one module at a time.
Parameters
[in]connectionHandle for multiple connections.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // activate all available trace modules (not recommended!)
2 MLPIRESULT result = mlpiTraceActivateAllModules(connection);
3 if (MLPI_FAILED(result)) {
4  printf("\ncall of MLPI function failed with 0x%08x!", result);
5  return result;
6 }
MLPIRESULT mlpiTraceDeactivateAllModules ( const MLPIHANDLE  connection)

This function deactivates all available trace modules.

Parameters
[in]connectionHandle for multiple connections.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // activate all available trace modules
2 MLPIRESULT result = mlpiTraceDeactivateAllModules(connection);
3 if (MLPI_FAILED(result)) {
4  printf("\ncall of MLPI function failed with 0x%08x!", result);
5  return result;
6 }
MLPIRESULT mlpiTraceGetNumberOfModules ( const MLPIHANDLE  connection,
ULONG *  numberOfModules 
)

This function returns the number of registered modules.

Parameters
[in]connectionHandle for multiple connections.
[out]numberOfModulesNumber of registered modules.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 ULONG numModules=0;
2 MLPIRESULT result = mlpiTraceGetNumberOfModules(connection, &numModules);
3 if (MLPI_FAILED(result)) {
4  printf("\ncall of MLPI function failed with 0x%08x!", result);
5  return result;
6 }
7 
8 printf("\nNumber of available trace modules: %d", numModules);
MLPIRESULT mlpiTraceGetModuleList ( const MLPIHANDLE  connection,
MlpiTraceModuleInformation *  moduleInfo,
const ULONG  numElements,
ULONG *  numElementsRet = 0 
)

This function returns a list of all modules currently available in the tracing system. The module information also contains the name of each module. This name can be used with other calls to the tracing system.

Parameters
[in]connectionHandle for multiple connections.
[out]moduleInfoPointer to an array which will receive the module information. One element for each module.
[in]numElementsArray size of buffer given to function in number of elements.
[out]numElementsRetReturns the actual number of elements returned.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 ULONG numModules=0;
2 MlpiTraceModuleInformation modules[MLPI_TRACE_MAX_MODULES];
3 
4 // read array of available modules
5 MLPIRESULT result = mlpiTraceGetModuleList(connection, modules, _countof(modules), &numModules);
6 if (MLPI_FAILED(result)) {
7  printf("\ncall of MLPI function failed with 0x%08x!", result);
8  return result;
9 }
10 
11 // print all modules found
12 printf("\nFound %d Modules\n", numModules);
13 printf("\n ModuleName | Active | StdOut | Main | Separat| Buffer ");
14 printf("\n---------------------+--------+--------+--------+--------+-------- ");
15 for (ULONG i=0; i<numModules; i++)
16 {
17  printf("\n%20S", modules[i].moduleName);
18  printf(" |%7s", (modules[i].isActive) ? "TRUE" : "FALSE");
19  printf(" |%7s", (modules[i].toStdOut) ? "TRUE" : "FALSE");
20  printf(" |%7s", (modules[i].toMainBuffer) ? "TRUE" : "FALSE");
21  printf(" |%7s", (modules[i].toSeparateBuffer) ? "TRUE" : "FALSE");
22  printf(" | %s", W2A16(modules[i].bufferName));
23 }