Open Core Interface - MLPI
MLPI-MotionLogicProgrammingInterface(mlpi4LabVIEW)  1.26.2
Server versions before 1.26.0.0
Collaboration diagram for Server versions before 1.26.0.0:

Version and permission information.

The following table shows the requirements regarding the minimum server version (Server versions of MLPI) and the user permissions needed to execute the desired functions. Furthermore, the table shows the current user and permissions setup of the 'accounts.xml' placed on the SYSTEM partition of the control. When using the permission "MLPI_SECURITYLIB_PERMISSION_ALL" with the value "true", all functions of this library are enabled for the given user account.

Note
Functions with permission MLPI_SECURITYLIB_PERMISSION_ALWAYS cannot be blocked.
List of permissions for mlpiSecurityLib that can be configured in 'accounts.xml'
  • MLPI_SECURITYLIB_PERMISSION_ALWAYS
  • MLPI_SECURITYLIB_PERMISSION_CONFIG
  • MLPI_SECURITYLIB_PERMISSION_INFO
  • MLPI_SECURITYLIB_PERMISSION_ALL
Function Server version Permission a(1) i(1) i(2) i(3) m(1)
mlpiSecurityGetNetworkServiceInformation 1.15.0.0 "MLPI_SECURITYLIB_PERMISSION_INFO" x x x x
mlpiSecurityGetNetworkServiceActivation 1.15.0.0 "MLPI_SECURITYLIB_PERMISSION_INFO" x x x x
mlpiSecuritySetNetworkServiceActivation 1.15.0.0 "MLPI_SECURITYLIB_PERMISSION_SETUP" x x x x
mlpiSecurityGetNetworkServiceConfiguration 1.19.0.0 "MLPI_SECURITYLIB_PERMISSION_INFO" x x x x
mlpiSecuritySetNetworkServiceConfiguration 1.19.0.0 "MLPI_SECURITYLIB_PERMISSION_SETUP" x x x x
shortcut user account
a(1) administrator
i(1) indraworks
i(2) indraworksonline
i(3) indraworksadministrator
m(1) MlcTrending