|
Macros | |
| #define | MLPI_ROBOT_COORDINATES_IN_POINT (16) |
| #define | MLPI_ROBOT_MAX_POS_AXIS (3) |
| #define | MLPI_ROBOT_AXIS_COUNT (16) |
| #define | MLPI_ROBOT_MAX_UNIT_LEN (12) |
| #define | MLPI_ROBOT_MAX_CSNAME_LEN (30) |
| #define | MLPI_ROBOT_MAX_COORDINATE_SYSTEMS (19) |
| #define | MLPI_ROBOT_MAX_SAFEZONES (32) |
| #define | MLPI_ROBOT_MAX_TEACH_NAME_LEN (21) |
Typedefs | |
| typedef enum MlpiRobotAxisTypes | MlpiRobotAxisTypes |
| typedef enum MlpiRobotSetMode | MlpiRobotSetMode |
| typedef enum MlpiRobotCoordinateSystem | MlpiRobotCoordinateSystem |
| typedef enum MlpiRobotCSType | MlpiRobotCSType |
| typedef enum MlpiRobotPointType | MlpiRobotPointType |
| typedef enum MlpiRobotSlopeType | MlpiRobotSlopeType |
| typedef enum MlpiRobotSyncErrorReactionMode | MlpiRobotSyncErrorReactionMode |
| typedef enum MlpiRobotCyclicMode | MlpiRobotCyclicMode |
| typedef enum MlpiRobotMechCmd | MlpiRobotMechCmd |
| typedef enum MlpiRobotSafeZoneType | MlpiRobotSafeZoneType |
| typedef enum MlpiRobotTeachInWriteOption | MlpiRobotTeachInWriteOption |
| typedef enum MlpiRobotTeachInPointFileOption | MlpiRobotTeachInPointFileOption |
| typedef enum MlpiRobotCmdInfoType | MlpiRobotCmdInfoType |
| typedef struct MlpiRobotMotionStatus | MlpiRobotMotionStatus |
| typedef struct MlpiRobotPoint | MlpiRobotPoint |
| typedef struct MlpiRobotMoveLinearAbsolute | MlpiRobotMoveLinearAbsolute |
| typedef struct MlpiRobotMoveLinearRelative | MlpiRobotMoveLinearRelative |
| typedef struct MlpiRobotMoveDirectAbsolute | MlpiRobotMoveDirectAbsolute |
| typedef struct MlpiRobotMoveDirectRelative | MlpiRobotMoveDirectRelative |
| typedef struct MlpiRobotMoveCircularAbsolute | MlpiRobotMoveCircularAbsolute |
| typedef struct MlpiRobotMoveCircularRelative | MlpiRobotMoveCircularRelative |
| typedef struct MlpiRobotMoveJumpAbsolute | MlpiRobotMoveJumpAbsolute |
| typedef struct MlpiRobotSetBeltConfiguration | MlpiRobotSetBeltConfiguration |
| typedef struct MlpiRobotGetBeltConfiguration | MlpiRobotGetBeltConfiguration |
| typedef struct MlpiRobotSetBeltErrorReaction | MlpiRobotSetBeltErrorReaction |
| typedef struct MlpiRobotGetBeltErrorReaction | MlpiRobotGetBeltErrorReaction |
| typedef struct MlpiRobotSyncOffWithLimits | MlpiRobotSyncOffWithLimits |
| typedef struct MlpiRobotSyncOnWithLimits | MlpiRobotSyncOnWithLimits |
| typedef struct MlpiRobotSetTrafoParameter | MlpiRobotSetTrafoParameter |
| typedef struct MlpiRobotGetTrafoParameter | MlpiRobotGetTrafoParameter |
| typedef struct MlpiRobotOpenCyclicChannel | MlpiRobotOpenCyclicChannel |
| typedef struct MlpiRobotCyclicChannel | MlpiRobotCyclicChannel |
| typedef struct MlpiRobotPerformanceResult | MlpiRobotPerformanceResult |
| typedef struct MlpiRobotMechanicData | MlpiRobotMechanicData |
| typedef struct MlpiKinematicsValues | MlpiKinematicsValues |
| typedef struct MlpiKinematicsUnits | MlpiKinematicsUnits |
| typedef struct MlpiRobotStop | MlpiRobotStop |
| typedef struct MlpiRobotInterrupt | MlpiRobotInterrupt |
| typedef struct MlpiRobotSafeZoneData | MlpiRobotSafeZoneData |
| typedef struct MlpiRobotJogStepData | MlpiRobotJogStepData |
| typedef struct MlpiRobotJogContData | MlpiRobotJogContData |
| typedef struct MlpiRobotStopCmdData | MlpiRobotStopCmdData |
| typedef struct MlpiRobotBeltDesyncRelData | MlpiRobotBeltDesyncRelData |
| typedef struct MlpiRobotTeachInDataWrite | MlpiRobotTeachInDataWrite |
| typedef struct MlpiRobotTeachInDataRead | MlpiRobotTeachInDataRead |
| typedef struct MlpiRobotTeachInDataReadNext | MlpiRobotTeachInDataReadNext |
| typedef struct MlpiRobotTeachInDataDeletePoints | MlpiRobotTeachInDataDeletePoints |
| typedef struct MlpiRobotTeachInDataFileData | MlpiRobotTeachInDataFileData |
| typedef struct MlpiRobotTeachInDataDeleteFileData | MlpiRobotTeachInDataDeleteFileData |
| typedef struct MlpiRobotGetStatusSummary | MlpiRobotGetStatusSummary |
| typedef struct MlpiRobotCoordinateSystemInfo | MlpiRobotCoordinateSystemInfo |
| typedef struct MlpiRobotCmdInfo | MlpiRobotCmdInfo |
| typedef struct MlpiRobotChangeToolParameter | MlpiRobotChangeToolParameter |
Enumerations |
List of used types, enumerations, structures and more...
| #define MLPI_ROBOT_COORDINATES_IN_POINT (16) |
number of coordinates in a point
Definition at line 319 of file mlpiRobotLib.h.
| #define MLPI_ROBOT_MAX_POS_AXIS (3) |
number of positioning axes
Definition at line 320 of file mlpiRobotLib.h.
| #define MLPI_ROBOT_AXIS_COUNT (16) |
number of axis of a robot
Definition at line 321 of file mlpiRobotLib.h.
| #define MLPI_ROBOT_MAX_UNIT_LEN (12) |
maximum length of unit name
Definition at line 322 of file mlpiRobotLib.h.
| #define MLPI_ROBOT_MAX_CSNAME_LEN (30) |
maximum length of coordinate system name
Definition at line 323 of file mlpiRobotLib.h.
| #define MLPI_ROBOT_MAX_COORDINATE_SYSTEMS (19) |
maximum number of coordinate systems
Definition at line 324 of file mlpiRobotLib.h.
| #define MLPI_ROBOT_MAX_SAFEZONES (32) |
maximum number of safezones
Definition at line 326 of file mlpiRobotLib.h.
| #define MLPI_ROBOT_MAX_TEACH_NAME_LEN (21) |
maximum name length of teach points
Definition at line 327 of file mlpiRobotLib.h.
| typedef enum MlpiRobotAxisTypes MlpiRobotAxisTypes |
This enumeration defines the types of axes used in a robot. This is parameter K-0-0008.
| typedef enum MlpiRobotSetMode MlpiRobotSetMode |
This enumeration defines the set mode of movement commands.
| typedef enum MlpiRobotCoordinateSystem MlpiRobotCoordinateSystem |
This enumeration defines coordinate systems of a robot.
| typedef enum MlpiRobotCSType MlpiRobotCSType |
This enumeration defines the type of the coordinate system.
| typedef enum MlpiRobotPointType MlpiRobotPointType |
This enumeration defines the point type.
| typedef enum MlpiRobotSlopeType MlpiRobotSlopeType |
This enumeration defines the slope types of movement commands.
This enumeration defines the error reaction mode of a belt.
| typedef enum MlpiRobotCyclicMode MlpiRobotCyclicMode |
This enum defines the type of a cyclic position command.
| typedef enum MlpiRobotMechCmd MlpiRobotMechCmd |
This enum defines the command for a mechanical object.
| typedef enum MlpiRobotSafeZoneType MlpiRobotSafeZoneType |
This enum defines the type of a save zone.
| typedef enum MlpiRobotTeachInWriteOption MlpiRobotTeachInWriteOption |
This enum defines the possible options for writing a point while the TeachIn functions.
This enum defines the options, how a file can be loaded or saved.
| typedef enum MlpiRobotCmdInfoType MlpiRobotCmdInfoType |
This enum defines the type of information which should be read.
| MlpiRobotMotionStatus |
This structure defines the status of a robot movement command.
Elements of struct MlpiRobotMotionStatus
| Type | Element | Description |
|---|---|---|
| BOOL8 | done | TRUE when command is completed |
| BOOL8 | active | TRUE as long as command is active |
| BOOL8 | inbuffer | TRUE when command is in buffer |
| BOOL8 | commandaborted | TRUE when command has been aborted by another command |
| BOOL8 | error | TRUE when motion command issued an error |
| USHORT | errorID | Identifier of error |
| USHORT | table | Table identifier of error |
| ULONG | additional1 | Additional diagnosis number1 |
| ULONG | additional2 | Additional diagnosis number2 |
| MlpiRobotPoint |
This structure defines a point.
Elements of struct MlpiRobotPoint
| Type | Element | Description |
|---|---|---|
| array of DOUBLE | coordinate | Array of coordinates of a point with MLPI_ROBOT_COORDINATES_IN_POINT elements. |
| MlpiRobotMoveLinearAbsolute |
This structure defines the parameters of a linear absolute movement.
Elements of struct MlpiRobotMoveLinearAbsolute
| Type | Element | Description |
|---|---|---|
| MlpiRobotPoint | point | End Point of movement |
| DOUBLE | velocity | Maximum velocity of movement |
| DOUBLE | acceleration | Maximum acceleration of movement |
| DOUBLE | deceleration | Maximum deceleration of movement |
| DOUBLE | jerk | Maximum jerk of movement |
| DOUBLE | blendingRadius | Commanded radius of blending movement |
| MlpiRobotSetMode | setMode | set mode |
| MlpiRobotCoordinateSystem | coordSystem | coordinate system |
| MlpiRobotSlopeType | slopeType | slope type |
| MlpiRobotMoveLinearRelative |
This structure defines the parameters of a linear relative movement.
Elements of struct MlpiRobotMoveLinearRelative
| Type | Element | Description |
|---|---|---|
| MlpiRobotPoint | distance | Distance of movement |
| DOUBLE | velocity | Maximum velocity of movement |
| DOUBLE | acceleration | Maximum acceleration of movement |
| DOUBLE | deceleration | Maximum deceleration of movement |
| DOUBLE | jerk | Maximum jerk of movement |
| DOUBLE | blendingRadius | Commanded radius of blending movement |
| MlpiRobotSetMode | setMode | set mode |
| MlpiRobotCoordinateSystem | coordSystem | coordinate system |
| MlpiRobotSlopeType | slopeType | slope type |
| MlpiRobotMoveDirectAbsolute |
This structure defines the parameters of an absolute direct movement.
Elements of struct MlpiRobotMoveDirectAbsolute
| Type | Element | Description |
|---|---|---|
| MlpiRobotPoint | point | End Point of movement |
| DOUBLE | velocity | Maximum velocity of movement |
| DOUBLE | acceleration | Maximum acceleration of movement |
| DOUBLE | deceleration | Maximum deceleration of movement |
| DOUBLE | jerk | Maximum jerk of movement |
| DOUBLE | blendingRadius | Commanded radius of blending movement |
| MlpiRobotSetMode | setMode | set mode |
| MlpiRobotCoordinateSystem | coordSystem | coordinate system |
| MlpiRobotSlopeType | slopeType | slope type |
| MlpiRobotMoveDirectRelative |
This structure defines the parameters of a direct relative movement.
Elements of struct MlpiRobotMoveDirectRelative
| Type | Element | Description |
|---|---|---|
| MlpiRobotPoint | distance | Distance of movement |
| DOUBLE | velocity | Maximum velocity of movement |
| DOUBLE | acceleration | Maximum acceleration of movement |
| DOUBLE | deceleration | Maximum deceleration of movement |
| DOUBLE | jerk | Maximum jerk of movement |
| DOUBLE | blendingRadius | Commanded radius of blending movement |
| MlpiRobotSetMode | setMode | set mode |
| MlpiRobotCoordinateSystem | coordSystem | coordinate system |
| MlpiRobotSlopeType | slopeType | slope type |
| MlpiRobotMoveCircularAbsolute |
This structure defines the parameters of an absolute circular movement.
Elements of struct MlpiRobotMoveCircularAbsolute
| Type | Element | Description |
|---|---|---|
| MlpiRobotPoint | auxPoint | Aux Point of movement |
| MlpiRobotPoint | endPoint | End Point of movement |
| DOUBLE | velocity | Maximum velocity of movement |
| DOUBLE | acceleration | Maximum acceleration of movement |
| DOUBLE | deceleration | Maximum deceleration of movement |
| DOUBLE | jerk | Maximum jerk of movement |
| DOUBLE | blendingRadius | Commanded radius of blending movement |
| MlpiRobotSetMode | setMode | set mode |
| MlpiRobotCoordinateSystem | coordSystem | coordinate system |
| MlpiRobotSlopeType | slopeType | slope type |
| MlpiRobotMoveCircularRelative |
This structure defines the parameters of a circular relative movement.
Elements of struct MlpiRobotMoveCircularRelative
| Type | Element | Description |
|---|---|---|
| MlpiRobotPoint | auxPoint | Aux Point of movement |
| MlpiRobotPoint | endPoint | End Point of movement |
| DOUBLE | velocity | Maximum velocity of movement |
| DOUBLE | acceleration | Maximum acceleration of movement |
| DOUBLE | deceleration | Maximum deceleration of movement |
| DOUBLE | jerk | Maximum jerk of movement |
| DOUBLE | blendingRadius | Commanded radius of blending movement |
| MlpiRobotSetMode | setMode | set mode |
| MlpiRobotCoordinateSystem | coordSystem | coordinate system |
| MlpiRobotSlopeType | slopeType | slope type |
| MlpiRobotMoveJumpAbsolute |
This structure defines the parameters of a jump absolute movement.
Elements of struct MlpiRobotMoveJumpAbsolute
| Type | Element | Description |
|---|---|---|
| MlpiRobotPoint | point | End Point of movement |
| DOUBLE | velocity | Maximum velocity of movement |
| DOUBLE | acceleration | Maximum acceleration of movement |
| DOUBLE | deceleration | Maximum deceleration of movement |
| DOUBLE | jerk | Maximum jerk of movement |
| DOUBLE | blendingRadius | Commanded radius of blending movement |
| MlpiRobotSetMode | setMode | set mode |
| MlpiRobotCoordinateSystem | coordSystem | coordinate system |
| MlpiRobotSlopeType | slopeType | slope type |
| DOUBLE | startHeight | Minimal start height before the horizontal movement |
| DOUBLE | maxHeight | Maximum height of movement |
| DOUBLE | endHeight | Minimal end height after the horizontal movement |
| MlpiRobotSetBeltConfiguration |
This structure defines the parameters for the configuration of a belt.
Elements of struct MlpiRobotSetBeltConfiguration
| Type | Element | Description |
|---|---|---|
| MlpiAxisRef | belt | Reference to the belt |
| DOUBLE | posX | X position of the belt in MCS |
| DOUBLE | posY | Y position of the belt in MCS |
| DOUBLE | posZ | Z position of the belt in MCS |
| DOUBLE | rotA | rotation of belt around x axis in MCS |
| DOUBLE | rotB | rotation of belt around y axis in MCS |
| DOUBLE | rotC | rotation of belt around z axis in MCS |
| DOUBLE | begin | begin length of belt synchronous working area |
| DOUBLE | total | total length of belt synchronous working area |
| MlpiRobotGetBeltConfiguration |
This structure defines the belt configuration.
Elements of struct MlpiRobotGetBeltConfiguration
| Type | Direction | Element | Description |
|---|---|---|---|
| MlpiAxisRef | [in] | belt | Reference to the belt |
| DOUBLE | [out] | posX | X position of the belt in MCS |
| DOUBLE | [out] | posY | Y position of the belt in MCS |
| DOUBLE | [out] | posZ | Z position of the belt in MCS |
| DOUBLE | [out] | rotA | rotation of belt around x axis in MCS |
| DOUBLE | [out] | rotB | rotation of belt around y axis in MCS |
| DOUBLE | [out] | rotC | rotation of belt around z axis in MCS |
| DOUBLE | [out] | begin | begin length of belt synchronous working area |
| DOUBLE | [out] | total | total length of belt synchronous working area |
| MlpiRobotCSType | [out] | csType | Type of coordinate system |
| MlpiRobotSetBeltErrorReaction |
This structure defines the parameters for the configuration of the error reaction of a belt.
Elements of struct MlpiRobotSetBeltErrorReaction
| Type | Element | Description |
|---|---|---|
| MlpiAxisRef | belt | Reference to the belt |
| DOUBLE | time | Defines the time in seconds to stop the belt synchronous movement when error reaction mode of belt is time |
| DOUBLE | decelaration | Defines the deceleration to stop the belt synchronous movement when error reaction mode is desynchronization with limits |
| DOUBLE | jerk | Defines the jerk to stop the belt synchronous movement when error reaction mode is desynchronization with limits |
| MlpiRobotSyncErrorReactionMode | errorType | Type of error reaction |
| MlpiRobotGetBeltErrorReaction |
This structure defines the parameters of the configuration of the error reaction of a belt.
Elements of struct MlpiRobotSetBeltErrorReaction
| Type | Direction | Element | Description |
|---|---|---|---|
| MlpiAxisRef | [in] | belt | Reference to the belt |
| DOUBLE | [out] | time | Defines the time in seconds to stop the belt synchronous movement when error reaction mode of belt is time |
| DOUBLE | [out] | deceleration | Defines the deceleration to stop the belt synchronous movement when error reaction mode is desynchronization with limits |
| DOUBLE | [out] | jerk | Defines the jerk to stop the belt synchronous movement when error reaction mode is desynchronization with limits |
| MlpiRobotSyncErrorReactionMode | [out] | errorType | Type of error reaction |
| MlpiRobotSyncOffWithLimits |
This structure defines the parameters for configuring a desynchronizing movement of a belt with limits.
Elements of struct MlpiRobotSyncOffWithLimits
| Type | Element | Description |
|---|---|---|
| MlpiAxisRef | belt | Reference to the belt |
| DOUBLE | deceleration | Maximum deceleration of movement |
| DOUBLE | jerk | Maximum jerk of movement |
| DOUBLE | blendingRadius | Maximum radius of blending movement |
| MlpiRobotSetMode | setMode | set mode |
| MlpiRobotSyncOnWithLimits |
This structure defines the parameters for configuring a synchronizing movement of a belt with limits.
Elements of struct MlpiRobotSyncOnWithLimits
| Type | Element | Description |
|---|---|---|
| MlpiAxisRef | belt | Reference to the belt |
| DOUBLE | acceleration | Maximum acceleration of movement |
| DOUBLE | jerk | Maximum jerk of movement |
| MlpiRobotSetTrafoParameter |
This structure defines the parameters for configuring a product coordinate system.
Elements of struct MlpiRobotSetTrafoParameter
| Type | Element | Description |
|---|---|---|
| MlpiRobotCoordinateSystem | coordSystem | Reference to the coordinate system |
| DOUBLE | posX | X position of the belt in MCS |
| DOUBLE | posY | Y position of the belt in MCS |
| DOUBLE | posZ | Z position of the belt in MCS |
| DOUBLE | rotA | rotation of belt around x axis in MCS |
| DOUBLE | rotB | rotation of belt around y axis in MCS |
| DOUBLE | rotC | rotation of belt around z axis in MCS |
| MlpiRobotGetTrafoParameter |
This structure defines the parameter of a transformation.
Elements of struct MlpiRobotGetTrafoParameter
| Type | Direction | Element | Description |
|---|---|---|---|
| MlpiRobotCoordinateSystem | [in] | coordSystem | Reference to the coordinate system |
| DOUBLE | [out] | posX | X position of the coordinate system in MCS |
| DOUBLE | [out] | posY | Y position of the coordinate system in MCS |
| DOUBLE | [out] | posZ | Z position of the coordinate system in MCS |
| DOUBLE | [out] | rotA | rotation of the coordinate system around x axis in MCS |
| DOUBLE | [out] | rotB | rotation of the coordinate system around y axis in MCS |
| DOUBLE | [out] | rotC | rotation of the coordinate system around z axis in MCS |
| MlpiRobotCSType | [out] | csType | Type of coordinate system |
| MlpiRobotOpenCyclicChannel |
This structure defines the parameters for opening a cyclic position channel.
Elements of struct MlpiRobotOpenCyclicChannel
| Type | Element | Description |
|---|---|---|
| DOUBLE | deceleration | Maximum deceleration of movement |
| DOUBLE | jerk | Maximum jerk of movement |
| DOUBLE | blendingRadius | Commanded radius of blending movement |
| MlpiRobotSetMode | setMode | set mode |
| MlpiRobotCyclicChannel |
This structure defines the parameters for a cyclic position.
Elements of struct MlpiRobotCyclicChannel
| Type | Element | Description |
|---|---|---|
| MlpiRobotCoordinateSystem | coordSystem | coordinate system |
| MlpiRobotPoint | point | Point of movement |
| MlpiRobotCyclicMode | cyclicMode | Mode of movement |
| MlpiRobotPerformanceResult |
This structure defines the information for a performance measurement.
Elements of struct MlpiRobotPerformanceResult
| Type | Element | Description |
|---|---|---|
| WCHAR16 | name[16] | Name of the performance measurement. |
| LONG | count | Count over recorded measurements. |
| DOUBLE | min | Minimum over all recorded measurements. |
| DOUBLE | max | Maximum over all recorded measurements. |
| DOUBLE | avg | Average over all recorded measurements. |
| MlpiRobotMechanicData |
This structure defines the information about the mechanical structure of a robot.
Elements of struct MlpiRobotMechanicData
| Type | Element | Description |
|---|---|---|
| MlpiRobotMechCmd | cmd | Command for the object. |
| WCHAR16 | object[8] | Object id. |
| DOUBLE | x | x data for the command. |
| DOUBLE | y | y data for the command. |
| DOUBLE | z | z data for the command. |
| MlpiKinematicsValues |
Structure containing operation information about a kinematics. These values do change as soon as the kinematics is in operation. You may want to use this structure to read several sets of kinematics information using one single function call during operation of the kinematics. This provides increased performance in comparison to reading the values bit by bit. Especially when reading the values for multiple kinematics.
Elements of struct MlpiKinematicsValues
| Type | Element | Description |
|---|---|---|
| ULONG | state | Kinematics state of the kinematics. |
| ULONG | stateExtended | Extended kinematics state of the kinematics. |
| ULONG | diagnosisNumber | DiagnosisNumber of the kinematics. |
| FLOAT | actualPosition[MLPI_ROBOT_COORDINATES_IN_POINT] | Actual position of the kinematics. |
| FLOAT | actualVelocity | Actual velocity of the kinematics. |
| FLOAT | actualAcceleration | Actual acceleration of the kinematics. |
| MlpiKinematicsUnits |
Structure containing units of the kinematics as strings. You may want to use this structure to read all units of a kinematics information set using one single function call.
Elements of struct MlpiKinematicsUnits
| Type | Element | Description |
|---|---|---|
| WCHAR16 | position[MLPI_ROBOT_MAX_UNITS_LEN] | Position unit of the kinematics. e.g. 'mm'. |
| WCHAR16 | velocity[MLPI_ROBOT_MAX_UNITS_LEN] | Velocity unit of the kinematics. e.g. 'mm/s'. |
| WCHAR16 | acceleration[MLPI_ROBOT_MAX_UNITS_LEN] | Acceleration unit of the kinematics. e.g. 'mm/s2'. |
| MlpiRobotStop |
This structure defines the parameters for stopping the group.
Elements of struct MlpiRobotStop
| Type | Element | Description |
|---|---|---|
| DOUBLE | deceleration | Maximum deceleration of movement |
| DOUBLE | jerk | Maximum jerk of movement |
| BOOL8 | stop | TRUE: stopping, FALSE: exit stopping mode |
| MlpiRobotInterrupt |
This structure defines the parameters for interrupting the group.
Elements of struct MlpiRobotInterrupt
| Type | Element | Description |
|---|---|---|
| DOUBLE | deceleration | Maximum deceleration of movement |
| DOUBLE | jerk | Maximum jerk of movement |
| MlpiRobotSafeZoneData |
This structure defines the parameters for a save zone.
Elements of struct MlpiRobotSafeZoneData
| Type | Element | Description |
|---|---|---|
| USHORT | zoneNumber | zone number |
| MlpiRobotSafeZoneType | zoneType | zone type |
| DOUBLE | pointPos[MLPI_ROBOT_MAX_POS_AXIS] | minimum position of zone |
| DOUBLE | pointNeg[MLPI_ROBOT_MAX_POS_AXIS] | maximum position of zone |
| MlpiRobotJogStepData |
This structure defines the parameters of a jog step movement.
Elements of struct MlpiRobotJogStepData
| Type | Element | Description |
|---|---|---|
| MlpiRobotPoint | distance | Distance of movement |
| DOUBLE | velocity | Maximum velocity of movement |
| DOUBLE | acceleration | Maximum acceleration of movement |
| DOUBLE | deceleration | Maximum deceleration of movement |
| DOUBLE | jerk | Maximum jerk of movement |
| MlpiRobotCoordinateSystem | coordSystem | coordinate system |
| MlpiRobotJogContData |
This structure defines the parameters of a continuous jog movement.
Elements of struct MlpiRobotJogContData
| Type | Element | Description |
|---|---|---|
| MlpiRobotPoint | direction | Direction of movement |
| DOUBLE | velocity | Maximum velocity of movement |
| DOUBLE | acceleration | Maximum acceleration of movement |
| DOUBLE | deceleration | Maximum deceleration of movement |
| DOUBLE | jerk | Maximum jerk of movement |
| MlpiRobotCoordinateSystem | coordSystem | coordinate system |
| MlpiRobotStopCmdData |
This structure defines the parameters of a stop command.
Elements of struct MlpiRobotStopCmdData
| Type | Element | Description |
|---|---|---|
| MLPIMOTIONHANDLE | cmdID | ID of the command that will be stopped |
| MlpiRobotBeltDesyncRelData |
This structure defines the parameters of a relative desynchronization configuration.
Elements of struct MlpiRobotBeltDesyncRelData
| Type | Element | Description |
|---|---|---|
| MlpiAxisRef | belt | Reference to the axis |
| DOUBLE | startPercent | percentage of start relative desynchronization |
| DOUBLE | endPercent | percentage of end relative desynchronization |
| MlpiRobotTeachInDataWrite |
This structure defines the parameters of the TeachInWrite command.
Elements of struct MlpiRobotTeachInDataWrite
| Type | Element | Description |
|---|---|---|
| WCHAR16 | pointName[MLPI_ROBOT_MAX_TEACH_NAME_LEN] | Name of the point that will be saved |
| MlpiRobotPoint | teachPoint | Point that will be saved |
| MlpiRobotCoordinateSystem | coordSys | Coordinate system of the point |
| USHORT | options | Option, what will be written and how |
| MlpiRobotTeachInDataRead |
This structure defines the parameters of the TeachInRead command.
Elements of struct MlpiRobotTeachInDataRead
| Type | Direction | Element | Description |
|---|---|---|---|
| WCHAR16 | [in] | pointName[MLPI_ROBOT_MAX_TEACH_NAME_LEN] | Name of the point that will be loaded |
| MlpiRobotPoint | [out] | teachPoint | Point that will be returned |
| MlpiRobotCoordinateSystem | [out] | coordSys | Coordinate system of the point |
| MlpiRobotTeachInDataReadNext |
This structure defines the parameters of the TeachInDataReadNext command.
Elements of struct MlpiRobotTeachInDataReadNext
| Type | Direction | Element | Description |
|---|---|---|---|
| WCHAR16 | [in] | pointNameInput[MLPI_ROBOT_MAX_TEACH_NAME_LEN] | Name of the current point |
| WCHAR16 | [out] | pointNameOutput[MLPI_ROBOT_MAX_TEACH_NAME_LEN] | Name of the next point after current |
| MlpiRobotPoint | [out] | teachPoint | Point that will be saved |
| MlpiRobotCoordinateSystem | [out] | coordSys | Coordinate system of the point |
| MlpiRobotTeachInDataDeletePoints |
This structure defines the parameters of the TeachInDataDeletePoints command.
Elements of struct MlpiRobotTeachInDataDeletePoints
| Type | Element | Description |
|---|---|---|
| WCHAR16 | pointName[MLPI_ROBOT_MAX_TEACH_NAME_LEN] | Name of the point that will be deleted |
| MlpiRobotTeachInDataFileData |
This structure defines the parameters of the TeachInDataFileData command.
Elements of struct MlpiRobotTeachInDataFileData
| Type | Element | Description |
|---|---|---|
| WCHAR16 | fileName[MLPI_ROBOT_MAX_TEACH_NAME_LEN] | Name of the file that will be saved or loaded |
| MlpiRobotTeachInPointFileOption | fileOptions | Option, how the loading or writing will happen |
| MlpiRobotTeachInDataDeleteFileData |
This structure defines the parameters of the TeachInDataFileData command.
Elements of struct MlpiRobotTeachInDataDeleteFileData
| Type | Element | Description |
|---|---|---|
| WCHAR16 | fileName[MLPI_ROBOT_MAX_TEACH_NAME_LEN] | Name of the file that will be deleted |
| MlpiRobotGetStatusSummary |
This structure defines the parameters of the GetStatusSummary command.
Elements of struct MlpiRobotGetStatusSummary
| Type | Direction | Element | Description |
|---|---|---|---|
| MlpiGroupRef | [in] | group | Reference to the group. |
| ULONG | [in] | coordSys | Coordinate System. |
| ULONG | [out] | state | Kinematics state |
| ULONG | [out] | stateExtended | Extended kinematics state |
| ULONG | [out] | diagnosisNumber | Diagnosis number of the kinematics. |
| USHORT | [out] | dimension | Dimension of a point of the kinematics |
| MlpiRobotPoint | [out] | actualPosition | Actual position of the kinematics. |
| WCHAR16[MLPI_ROBOT_MAX_UNITS_LEN] | [out] | actualPosUnit | Unit of actual position. |
| FLOAT | [out] | actualVelocity | Actual velocity of the kinematics. |
| FLOAT | [out] | actualAcceleration | Actual acceleration of the kinematics. |
| FLOAT | [out] | actualJerk | Actual jerk of the kinematics. |
| WCHAR16[MLPI_ROBOT_MAX_UNIT_LEN] | [out] | pathUnits | Unit of Vel, Acc and Jrk. |
| WCHAR16[MLPI_ROBOT_MAX_UNIT_LEN] | [out] | timeBase | Unit of time. |
| MlpiRobotCoordinateSystemInfo |
This structure defines the parameters of the GetCSInfo command.
Elements of struct MlpiRobotCoordinateSystemInfo
| Type | Element | Description |
|---|---|---|
| ULONG | cs | Reference to the coordinate system. |
| USHORT | dimension | Dimension of a point of the kinematics. |
| WCHAR16[MLPI_ROBOT_MAX_CSNAME_LEN] | name | Name of the kinematics. |
| WCHAR16[MLPI_ROBOT_MAX_UNITS_LEN] | posunits | Unit of Vel, Acc and Jrk. |
| MlpiRobotCmdInfo |
This structure defines the information about the mechanical structure of a robot.
Elements of struct MlpiRobotCmdInfo
| Type | Element | Description |
|---|---|---|
| ULONG | commandID | ID of the command. |
| MlpiRobotCmdInfoType | type | Type of given information. |
| DOUBLE | value | Value of the information. |
| MlpiRobotChangeToolParameter |
This structure defines the information for a tool change command.
Elements of struct MlpiRobotChangeToolParameter
| Type | Element | Description |
|---|---|---|
| DOUBLE | posX | X position of the PCS in MCS. |
| DOUBLE | posY | Y position of the PCS in MCS. |
| DOUBLE | posZ | Z position of the PCS in MCS. |
| DOUBLE | rotA | rotation of PCS around x axis in MCS. |
| DOUBLE | rotB | rotation of PCS around y axis in MCS. |
| DOUBLE | rotC | rotation of PCS around z axis in MCS. |
| enum MlpiRobotAxisTypes |
This enumeration defines the types of axes used in a robot. This is parameter K-0-0008.
Definition at line 334 of file mlpiRobotLib.h.
| enum MlpiRobotSetMode |
This enumeration defines the set mode of movement commands.
| Enumerator | |
|---|---|
| MLPI_ROBOT_SETMODE_TO |
no blending |
| MLPI_ROBOT_SETMODE_VIA |
blending |
Definition at line 343 of file mlpiRobotLib.h.
This enumeration defines coordinate systems of a robot.
Definition at line 350 of file mlpiRobotLib.h.
| enum MlpiRobotCSType |
This enumeration defines the type of the coordinate system.
| Enumerator | |
|---|---|
| MLPI_ROBOT_CARTESIAN |
cartesian coordinate system |
| MLPI_ROBOT_CYLINDRIC |
cylindric coordinate system |
Definition at line 375 of file mlpiRobotLib.h.
| enum MlpiRobotPointType |
This enumeration defines the point type.
| Enumerator | |
|---|---|
| MLPI_ROBOT_POINT_TYPE_PREP |
position of preparation |
| MLPI_ROBOT_POINT_TYPE_EXEC |
position of execution |
Definition at line 384 of file mlpiRobotLib.h.
| enum MlpiRobotSlopeType |
This enumeration defines the slope types of movement commands.
Definition at line 392 of file mlpiRobotLib.h.
This enumeration defines the error reaction mode of a belt.
Definition at line 400 of file mlpiRobotLib.h.
| enum MlpiRobotCyclicMode |
This enum defines the type of a cyclic position command.
| Enumerator | |
|---|---|
| MLPI_ROBOT_CYCLIC_MODE_POS_ABS |
Absolute position. |
| MLPI_ROBOT_CYCLIC_MODE_POS_REL |
Relative position delta to last position. |
| MLPI_ROBOT_CYCLIC_MODE_VEL |
Velocity in robot units. |
Definition at line 408 of file mlpiRobotLib.h.
| enum MlpiRobotMechCmd |
This enum defines the command for a mechanical object.
Definition at line 416 of file mlpiRobotLib.h.
This enum defines the type of a save zone.
Definition at line 429 of file mlpiRobotLib.h.
This enum defines the possible options for writing a point while the TeachIn functions.
Definition at line 437 of file mlpiRobotLib.h.
This enum defines the options, how a file can be loaded or saved.
Definition at line 445 of file mlpiRobotLib.h.
| enum MlpiRobotCmdInfoType |
This enum defines the type of information which should be read.
Definition at line 453 of file mlpiRobotLib.h.