|
Typedefs | |
| typedef unsigned long long | MLPIMOTIONHANDLE |
| typedef struct MlpiAxisRef | MlpiAxisRef |
| typedef struct MlpiGroupRef | MlpiGroupRef |
| typedef struct MlpiMotionStatus | MlpiMotionStatus |
| typedef struct MlpiAxisInformation | MlpiAxisInformation |
| typedef struct MlpiAxisValues | MlpiAxisValues |
| typedef struct MlpiAxisUnits | MlpiAxisUnits |
| typedef struct MlpiAxisStatus | MlpiAxisStatus |
| typedef struct MlpiMotionStop | MlpiMotionStop |
| typedef struct MlpiMotionPower | MlpiMotionPower |
| typedef struct MlpiMotionGearIn | MlpiMotionGearIn |
| typedef struct MlpiMotionGearInPos | MlpiMotionGearInPos |
| typedef struct MlpiMotionCamIn | MlpiMotionCamIn |
| typedef struct MlpiMotionMotionProfile | MlpiMotionMotionProfile |
| typedef struct MlpiMotionFlexProfileStep | MlpiMotionFlexProfileStep |
| typedef struct MlpiMotionFlexProfile | MlpiMotionFlexProfile |
| typedef struct MlpiMotionMoveVelocity | MlpiMotionMoveVelocity |
| typedef struct MlpiMotionPhasing | MlpiMotionPhasing |
| typedef struct MlpiMotionMoveAbsolute | MlpiMotionMoveAbsolute |
| typedef struct MlpiMotionMoveContinuousAbsolute | MlpiMotionMoveContinuousAbsolute |
| typedef struct MlpiMotionMoveContinuousRelative | MlpiMotionMoveContinuousRelative |
| typedef struct MlpiMotionMoveRelative | MlpiMotionMoveRelative |
| typedef struct MlpiMotionMoveAdditive | MlpiMotionMoveAdditive |
| typedef struct MlpiMotionAdminAxisGroup | MlpiMotionAdminAxisGroup |
| typedef struct MlpiMotionTorqueControl | MlpiMotionTorqueControl |
| typedef struct MlpiMotionCyclic | MlpiMotionCyclic |
Enumerations |
List of used types, enumerations, structures and more...
| typedef unsigned long long MLPIMOTIONHANDLE |
MLPI-API handle value used for motion functions.
Definition at line 615 of file mlpiMotionLib.h.
| MlpiAxisRef |
This structure defines the axis through the definition of control and axis number.
Elements of struct MlpiAxisRef
| Type | Element | Description |
|---|---|---|
| MlpiControl | controlNo | Addressed control. |
| MlpiAxisNumber | axisNo | Addressed axis. |
| MlpiGroupRef |
This structure defines the group through the definition of control and group number.
Elements of struct MlpiGroupRef
| Type | Element | Description |
|---|---|---|
| MlpiControl | controlNo | Addressed control. |
| MlpiGroupNumber | groupNo | Addressed group. |
| MlpiMotionStatus |
This structure defines the status of a motion command.
Elements of struct MlpiMotionStatus
| Type | Element | Description |
|---|---|---|
| BOOL8 | done | TRUE when command is completed. |
| BOOL8 | active | TRUE as long as command is active. |
| BOOL8 | aborted | TRUE when command has been aborted by another command. |
| BOOL8 | error | TRUE when motion command issued an error. |
| USHORT | errorID | Short description of error. |
| USHORT | table | Additional description of error. |
| ULONG | additional1 | Additional diagnosis number1. |
| ULONG | additional2 | Additional diagnosis number2. |
| MlpiAxisInformation |
Structure containing parametric information about an axis. These values no longer change, once the axis is in operation mode.
Elements of struct MlpiAxisInformation
| Type | Element | Description |
|---|---|---|
| MlpiAxisRef | axis | Logical axis address. |
| ULONG | deviceAddress | (SERCOS) device address. |
| MlpiAxisType | axisType | Type of axis (virtual, real, etc...). |
| WCHAR16 | name | The axis name. |
| MlpiAxisValues |
Structure containing operation information about an axis. These values do change as soon as the axis is in operation. You may want to use this structure to read several sets of axis information using one single function call during operation of the axis. This gives increased performance in comparison to reading the values bit by bit. Especially when reading the values for multiple axes.
Elements of struct MlpiAxisValues
| Type | Direction | Element | Description |
|---|---|---|---|
| MlpiAxisRef | [in] | axis | Logical axis address. |
| DOUBLE | [out] | actualPosition | Actual position of the axis. See mlpiMotionGetActualPosition. |
| DOUBLE | [out] | actualVelocity | Actual velocity of the axis. See mlpiMotionGetActualVelocity. |
| DOUBLE | [out] | actualAcceleration | Actual acceleration of the axis. See mlpiMotionGetActualAcceleration. |
| DOUBLE | [out] | actualTorque | Actual torque of the axis. See mlpiMotionGetActualTorque. |
| ULONG | [out] | state | Axis state of the axis. See mlpiMotionGetState. |
| ULONG | [out] | stateExtended | Extended axis state of the axis. See mlpiMotionGetStateExtended. |
| ULONG | [out] | diagnosisNumber | Current diagnosis number of the axis. See mlpiMotionGetDiagnosisNumber. |
| ULONG | [out] | condition | Condition of the axis. See mlpiMotionGetCondition. |
| MlpiAxisUnits |
Structure containing units of the axis as strings. You may want to use this structure to read all units of an axis information set using one single function call.
Elements of struct MlpiAxisUnits
| Type | Direction | Element | Description |
|---|---|---|---|
| MlpiAxisRef | [in] | axis | Logical axis address. |
| WCHAR16 | [out] | position | Position unit of the axis. e.g. 'Degree'. |
| WCHAR16 | [out] | velocity | Velocity unit of the axis. e.g. 'Rpm'. |
| WCHAR16 | [out] | acceleration | Acceleration unit of the axis. e.g. 'rad/sec'. |
| WCHAR16 | [out] | jerk | Jerk unit of the axis. e.g. 'rad/sec^2'. |
| WCHAR16 | [out] | torque | Torque unit of the axis. e.g. 'Nm'. |
| MlpiAxisStatus |
Structure containing status information about an axis. These values do change as soon as the axis is in operation. You may want to use this structure to read several sets of axis status information using one single function call during operation of the axis.
Elements of struct MlpiAxisStatus
| Type | Direction | Element | Description |
|---|---|---|---|
| MlpiAxisRef | [in] | axis | Logical axis address. |
| ULLONG | [out] | state | Axis state of the axis. See mlpiMotionGetState. |
| ULONG | [out] | stateExtended | Extended axis state of the axis. See mlpiMotionGetStateExtended. |
| ULONG | [out] | diagnosisNumber | Current diagnosis number of the axis. See mlpiMotionGetDiagnosisNumber. |
| ULONG | [out] | condition | Condition of the axis. See mlpiMotionGetCondition. |
| MlpiMotionStop |
Structure to command stop to an axis.
Elements of struct MlpiMotionStop
| Type | Element | Description |
|---|---|---|
| MlpiAxisRef | axis | Reference to the axis. |
| DOUBLE | deceleration | Deceleration in drives unit. |
| DOUBLE | jerk | Jerk in drives unit. |
| BOOL8 | stop | 1: stopping, 0: exit Stopping mode. Important Note: This command is special in the way that it has to be called once with 'stop' = TRUE. This will bring the axis to a standstill. Once the axis is standing still, the command has to be called again with 'stop' = FALSE in order to enter the PLCopen 'Stand Still' mode. |
| MlpiMotionPower |
Structure to command power to an axis.
Elements of struct MlpiMotionPower
| Type | Element | Description |
|---|---|---|
| MlpiAxisRef | axis | Reference to the axis. |
| BOOL8 | power | 1: Power on, 0: Power off. |
| MlpiMotionGearIn |
This structure defines a velocity synchronization of the slave to the master using a gear and fine adjust.
Elements of struct MlpiMotionGearIn
| Type | Element | Description |
|---|---|---|
| MlpiAxisRef | axis | Reference to the slave axis. |
| ULONG | numerator | Gear ratio numerator. |
| ULONG | denominator | Gear ratio denominator. |
| DOUBLE | fineadjust | Fine adjust for gear in %. |
| MlpiAxisRef | master | Reference to the master axis. |
| MlpiMotionGearInPos |
This structure defines a position synchronization of the slave to the master using a gear and fine adjust.
Elements of struct MlpiMotionGearInPos
| Type | Element | Description |
|---|---|---|
| MlpiAxisRef | axis | Reference to the slave axis. |
| ULONG | numerator | Gear ratio numerator. |
| ULONG | denominator | Gear ratio denominator. |
| DOUBLE | fineadjust | Fine adjust for gear in %. |
| MlpiStartMode | startMode | Synchronization mode. |
| MlpiSyncDirection | syncMode | Synchronization direction. |
| MlpiAxisRef | master | Reference to the master axis. |
| MlpiMotionCamIn |
This structure defines a position synchronization of the slave to the master using gear, fine adjust and a cam table.
Elements of struct MlpiMotionCamIn
| Type | Element | Description |
|---|---|---|
| MlpiAxisRef | axis | Reference to the slave axis. |
| ULONG | numerator | Gear ratio numerator. |
| ULONG | denominator | Gear ratio denominator. |
| DOUBLE | fineadjust | Fine adjust for gear in %. |
| DOUBLE | camShaftDistance | Cam shaft distance in slave units. |
| MlpiStartMode | startMode | Synchronization mode. |
| MlpiSyncDirection | syncMode | Synchronization direction. |
| MlpiCamTableId | camTable | ID of the Cam table to be used. |
| MlpiAxisRef | master | Reference to the master axis. |
| MlpiMotionMotionProfile |
This structure defines a position synchronization of the slave to the master using gear, fine adjust and a motion profile. This command can only be used on IndraDrives with interpolation in the drive.
Elements of struct MlpiMotionMotionProfile
| Type | Element | Description |
|---|---|---|
| MlpiAxisRef | axis | Reference to the slave axis. |
| ULONG | numerator | Gear ratio numerator. |
| ULONG | denominator | Gear ratio denominator. |
| DOUBLE | fineadjust | Fine adjust for gear in %. |
| BOOL8 | relativePositioning | Determines if offset angle of the parameter A-0-2901 should be active. |
| MlpiProfileSetSelection | setSelection | Selects the active set. |
| MlpiStartMode | startMode | Synchronization mode. |
| MlpiSyncDirection | syncMode | Synchronization direction. |
| MlpiAxisRef | master | Reference to the master axis. |
| MlpiMotionFlexProfileStep |
This struct defines a single step of a FlexProfile. Use multiple steps to create a profile.
Elements of struct MlpiMotionFlexProfileStep
| Type | Element | Description |
|---|---|---|
| MlpiProfileMasterType | master | Definition of master type. |
| DOUBLE | camShaftDistance | Cam shaft distance (Hub). |
| DOUBLE | range | Definition of master range. |
| MlpiLawType | motionLaw | Definition of motion law. |
| MlpiProfileStepType | stepType | Segment type: relation between master and slave. |
| DOUBLE | startVel | Slave axis starting velocity. |
| DOUBLE | startAcc | Slave axis starting acceleration. |
| DOUBLE | startJrk | Slave axis starting jerk. |
| DOUBLE | endVel | Slave axis ending velocity. |
| DOUBLE | endAcc | Slave axis ending acceleration. |
| DOUBLE | endJrk | Slave axis ending jerk. |
| DOUBLE | travelVel | Slave axis velocity during move (not implemented for all motion laws). |
| DOUBLE | limitAcc | Slave axis acceleration during move (not implemented for all motion laws). |
| DOUBLE | limitJrk | Slave axis jerk during move (not implemented for all motion laws). |
| DOUBLE | turningPointDisplacement | Displacement of point of inflection. |
| MlpiMotionFlexProfile |
This structure defines a position synchronization of the slave to the master using gear, fine adjust and a flex profile. This command can only be used on IndraDrives with interpolation in the control.
Elements of struct MlpiMotionFlexProfile
| Type | Element | Description |
|---|---|---|
| MlpiAxisRef | axis | Reference to the slave axis. |
| ULONG | numerator | Gear ratio numerator. |
| ULONG | denominator | Gear ratio denominator. |
| DOUBLE | fineadjust | Fine adjust for gear in %. |
| MlpiProfileSetSelection | setSelection | Selects the active set |
| BOOL8 | useSwitchingPositioning | Determines whether switching position will be used. |
| DOUBLE | switchingPosition | Switching position. |
| MlpiProfileStartPoint | profileEntry | Switching conditions. |
| DOUBLE | masterOffset | Master offset. |
| DOUBLE | slaveOffset | Slave offset. |
| MlpiSyncType | syncType | Synchronization type. |
| DOUBLE | syncVelocity | Synchronization velocity. |
| DOUBLE | syncAcceleration | Synchronization acceleration. |
| MlpiProfileExecutionMode | executionMode | Execution mode. |
| MlpiAxisRef | master | Reference to the master axis. |
| MlpiMotionMoveVelocity |
This structure defines a velocity move of a single axis.
Elements of struct MlpiMotionMoveVelocity
| Type | Element | Description |
|---|---|---|
| MlpiAxisRef | axis | Reference to the slave axis. |
| DOUBLE | velocity | Velocity in drives unit. |
| DOUBLE | acceleration | Acceleration in drives unit. |
| DOUBLE | deceleration | Deceleration in drives unit. |
| DOUBLE | jerk | Jerk in drives unit. |
| MlpiMotionPhasing |
This structure defines a phase shift of a slave axis that can either be applied to the master position of that slave or to the gear/cam/flex profile/motion profile.
Elements of struct MlpiMotionPhasing
| Type | Element | Description |
|---|---|---|
| MlpiAxisRef | axis | Reference to the slave axis. |
| DOUBLE | phaseShift | Phase shift in drives unit (master or slave). |
| DOUBLE | velocity | Velocity in drives unit. |
| DOUBLE | acceleration | Acceleration in drives unit. |
| DOUBLE | deceleration | Deceleration in drives unit. |
| MlpiMotionMoveAbsolute |
This structure defines an absolute position move of a single axis.
Elements of struct MlpiMotionMoveAbsolute
| Type | Element | Description |
|---|---|---|
| MlpiAxisRef | axis | Reference to the slave axis. |
| DOUBLE | position | Target position in drives unit. |
| DOUBLE | velocity | Velocity in drives unit. |
| DOUBLE | acceleration | Acceleration in drives unit. |
| DOUBLE | deceleration | Deceleration in drives unit. |
| DOUBLE | jerk | Jerk in drives unit. |
| MlpiMotionMoveContinuousAbsolute |
This structure defines a continuous absolute move of a single axis.
Elements of struct MlpiMotionMoveContinuousAbsolute
| Type | Element | Description |
|---|---|---|
| MlpiAxisRef | axis | Reference to the slave axis. |
| DOUBLE | position | Target position in drives unit. |
| DOUBLE | endVelocity | End Velocity in drives unit. |
| DOUBLE | velocity | Velocity in drives unit. |
| DOUBLE | acceleration | Acceleration in drives unit. |
| DOUBLE | deceleration | Deceleration in drives unit. |
| DOUBLE | jerk | Jerk in drives unit. |
| MlpiMotionMoveContinuousRelative |
This structure defines a continuous relative move of a single axis.
Elements of struct MlpiMotionMoveContinuousRelative
| Type | Element | Description |
|---|---|---|
| MlpiAxisRef | axis | Reference to the slave axis. |
| DOUBLE | distance | Distance in drives unit. |
| DOUBLE | endVelocity | End Velocity in drives unit. |
| DOUBLE | velocity | Velocity in drives unit. |
| DOUBLE | acceleration | Acceleration in drives unit. |
| DOUBLE | deceleration | Deceleration in drives unit. |
| DOUBLE | jerk | Jerk in drives unit. |
| MlpiMotionMoveRelative |
This structure defines a relative position move of a single axis.
Elements of struct MlpiMotionMoveRelative
| Type | Element | Description |
|---|---|---|
| MlpiAxisRef | axis | Reference to the slave axis. |
| DOUBLE | distance | Distance in drives unit. |
| DOUBLE | velocity | Velocity in drives unit. |
| DOUBLE | acceleration | Acceleration in drives unit. |
| DOUBLE | deceleration | Deceleration in drives unit. |
| DOUBLE | jerk | Jerk in drives unit. |
| MlpiMotionMoveAdditive |
This structure defines an additive position move of a single axis.
Elements of struct MlpiMotionMoveAdditive
| Type | Element | Description |
|---|---|---|
| MlpiAxisRef | axis | Reference to the slave axis. |
| DOUBLE | distance | Distance in drives unit (is added to the target position). |
| DOUBLE | velocity | Velocity in drives unit. |
| DOUBLE | acceleration | Acceleration in drives unit. |
| DOUBLE | deceleration | Deceleration in drives unit. |
| DOUBLE | jerk | Jerk in drives unit. |
| MlpiMotionAdminAxisGroup |
This structure defines information for adding and removing an axis to or from a group.
Elements of struct MlpiMotionAdminAxisGroup
| Type | Element | Description |
|---|---|---|
| MlpiAxisRef | axis | Axis to add to the group. |
| MlpiGroupRef | group | Group to add the axis. |
| MlpiMotionTorqueControl |
Structure to command torque to an axis.
Elements of struct MlpiMotionTorqueControl
| Type | Element | Description |
|---|---|---|
| MlpiAxisRef | axis | Reference to the axis. |
| DOUBLE | torque | Torque in drives unit. |
| DOUBLE | torqueRamp | TorqueRamp in drives unit. |
| MlpiMotionCyclic |
This structure is used when operating the axis in cyclic position command mode. A cyclic value (position or velocity) must be updated every sercos cycle.
Elements of struct MlpiMotionCyclic
| Type | Element | Description |
|---|---|---|
| MlpiAxisRef | axis | Reference to the axis. |
| DOUBLE | cyclicValue | Cyclic value (position, velocity, ...). |
| enum MlpiAxisType |
This enumeration defines the type of axis.
Definition at line 625 of file mlpiMotionLib.h.
The motion profile or flex profile works based on a set of parameters. In order to change a set consistently, the set that is not in use should be changed. Once the change is done, the set can be verified and then used.
| Enumerator | |
|---|---|
| MLPI_PROFILE_SET_0 |
Set 0 on axis. |
| MLPI_PROFILE_SET_1 |
Set 1 on axis. |
| MLPI_PROFILE_SET_2 |
Set 2 on axis. |
| MLPI_PROFILE_SET_3 |
Set 3 on axis. |
Definition at line 638 of file mlpiMotionLib.h.
| enum MlpiSyncDirection |
This enumeration defines the direction in which synchronization takes place.
Definition at line 648 of file mlpiMotionLib.h.
| enum MlpiSyncType |
This enumeration defines the direction and type in which synchronization takes place. Only for FlexProfile!
Definition at line 657 of file mlpiMotionLib.h.
| enum MlpiStartMode |
This enumeration defines how the synchronization is done.
Definition at line 667 of file mlpiMotionLib.h.
This enumeration defines the method of how a flex profile interprets the start point.
Definition at line 677 of file mlpiMotionLib.h.
| enum MlpiProfileStepType |
This enumeration defines the relation between master and slave for each flex profile step.
Definition at line 688 of file mlpiMotionLib.h.
This enumeration defines how the flex profile is executed.
| Enumerator | |
|---|---|
| MLPI_EXECUTE_CYCLIC |
Cyclic execution. |
| MLPI_EXECUTE_SINGLE |
Single execution. When the profile is finished, the axis will continue to run with end velocity of the profile. |
Definition at line 699 of file mlpiMotionLib.h.
Enumeration for Flex profile master definition.
| Enumerator | |
|---|---|
| MLPI_MASTER_TIME |
Master is time-based. |
| MLPI_MASTER_AXIS0 |
Master is position-based. |
Definition at line 707 of file mlpiMotionLib.h.
| enum MlpiCamTableId |
This enumeration defines the available cam numbers. The cams actually available depend on the hardware used.
Definition at line 715 of file mlpiMotionLib.h.
| enum MlpiLawType |
Enumeration for Flex profile motion laws for segments.
Definition at line 821 of file mlpiMotionLib.h.
| enum MlpiControl |
This enumeration defines the control that should be addressed.
Definition at line 972 of file mlpiMotionLib.h.
| enum MlpiAxisNumber |
This enumeration defines the available axis numbers.
Definition at line 1078 of file mlpiMotionLib.h.
| enum MlpiGroupNumber |
This enumeration defines the available kinematics group numbers.
Definition at line 1184 of file mlpiMotionLib.h.