Open Core Interface - MLPI
MLPI-MotionLogicProgrammingInterface(mlpi4LabVIEW)  1.26.2
Read memory area
Collaboration diagram for Read memory area:

Functions

MLPIRESULT mlpiLogicReadMemoryAreaBool8 (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG bitOffset, BOOL8 *data)
 
MLPIRESULT mlpiLogicReadMemoryAreaChar (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, CHAR *data)
 
MLPIRESULT mlpiLogicReadMemoryAreaUchar (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, UCHAR *data)
 
MLPIRESULT mlpiLogicReadMemoryAreaShort (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, SHORT *data)
 
MLPIRESULT mlpiLogicReadMemoryAreaUshort (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, USHORT *data)
 
MLPIRESULT mlpiLogicReadMemoryAreaLong (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, LONG *data)
 
MLPIRESULT mlpiLogicReadMemoryAreaUlong (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, ULONG *data)
 
MLPIRESULT mlpiLogicReadMemoryAreaLlong (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, LLONG *data)
 
MLPIRESULT mlpiLogicReadMemoryAreaUllong (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, ULLONG *data)
 
MLPIRESULT mlpiLogicReadMemoryAreaFloat (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, FLOAT *data)
 
MLPIRESULT mlpiLogicReadMemoryAreaDouble (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, DOUBLE *data)
 
MLPIRESULT mlpiLogicReadMemoryAreaArrayChar (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, CHAR *data, const ULONG numElements, ULONG *numElementsRet)
 
MLPIRESULT mlpiLogicReadMemoryAreaArrayUchar (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, UCHAR *data, const ULONG numElements, ULONG *numElementsRet)
 
MLPIRESULT mlpiLogicReadMemoryAreaArrayShort (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, SHORT *data, const ULONG numElements, ULONG *numElementsRet)
 
MLPIRESULT mlpiLogicReadMemoryAreaArrayUshort (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, USHORT *data, const ULONG numElements, ULONG *numElementsRet)
 
MLPIRESULT mlpiLogicReadMemoryAreaArrayLong (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, LONG *data, const ULONG numElements, ULONG *numElementsRet)
 
MLPIRESULT mlpiLogicReadMemoryAreaArrayUlong (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, ULONG *data, const ULONG numElements, ULONG *numElementsRet)
 
MLPIRESULT mlpiLogicReadMemoryAreaArrayLlong (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, LLONG *data, const ULONG numElements, ULONG *numElementsRet)
 
MLPIRESULT mlpiLogicReadMemoryAreaArrayUllong (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, ULLONG *data, const ULONG numElements, ULONG *numElementsRet)
 
MLPIRESULT mlpiLogicReadMemoryAreaArrayFloat (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, FLOAT *data, const ULONG numElements, ULONG *numElementsRet)
 
MLPIRESULT mlpiLogicReadMemoryAreaArrayDouble (const MLPIHANDLE connection, const WCHAR16 *application, const MlpiApplicationMemoryArea area, const ULONG byteOffset, DOUBLE *data, const ULONG numElements, ULONG *numElementsRet)
 

Detailed Description

These functions read the following memory areas: "%Ix" (Input), "%Qx" (Output) and "%Mx" (Marker)

The table shows the PLC data types within the IEC61131 environment 'IndraLogic' and the corresponding data types within the C/C++ environment (e.g. 'Workbench OEM') of the MLPI. On reading from memory areas, on default, you use the functions below named after the MLPI data type like mlpiLogicReadMemoryAreaShort. If you include the header mlpiLogicHelper.h, you can also use the equivalent functions named after the IEC61131 data types like mlpiLogicReadMemoryAreaWord or like mlpiLogicReadMemoryAreaInt.

Note
Reading on outputs and writing on inputs is not supported yet.
Number of Bits Data types of PLC Data types of MLPI
8 BOOL BOOL8
8 SINT CHAR
16 INT SHORT
32 DINT LONG
64 LINT LLONG
8 USINT UCHAR
16 UINT USHORT
32 UDINT ULONG
64 ULINT ULLONG
8 BYTE UCHAR
16 WORD USHORT
32 DWORD ULONG
64 LWORD ULLONG
32 REAL FLOAT
64 LREAL DOUBLE
8n STRING WCHAR16
16n WSTRING WCHAR16

Function Documentation

MLPIRESULT mlpiLogicReadMemoryAreaBool8 ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  bitOffset,
BOOL8 *  data 
)

This function reads a bit as a BOOL8 (BOOL8, MlpiLogicType) from the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]bitOffsetBit offset based on zero (e.g. IX0.0).
[out]dataPointer to variable where the value will be stored.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Read the data value from the memory area %IX1.5.
2 BOOL8 data = FALSE;
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicReadMemoryAreaBool8(connection, application, MLPI_MEMORY_AREA_INPUT, 13, &data);
MLPIRESULT mlpiLogicReadMemoryAreaChar ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
CHAR *  data 
)

This function reads the 8-bit signed data value (SINT, MlpiLogicType) from the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. IB0).
[out]dataPointer to variable where the value will be stored.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Read the data value from the memory area %IB42.
2 CHAR data = 0;
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicReadMemoryAreaChar(connection, application, MLPI_MEMORY_AREA_INPUT, 42, &data);
MLPIRESULT mlpiLogicReadMemoryAreaUchar ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
UCHAR *  data 
)

This function reads the 8-bit unsigned data value (BYTE, USINT, MlpiLogicType) from the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. IB0).
[out]dataPointer to variable where the value will be stored.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Read the data value from the memory area %IB42.
2 UCHAR data = 0;
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicReadMemoryAreaUchar(connection, application, MLPI_MEMORY_AREA_INPUT, 42, &data);
MLPIRESULT mlpiLogicReadMemoryAreaShort ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
SHORT *  data 
)

This function reads the 16-bit signed data value (INT, MlpiLogicType) from the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. IB0).
[out]dataPointer to variable where the value will be stored.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Read the data value from the memory area %IW42.
2 SHORT data = 0;
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicReadMemoryAreaShort(connection, application, MLPI_MEMORY_AREA_INPUT, 42, &data);
MLPIRESULT mlpiLogicReadMemoryAreaUshort ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
USHORT *  data 
)

This function reads the 16-bit unsigned data value (WORD, UINT, MlpiLogicType) from the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. IB0).
[out]dataPointer to variable where the value will be stored.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Read the data value from the memory area %IW42.
2 USHORT data = 0;
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicReadMemoryAreaUshort(connection, application, MLPI_MEMORY_AREA_INPUT, 42, &data);
MLPIRESULT mlpiLogicReadMemoryAreaLong ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
LONG *  data 
)

This function reads the 32-bit signed data value (DINT, MlpiLogicType) from the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. IB0).
[out]dataPointer to variable where the value will be stored.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Read the data value from the memory area %ID42.
2 LONG data = 0;
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicReadMemoryAreaLong(connection, application, MLPI_MEMORY_AREA_INPUT, 42, &data);
MLPIRESULT mlpiLogicReadMemoryAreaUlong ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
ULONG *  data 
)

This function reads the 32-bit unsigned data value (DWORD, UDINT, MlpiLogicType) from the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. IB0).
[out]dataPointer to variable where the value will be stored.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Read the data value from the memory area %ID42.
2 ULONG data = 0;
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicReadMemoryAreaUlong(connection, application, MLPI_MEMORY_AREA_INPUT, 42, &data);
MLPIRESULT mlpiLogicReadMemoryAreaLlong ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
LLONG *  data 
)

This function reads the 64-bit signed data value (LINT, MlpiLogicType) from the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. IB0).
[out]dataPointer to variable where the value will be stored.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Read the data value from the memory area %IL42.
2 LLONG data = 0;
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicReadMemoryAreaLlong(connection, application, MLPI_MEMORY_AREA_INPUT, 42, &data);
MLPIRESULT mlpiLogicReadMemoryAreaUllong ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
ULLONG *  data 
)

This function reads the 64-bit unsigned data value (LWORD, ULINT, MlpiLogicType) from the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. IB0).
[out]dataPointer to variable where the value will be stored.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Read the data value from the memory area %IL42.
2 ULLONG data = 0;
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicReadMemoryAreaUllong(connection, application, MLPI_MEMORY_AREA_INPUT, 42, &data);
MLPIRESULT mlpiLogicReadMemoryAreaFloat ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
FLOAT *  data 
)

This function reads the 32-bit floating point data value (single precision, REAL, MlpiLogicType) from the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. IB0).
[out]dataPointer to variable where the value will be stored.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Read the data value from the memory area %ID42.
2 FLOAT data = 0.0;
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicReadMemoryAreaFloat(connection, application, MLPI_MEMORY_AREA_INPUT, 42, &data);
MLPIRESULT mlpiLogicReadMemoryAreaDouble ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
DOUBLE *  data 
)

This function reads the 64-bit floating point data value (double precision, LREAL, MlpiLogicType) from the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. IB0).
[out]dataPointer to variable where the value will be stored.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Read the data value from the memory area %IL42.
2 DOUBLE data = 0.0;
3 WCHAR16 application = L"Application";
4 MLPIRESULT result = mlpiLogicReadMemoryAreaDouble(connection, application, MLPI_MEMORY_AREA_INPUT, 42, &data);
MLPIRESULT mlpiLogicReadMemoryAreaArrayChar ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
CHAR *  data,
const ULONG  numElements,
ULONG *  numElementsRet 
)

This function reads an array of 8-bit signed data values (SINT, MlpiLogicType) from the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. IB0).
[out]dataPointer to variable where the values will be stored.
[in]numElementsNumber of CHAR elements in 'data' available to read.
[out]numElementsRetNumber of elements used.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Read the data values from the memory area %IB0 to %IB1.
2 CHAR data[2];
3 ULONG numElementsRet = 0;
4 WCHAR16 application = L"Application";
5 memset(data, 0, sizeof(data));
6 MLPIRESULT result = mlpiLogicReadMemoryAreaArrayChar(connection, application, MLPI_MEMORY_AREA_INPUT, 0, data, _countof(data), &numElementsRet);
MLPIRESULT mlpiLogicReadMemoryAreaArrayUchar ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
UCHAR *  data,
const ULONG  numElements,
ULONG *  numElementsRet 
)

This function reads an array of 8-bit unsigned data values (BYTE, USINT, MlpiLogicType) from the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. IB0).
[out]dataPointer to variable where the values will be stored.
[in]numElementsNumber of UCHAR elements in data available to read.
[out]numElementsRetNumber of elements used.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Read the data values from the memory area %IB0 to %IB1.
2 UCHAR data[2];
3 ULONG numElementsRet = 0;
4 WCHAR16 application = L"Application";
5 memset(data, 0, sizeof(data));
6 MLPIRESULT result = mlpiLogicReadMemoryAreaArrayUchar(connection, application, MLPI_MEMORY_AREA_INPUT, 0, data, _countof(data), &numElementsRet);
MLPIRESULT mlpiLogicReadMemoryAreaArrayShort ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
SHORT *  data,
const ULONG  numElements,
ULONG *  numElementsRet 
)

This function reads an array of 16-bit signed data values (INT, MlpiLogicType) from the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. IB0).
[out]dataPointer to variable where the values will be stored.
[in]numElementsNumber of SHORT elements in data available to read.
[out]numElementsRetNumber of elements used.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Read the data value from the memory area %IW0 to %IW2.
2 SHORT data[2];
3 ULONG numElementsRet = 0;
4 WCHAR16 application = L"Application";
5 memset(data, 0, sizeof(data));
6 MLPIRESULT result = mlpiLogicReadMemoryAreaArrayShort(connection, application, MLPI_MEMORY_AREA_INPUT, 0, data, _countof(data), &numElementsRet);
MLPIRESULT mlpiLogicReadMemoryAreaArrayUshort ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
USHORT *  data,
const ULONG  numElements,
ULONG *  numElementsRet 
)

This function reads an array of 16-bit unsigned data values (WORD, UINT, MlpiLogicType) from the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. IB0).
[out]dataPointer to variable where the values will be stored.
[in]numElementsNumber of USHORT elements in data available to read.
[out]numElementsRetNumber of elements used.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Read the data value from the memory area %IW0 to %IW2.
2 USHORT data[2];
3 ULONG numElementsRet = 0;
4 WCHAR16 application = L"Application";
5 memset(data, 0, sizeof(data));
6 MLPIRESULT result = mlpiLogicReadMemoryAreaArrayUshort(connection, application, MLPI_MEMORY_AREA_INPUT, 0, data, _countof(data), &numElementsRet);
MLPIRESULT mlpiLogicReadMemoryAreaArrayLong ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
LONG *  data,
const ULONG  numElements,
ULONG *  numElementsRet 
)

This function reads an array of 32-bit signed data values (DINT, MlpiLogicType) from the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. IB0).
[out]dataPointer to variable where the values will be stored.
[in]numElementsNumber of LONG elements in data available to read.
[out]numElementsRetNumber of elements used.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Read the data value from the memory area %ID0 to %ID4.
2 LONG data[2];
3 ULONG numElementsRet = 0;
4 WCHAR16 application = L"Application";
5 memset(data, 0, sizeof(data));
6 MLPIRESULT result = mlpiLogicReadMemoryAreaArrayLong(connection, application, MLPI_MEMORY_AREA_INPUT, 0, data, _countof(data), &numElementsRet);
MLPIRESULT mlpiLogicReadMemoryAreaArrayUlong ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
ULONG *  data,
const ULONG  numElements,
ULONG *  numElementsRet 
)

This function reads an array of 32-bit unsigned data values (DWORD, UDINT, MlpiLogicType) from the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. IB0).
[out]dataPointer to variable where the values will be stored.
[in]numElementsNumber of ULONG elements in data available to read.
[out]numElementsRetNumber of elements used.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Read the data value from the memory area %ID0 to %ID4.
2 ULONG data[2];
3 ULONG numElementsRet = 0;
4 WCHAR16 application = L"Application";
5 memset(data, 0, sizeof(data));
6 MLPIRESULT result = mlpiLogicReadMemoryAreaArrayUlong(connection, application, MLPI_MEMORY_AREA_INPUT, 0, data, _countof(data), &numElementsRet);
MLPIRESULT mlpiLogicReadMemoryAreaArrayLlong ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
LLONG *  data,
const ULONG  numElements,
ULONG *  numElementsRet 
)

This function reads an array of 64-bit signed data values (LINT, MlpiLogicType) from the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. IB0).
[out]dataPointer to variable where the values will be stored.
[in]numElementsNumber of LLONG elements in data available to read.
[out]numElementsRetNumber of elements used.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Read the data value from the memory area %IL0 to %IL8.
2 LLONG data[2];
3 ULONG numElementsRet = 0;
4 WCHAR16 application = L"Application";
5 memset(data, 0, sizeof(data));
6 MLPIRESULT result = mlpiLogicReadMemoryAreaArrayLlong(connection, application, MLPI_MEMORY_AREA_INPUT, 0, data, _countof(data), &numElementsRet);
MLPIRESULT mlpiLogicReadMemoryAreaArrayUllong ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
ULLONG *  data,
const ULONG  numElements,
ULONG *  numElementsRet 
)

This function reads an array of 64-bit unsigned data values (LWORD, ULINT, MlpiLogicType) from the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. IB0).
[out]dataPointer to variable where the values will be stored.
[in]numElementsNumber of ULLONG elements in data available to read.
[out]numElementsRetNumber of elements used.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Read the data value from the memory area %IL0 to %IL8.
2 ULLONG data[2];
3 ULONG numElementsRet = 0;
4 WCHAR16 application = L"Application";
5 memset(data, 0, sizeof(data));
6 MLPIRESULT result = mlpiLogicReadMemoryAreaArrayUllong(connection, application, MLPI_MEMORY_AREA_INPUT, 0, data, _countof(data), &numElementsRet);
MLPIRESULT mlpiLogicReadMemoryAreaArrayFloat ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
FLOAT *  data,
const ULONG  numElements,
ULONG *  numElementsRet 
)

This function reads an array of 32-bit floating point data values (single precision, REAL, MlpiLogicType) from the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. IB0).
[out]dataPointer to variable where the values will be stored.
[in]numElementsNumber of FLOAT elements in data available to read.
[out]numElementsRetNumber of elements used.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Read the data value from the memory area %ID0 to %ID4.
2 FLOAT data[2];
3 ULONG numElementsRet = 0;
4 WCHAR16 application = L"Application";
5 memset(data, 0, sizeof(data));
6 MLPIRESULT result = mlpiLogicReadMemoryAreaArrayFloat(connection, application, MLPI_MEMORY_AREA_INPUT, 0, data, _countof(data), &numElementsRet);
MLPIRESULT mlpiLogicReadMemoryAreaArrayDouble ( const MLPIHANDLE  connection,
const WCHAR16 *  application,
const MlpiApplicationMemoryArea  area,
const ULONG  byteOffset,
DOUBLE *  data,
const ULONG  numElements,
ULONG *  numElementsRet 
)

This function reads an array of 64-bit floating point data values (double precision, LREAL, MlpiLogicType) from the memory area (MlpiApplicationMemoryArea).

Parameters
[in]connectionHandle for multiple connections.
[in]applicationName of application.
[in]areaMemory area of access (MlpiApplicationMemoryArea).
[in]byteOffsetByte offset based on zero (e.g. IB0).
[out]dataPointer to variable where the values will be stored.
[in]numElementsNumber of DOUBLE elements in data available to read.
[out]numElementsRetNumber of elements used.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // Read the data value from the memory area %IL0 to %IL8.
2 DOUBLE data[2];
3 ULONG numElementsRet = 0;
4 WCHAR16 application = L"Application";
5 memset(data, 0, sizeof(data));
6 MLPIRESULT result = mlpiLogicReadMemoryAreaArrayDouble(connection, application, MLPI_MEMORY_AREA_INPUT, 0, data, _countof(data), &numElementsRet);