Open Core Interface - MLPI
MLPI-MotionLogicProgrammingInterface(mlpi4LabVIEW)  1.26.2
Utility functions
Collaboration diagram for Utility functions:

Functions

MLPIRESULT mlpiApiDelay (const MLPIHANDLE connection, const ULONG delayMilliseconds)
 
MLPIRESULT mlpiApiGetClientCoreVersion (MlpiVersion *versionInfo)
 
MLPIRESULT mlpiApiGetServerCoreVersion (const MLPIHANDLE connection, MlpiVersion *versionInfo)
 
MLPIRESULT mlpiApiSetNameOfConnection (const MLPIHANDLE connection, const WCHAR16 *name)
 
MLPIRESULT mlpiApiSetLabelOfConnection (const MLPIHANDLE connection, const WCHAR16 *label)
 
MLPIRESULT mlpiApiGetOwnConnectionDescription (const MLPIHANDLE connection, MlpiConnectionDescription *description)
 
MLPIRESULT mlpiApiGetAllConnectionDescription (const MLPIHANDLE connection, MlpiConnectionDescription *description, const ULONG numElements, ULONG *numElementsRet)
 
MLPIRESULT mlpiApiCloseConnectionByUid (const MLPIHANDLE connection, const ULLONG uid)
 
MLPIRESULT mlpiApiCloseConnectionsByUser (const MLPIHANDLE connection, const WCHAR16 *user)
 
MLPIRESULT mlpiApiCloseConnectionsByUri (const MLPIHANDLE connection, const WCHAR16 *uri)
 
MLPIRESULT mlpiApiUserAccountControlReload (const MLPIHANDLE connection)
 
MLPIRESULT mlpiApiUserAccountControlLoadAccounts (const MLPIHANDLE connection, const WCHAR16 *path)
 
MLPIRESULT mlpiApiUserAccountControlUnloadAccounts (const MLPIHANDLE connection, const WCHAR16 *path)
 
MLPIRESULT mlpiApiGetOwnPermissions (const MLPIHANDLE connection, WCHAR16 *permissions, const ULONG numElements, ULONG *numElementsRet)
 
MLPIRESULT mlpiApiGetAccounts (const MLPIHANDLE connection, WCHAR16 *accounts, const ULONG numElements, ULONG *numElementsRet)
 
MLPIRESULT mlpiApiGetAccountPermissions (const MLPIHANDLE connection, const WCHAR16 *account, WCHAR16 *permissions, const ULONG numElements, ULONG *numElementsRet)
 
MLPIRESULT mlpiApiGetLibrarySupport (const MLPIHANDLE connection, MlpiLibrary *library, const ULONG numElements, ULONG *numElementsRet)
 

Detailed Description

Contains various functions which are handy for MLPI connection testing and information.

Function Documentation

MLPIRESULT mlpiApiDelay ( const MLPIHANDLE  connection,
const ULONG  delayMilliseconds 
)

This function does a simple delay on the server side. All this function performs is a blocking delay on the server side in the given amount of milliseconds. Use it during development or debugging of your application to simulate high traffic on your network. This way, you can test the behavior of your client application when MLPI communication slows down. The delay has no impact on the performance of the device.

Parameters
[in]connectionHandle for multiple connections.
[in]delayMillisecondsDelay in milliseconds to block.
Returns
Return value indicating success (>=0) or error (<0).
MLPIRESULT mlpiApiGetClientCoreVersion ( MlpiVersion *  versionInfo)

This function returns the version info of the MLPI client library.

Parameters
[out]versionInfoPointer to struct receiving the version info.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 MlpiVersion versionInfo;
2 memset(&versionInfo, 0, sizeof(versionInfo));
3 MLPIRESULT result = mlpiApiGetClientCoreVersion(&versionInfo);
4 
5 if (MLPI_FAILED(result)) {
6  printf("\ncall of MLPI function failed with 0x%08x!", (unsigned)result);
7 } else {
8  printf("\nVersion (Major, Minor, Bugfix, Patch): %d.%d.%d.%d Build: %d"
9  , versionInfo.major
10  , versionInfo.minor
11  , versionInfo.bugfix
12  , versionInfo.patch
13  , versionInfo.build);
14 }
MLPIRESULT mlpiApiGetServerCoreVersion ( const MLPIHANDLE  connection,
MlpiVersion *  versionInfo 
)

This function returns the version info of the MLPI server library.

Parameters
[in]connectionHandle for multiple connections.
[out]versionInfoPointer to struct receiving the version info.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 MlpiVersion versionInfo;
2 memset(&versionInfo, 0, sizeof(versionInfo));
3 MLPIRESULT result = mlpiApiGetServerCoreVersion(connection, &versionInfo);
4 
5 if (MLPI_FAILED(result)) {
6  printf("\ncall of MLPI function failed with 0x%08x!", (unsigned)result);
7 } else {
8  printf("\nVersion (Major, Minor, Bugfix, Patch): %d.%d.%d.%d Build: %d"
9  , versionInfo.major
10  , versionInfo.minor
11  , versionInfo.bugfix
12  , versionInfo.patch
13  , versionInfo.build);
14 }
MLPIRESULT mlpiApiSetNameOfConnection ( const MLPIHANDLE  connection,
const WCHAR16 *  name 
)

Using this function, you can assign a short descriptive name to your connection. It is not necessary to give your connection a name, but the name might be useful for debugging and maintaining your connections.

Parameters
[in]connectionHandle for multiple connections.
[in]nameUser-defined name of connection.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // let's call our connection 'The Hitchhiker's Guide to the Galaxy.'
2 MLPIRESULT result = mlpiApiSetNameOfConnection(connection, L"The Hitchhiker's Guide to the Galaxy.");
3 if (MLPI_FAILED(result)) {
4  printf("\ncall of MLPI function failed with 0x%08x!", (unsigned) result);
5  return result;
6 }
MLPIRESULT mlpiApiSetLabelOfConnection ( const MLPIHANDLE  connection,
const WCHAR16 *  label 
)

Using this function, you can assign a long descriptive label to your connection. It is not necessary to set the connection label, but the label might be useful for debugging and maintaining your connections.

Parameters
[in]connectionHandle for multiple connections.
[in]labelUser-defined label of connection.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // let's label our connection with 'The answer to the Ultimate Question of Life, the Universe, and Everything is... 42.'
2 MLPIRESULT result = mlpiApiSetLabelOfConnection(connection, L"The answer to the Ultimate Question of Life, the Universe, and Everything is... 42.");
3 if (MLPI_FAILED(result)) {
4  printf("\ncall of MLPI function failed with 0x%08x!", (unsigned) result);
5  return result;
6 }
MLPIRESULT mlpiApiGetOwnConnectionDescription ( const MLPIHANDLE  connection,
MlpiConnectionDescription *  description 
)

This function will return information about the own connection.

Parameters
[in]connectionHandle for multiple connections.
[out]descriptionPointer to struct receiving the connection descriptions.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 MlpiConnectionDescription description;
2 memset(&description, 0, sizeof(description));
3 
4 // get information about all connections
5 MLPIRESULT result = mlpiApiGetOwnConnectionDescription(connection, description);
6 if(MLPI_SUCCEEDED(result)) {
7  printf("\n\n* %d", i);
8  printf("\n\tuid: 0x%08X.%08X", (ULONG) (description.uid>>32), (ULONG) description.uid);
9  printf("\n\tuser: %s", W2A16(description.user));
10  printf("\n\turi: %s", description.uri);
11  printf("\n\tname: %s", W2A16(description.name));
12  printf("\n\tlabel: %s", W2A16(description.label));
13  printf("\n\tdate an time: %04u-%02u-%02u %02u-%02u-%02u (UTC)",
14  description.dateTime.year, description.dateTime.month, description.dateTime.day,
15  description.dateTime.hour, description.dateTime.minute, description.dateTime.second);
16  printf("\n\trequests: %d", description.requestCounter);
17  printf("\n\tlast request: %d", description.lastRequest);
18  printf("\n\tprotection: %d", description.protection);
19  printf("\n\twatchdog: %s", (description.watchdog==1) ? "TRUE" : "FALSE");
20 }
21 else {
22  printf("\ncall of MLPI function failed with 0x%08x!", (unsigned) result);
23  return result;
24 }
MLPIRESULT mlpiApiGetAllConnectionDescription ( const MLPIHANDLE  connection,
MlpiConnectionDescription *  description,
const ULONG  numElements,
ULONG *  numElementsRet 
)

This function will return information about all established connections of the device.

Parameters
[in]connectionHandle for multiple connections.
[out]descriptionPointer to struct receiving the connection descriptions.
[in]numElementsNumber of MlpiConnectionDescription elements available in 'description' to read.
[out]numElementsRetNumber of elements used.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 ULONG numElementsRet = 0;
2 MlpiConnectionDescription description[MLPI_API_MAX_NUMBER_OF_CONNECTIONS];
3 memset(description, 0, sizeof(description));
4 
5 // get information about all connections
6 MLPIRESULT result = mlpiApiGetAllConnectionDescription(connection, description, MLPI_API_MAX_NUMBER_OF_CONNECTIONS, &numElementsRet);
7 if(MLPI_SUCCEEDED(result)) {
8  for(ULONG i=0; i<numElementsRet; i++) {
9  printf("\n\n* %d", i);
10  printf("\n\tuid: 0x%08X.%08X", (ULONG) (description[i].uid>>32), (ULONG) description[i].uid);
11  printf("\n\tuser: %s", W2A16(description[i].user));
12  printf("\n\turi: %s", description[i].uri);
13  printf("\n\tname: %s", W2A16(description[i].name));
14  printf("\n\tlabel: %s", W2A16(description[i].label));
15  printf("\n\tdate an time: %04u-%02u-%02u %02u-%02u-%02u (UTC)",
16  description[i].dateTime.year, description[i].dateTime.month, description[i].dateTime.day,
17  description[i].dateTime.hour, description[i].dateTime.minute, description[i].dateTime.second);
18  printf("\n\trequests: %d", description[i].requestCounter);
19  printf("\n\tlast request: %d", description[i].lastRequest);
20  printf("\n\tprotection: %d", description[i].protection);
21  printf("\n\twatchdog: %s", (description[i].watchdog==1) ? "TRUE" : "FALSE");
22  }
23 }
24 else {
25  printf("\ncall of MLPI function failed with 0x%08x!", (unsigned) result);
26  return result;
27 }
MLPIRESULT mlpiApiCloseConnectionByUid ( const MLPIHANDLE  connection,
const ULLONG  uid 
)

This function closes a connection selected by the unique identifier (uid) of a connection. You can determine the uid by using the function mlpiApiGetOwnConnectionDescription.

Note
A connection cannot be closed if it runs in a protected mode (see MlpiApiProtection). In this case, the function will return the error MLPI_E_RD_WR_PROTECTION.
Parameters
[in]connectionHandle for multiple connections.
[in]uidUnique identifier of connection.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // close the connection with the uid 0x0000002A.12345678
2 MLPIRESULT result = mlpiApiCloseConnectionByUid(connection, 0x0000002A.12345678);
3 if (MLPI_FAILED(result)) {
4  printf("\ncall of MLPI function failed with 0x%08x!", (unsigned) result);
5  return result;
6 }
MLPIRESULT mlpiApiCloseConnectionsByUser ( const MLPIHANDLE  connection,
const WCHAR16 *  user 
)

This function closes one or multiple connections selected by the user.

Note
A connection cannot be closed if it runs in a protected mode (see MlpiApiProtection). In this case, the function will return the error MLPI_E_RD_WR_PROTECTION.
Parameters
[in]connectionHandle for multiple connections.
[in]userLogin user name of connection.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // close all connections of the user 'Batman'
2 MLPIRESULT result = mlpiApiCloseConnectionsByUser(connection, L"Batman");
3 if (MLPI_FAILED(result)) {
4  printf("\ncall of MLPI function failed with 0x%08x!", (unsigned) result);
5  return result;
6 }
MLPIRESULT mlpiApiCloseConnectionsByUri ( const MLPIHANDLE  connection,
const WCHAR16 *  uri 
)

This function closes one or multiple connections selected by a combination of the uniform resource identifier (uri) and the placeholder '*'.

Note
A connection cannot be closed if it runs in a protected mode (see MlpiApiProtection). In this case, the function will return the error MLPI_E_RD_WR_PROTECTION.
Parameters
[in]connectionHandle for multiple connections.
[in]uriURI of connection (e.g. "mlpi.tcp://'IP-address':'port'").
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // close all connections of the device with the uri 'mlpi.tcp://192.168.0.42*'
2 MLPIRESULT result = mlpiApiCloseConnectionsByUri(connection, L"mlpi.tcp://192.168.0.42*");
3 if (MLPI_FAILED(result)) {
4  printf("\ncall of MLPI function failed with 0x%08x!", (unsigned) result);
5  return result;
6 }
MLPIRESULT mlpiApiUserAccountControlReload ( const MLPIHANDLE  connection)

This function provides the reloading of all currently loaded account manifests know as 'accounts.xml'.

Note
The permissions of an established connection will not be influenced from new accounts settings.
Attention
A fail of reloading of the default account manifests maybe requires a reboot of the control because another new connection cannot be established furthermore.
Parameters
[in]connectionHandle for multiple connections.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // reload accounts of default account manifests and additional account manifests
2 MLPIRESULT result = mlpiApiUserAccountControlReload(connection);
3 if (MLPI_FAILED(result)) {
4  printf("\ncall of MLPI function failed with 0x%08x!", (unsigned) result);
5  return result;
6 }
MLPIRESULT mlpiApiUserAccountControlLoadAccounts ( const MLPIHANDLE  connection,
const WCHAR16 *  path 
)
Note
This function is deprecated since server version 1.19.0. Do not use this function in combination with the AccessControlLib!

This function provides the loading of the accounts of an additional account manifest.

Note
It's recommended, but not required to name the additional account manifest 'accounts.xml'.
Parameters
[in]connectionHandle for multiple connections.
[in]pathPath to the additional account manifest.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // load accounts of an additional account manifest
2 WCHAR16 path[256] = L"";
3 WCHAR16 file[] = L"bundles/com.boschrexroth.mlpi.test42/accounts.xml";
4 if ( MLPI_SUCCEEDED(mlpiSystemGetSpecialPath(MLPI_PATH_OEM, path, _countof(path))) )
5 {
6  wcscat(path, file);
7  MLPIRESULT result = mlpiApiUserAccountControlLoadAccounts(connection, path);
8  if (MLPI_FAILED(result)) {
9  printf("\ncall of MLPI function failed with 0x%08x!", (unsigned) result);
10  return result;
11  }
12 }
MLPIRESULT mlpiApiUserAccountControlUnloadAccounts ( const MLPIHANDLE  connection,
const WCHAR16 *  path 
)
Note
This function is deprecated since server version 1.19.0. Do not use this function in combination with the AccessControlLib!

This function provides the unloading of the accounts of an additional account manifest.

Note
The permissions of an established connection will not be influenced from new accounts settings.
Parameters
[in]connectionHandle for multiple connections.
[in]pathPath to the additional account manifest.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // unload accounts of an additional account manifest
2 WCHAR16 path[256] = L"";
3 WCHAR16 file[] = L"bundles/com.boschrexroth.mlpi.test42/accounts.xml";
4 if ( MLPI_SUCCEEDED(mlpiSystemGetSpecialPath(MLPI_PATH_OEM, path, _countof(path))) )
5 {
6  wcscat16(path, file);
7  MLPIRESULT result = mlpiApiUserAccountControlUnloadAccounts(connection, path);
8  if (MLPI_FAILED(result)) {
9  printf("\ncall of MLPI function failed with 0x%08x!", (unsigned) result);
10  return result;
11  }
12 }
MLPIRESULT mlpiApiGetOwnPermissions ( const MLPIHANDLE  connection,
WCHAR16 *  permissions,
const ULONG  numElements,
ULONG *  numElementsRet 
)

This function provides the reading of own permissions based on account manifest 'accounts.xml'.

Note
In case the buffer is too short, the function will still return the required number of WCHAR16 elements by 'numElementsRet'.
Parameters
[in]connectionHandle for multiple connections.
[out]permissionsString where the permissions will be stored.
[in]numElementsNumber of WCHAR16 elements available in 'permissions' to read.
[out]numElementsRetNumber of WCHAR16 elements in complete 'permissions'.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // read own permissions
2 ULONG numElementsRet = 0;
3 WCHAR16 permissions[4096] = L"";
4 
5 MLPIRESULT result = mlpiApiGetOwnPermissions(connection, permissions, _countof(permissions), &numElementsRet);
6 if (MLPI_FAILED(result)) {
7  printf("\ncall of MLPI function failed with 0x%08x!", (unsigned) result);
8  return result;
9 }
10 else
11 {
12  ULONG idx = 0;
13  CHAR permission[128] = "";
14  WCHAR16 *curr = permissions, *nxt = permissions;
15  while (true)
16  {
17  // find separator between two permissions or end of string
18  while ( (*nxt!=NULL) && (*nxt!=';') )
19  nxt++;
20  if(curr==nxt)
21  break;
22  // separate current permission string from next permission string
23  if(*nxt!=0)
24  *nxt++=0;
25  // convert and print permission string
26  wcstombs16(permission, curr, wcslen16(curr)+1);
27  printf("\n%d:\t%s", idx++, permission);
28  // go to next permission string
29  curr = nxt;
30  }
31 }
Example:
1 #include "mlpiApiHelper.h"
2 
3 ULONG numElementsRet = 0;
4 WCHAR16 permissions[4096] = L"";
5 
6 MLPIRESULT result = mlpiApiGetOwnPermissions(connection, permissions, _countof(permissions), &numElementsRet);
7 if (MLPI_FAILED(result)) {
8  printf("\ncall of MLPI function failed with 0x%08x!", (unsigned) result);
9  return result;
10 }
11 else
12 {
13  WCHAR16 requiredPermission[] = L"MLPI_APILIB_PERMISSION_CONNECTION_CLOSE";
14 
15  MlpiApiPermissionEvaluation evalPermission(permissions);
16 
17  if (evalPermission.hasPermission(requiredPermission))
18  log(L"\nThe logged in user has the permission '%s'.", requiredPermission);
19  else
20  warning(L"\nThe logged in user hasn't the permission '%s'.", requiredPermission);
21 }
MLPIRESULT mlpiApiGetAccounts ( const MLPIHANDLE  connection,
WCHAR16 *  accounts,
const ULONG  numElements,
ULONG *  numElementsRet 
)
Note
This function is deprecated since server version 1.19.0. Use the function mlpiAccessControlGetAllUserInfos from the AccessControlLib instead!

This function provides the reading of all available accounts based on account manifest 'accounts.xml'.

Note
An account with empty name will be replaced by the surrogate string MLPI_ACCOUNT_EMPTY_NAME but this surrogate string cannot used as login name!
Note: In case the buffer is too short, the function will still return the required number of WCHAR16
elements by 'numElementsRet'.
Parameters
[in]connectionHandle for multiple connections.
[out]accountsString where the accounts will be stored.
[in]numElementsNumber of WCHAR16 elements available in 'accounts' to read.
[out]numElementsRetNumber of WCHAR16 elements in complete 'accounts'.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // read all available accounts
2 ULONG numElementsRet = 0;
3 WCHAR16 accounts[1024] = L"";
4 
5 MLPIRESULT result = mlpiApiGetAccounts(connection, accounts, _countof(accounts), &numElementsRet);
6 if (MLPI_FAILED(result)) {
7  printf("\ncall of MLPI function failed with 0x%08x!", (unsigned) result);
8  return result;
9 }
10 else
11 {
12  ULONG idx = 0;
13  CHAR account[128] = "";
14  WCHAR16 *curr = accounts, *nxt = accounts;
15  while (true)
16  {
17  // find separator between two accounts or end of string
18  while ( (*nxt!=NULL) && (*nxt!=';') )
19  nxt++;
20  if(curr==nxt)
21  break;
22  // separate current account string from next account string
23  if (*nxt!=0)
24  *nxt++=0;
25  // remove surrogate string of account with empty name
26  if(wcscmp16(curr, MLPI_ACCOUNT_EMPTY_NAME)==0)
27  *curr = 0;
28  // convert account string
29  wcstombs16(account, curr, wcslen16(curr)+1);
30  printf("\n%d:\t%s", idx++, account);
31  // go to next account string
32  curr = nxt;
33  }
34 }
MLPIRESULT mlpiApiGetAccountPermissions ( const MLPIHANDLE  connection,
const WCHAR16 *  account,
WCHAR16 *  permissions,
const ULONG  numElements,
ULONG *  numElementsRet 
)

This function provides the reading of the permissions of an account based on account manifest 'accounts.xml'.

Note
In case the buffer is too short, the function will still return the required number of WCHAR16 elements by 'numElementsRet'.
Parameters
[in]connectionHandle for multiple connections.
[in]accountString that identifies the account for which permissions were read. Set to NULL to get your own permissions.
[out]permissionsString where the permissions will be stored.
[in]numElementsNumber of WCHAR16 elements available in 'permissions' to read.
[out]numElementsRetNumber of WCHAR16 elements in complete 'permissions'.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 // read permissions of account 'administrator'
2 ULONG numElementsRet = 0;
3 WCHAR16 permissions[4096] = L"";
4 
5 MLPIRESULT result = mlpiApiGetAccountPermissions(connection, L"administrator", permissions, _countof(permissions), &numElementsRet);
6 if (MLPI_FAILED(result)) {
7  printf("\ncall of MLPI function failed with 0x%08x!", (unsigned) result);
8  return result;
9 }
10 else
11 {
12  ULONG idx = 0;
13  CHAR permission[128] = "";
14  WCHAR16 *curr = permissions, *nxt = permissions;
15  while (true)
16  {
17  // find separator between two permissions or end of string
18  while ( (*nxt!=NULL) && (*nxt!=';') )
19  nxt++;
20  if(curr==nxt)
21  break;
22  // separate current permission string from next permission string
23  if (*nxt!=0)
24  *nxt++=0;
25  // convert and print permission string
26  wcstombs16(permission, curr, wcslen16(curr)+1);
27  printf("\n%d:\t%s", idx++, permission);
28  // go to next permission string
29  curr = nxt;
30  }
31 }
MLPIRESULT mlpiApiGetLibrarySupport ( const MLPIHANDLE  connection,
MlpiLibrary *  library,
const ULONG  numElements,
ULONG *  numElementsRet 
)

This function provides names and IDs of supported libraries.

Parameters
[in]connectionHandle for multiple connections.
[out]libraryStruct where names and IDs of supported libraries will be stored.
[in]numElementsNumber of MlpiLibrary elements available in 'library' to read.
[out]numElementsRetNumber of MlpiLibrary elements in complete 'library'.
Returns
Return value indicating success (>=0) or error (<0).
Example:
1 ULONG numElementsRet = 0;
2 MlpiLibrary library[32];
3 memset(library, 0, sizeof(library));
4 
5 // Get names and IDs of supported libraries.
6 MLPIRESULT result = mlpiApiGetLibrarySupport(connection, library, _countof(library), &numElementsRet);
7 if(MLPI_SUCCEEDED(result)) {
8  for(ULONG i=0; i<numElementsRet; i++) {
9  printf("\n\n* %d", i);
10  printf("\n\tname: %s", W2A16(library[i].name));
11  printf("\n\tid: %08X", library[i].id);
12  }
13 }
14 else {
15  printf("\ncall of MLPI function failed with 0x%08x!", (unsigned) result);
16  return result;
17 }