Work-API by Autonomy on Board GmbH

Work-API allows companies to connect any standard work tool (such as email, calendar, instant message, ...) directly to their machines. This provides better integration of machines into the overall work and communication processes. Deployed across machines from different manufacturers, Work-API helps standardize and simplify user-machine interaction.
With the Work-API solution, machine operators can interact with a machine in a natural way - as they would with another person. For example, a message can be sent via Microsoft Teams to create a job for the machine. Also, a question can be asked via Alexa about the number of pieces or an event can be set in Google Calendar to remind about maintenance work.