Question? Ask iXi!

Go back

MGA Ingenieurdienstleistungen GmbH

Logo of the company MGA

Voice Control from MGA is a software that runs directly on ctrlX OS. No additional hardware is required to implement voice control. The voice interaction is robust and works reliably even in noisy environments. The software operates completely offline for maximum cybersecurity.

Operating machines

Operation of a table saw with electrically adjustable stops. Instead of entering the dimensions via a control panel or retrieving the next cutting instruction from a recipe, this can be done through a voice command using a headset, which also serves as hearing protection. The operator has his hands free to handle the workpiece.

Maintenance

Maintenance technicians receive error messages audibly through a headset while they are moving between the various machines they oversee. Additionally, the technician is provided with information about the nature of the malfunction and possible solutions. This way, they already have this knowledge before heading to the malfunctioning machine.

Commissioning

During the commissioning of a new machine, the technician can give commands to the machine via voice without standing in front of the control panel. This allows them to be near the specific actuator they want to test and observe it directly. Benefit: a second commissioning technician is no longer needed.

Advantages

  • Easy, web-based design of dialogue.
  • System is eliminating background noises for reliable use in noisy environment.
  • Freely selectable wake words.
  • Available in 30 languages.
  • Software is running on premis – no access to the internet required for a maximum of cyber security.

Target Groups

  • Machine Builder
Experience the voice input app for ctrlX OS in this video by Marius Ritter, Project Manager at MGA.

About MGA

MGA, as an owner-managed medium-sized engineering company, has been a competent partner of mechanical engineering in the field of process automation and control technology for over 20 years. With over 50 employees, MGA is engaged in the design, programming and commissioning of machine controls.

Visit the Website

 

Voice Control App

Voice Control
for free hands in operating machines

ctrlX OS Store

Go back