Question? Ask iXi!

Go back

HELIO by HMI Project GmbH

HELIO Logo

Better user interfaces in record time. HELIO makes HMI development noticeably easier and measurably faster. Even complex visualizations can be easily configured without programming knowledge or complicated training. This makes HELIO one of the best tools for large corporate solutions and small individualists within the ctrlX OS Ecosystem.

Future-proof and Independent

HELIO uses web technology and is therefore platform-independent. It runs on all devices with an up-to-date browser - whether Windows, Linux, Mac, iOS, Android or ctrlX OS Devices. HMIs are stable, future-proof and flexible in terms of hardware and input methods such as mouse, keyboard or touch.

Optimized Usability

HELIO combines over 20 years of experience in user interface design in a design system with optimized controls and predefined templates for maximum usability. This helps to create user-centered HMIs - even without in-house UX expertise. Ideal for industrial use.

Flexibly Customizable

HELIO is fully customizable: from extensions and special features to own interfaces. With the help of the SDK, individual technical solutions outside the standard are possible. And HMI Project GmbH's UX/UI services are the perfect complement for demanding projects.

Advantages

  • Live and direct: developing with real-time data
  • HMI development without programming
  • Platform-independent and future-proof
  • All the advantages of modern web technology
  • Perfect usability out of the box

Target Groups

  • Machine Builder
  • Machine Operator
  • System Integrator

Topology

HELIO connects to ctrlX OS Devices via OPC UA. One or more clients can log in to the interface with a browser via the network and have the option of executing or editing HMIs there.

 

About HELIO by HMI Project GmbH

HELIO is developed by HMI Project GmbH. HMI Project was founded in 2011 by the designers Markus Buberl and Christian Rudolph in Würzburg and Philipp Kruse joined the team as technical director in 2015. Originally set up as a design studio, HMI Project expanded its portfolio early on to include software development with web technology. After many successful years in the service sector, the interdisciplinary team of 20 designers, usability experts and developers is now incorporating its industry expertise into HELIO's product development, setting new standards for high-quality, web-based HMIs in the industry.

Visit the Website

 

Die Zukunft der industriellen HMI

HELIO
The Future of Industrial HMI

ctrlX OS Store

 

Go back