Lua offers a higher-level function to load and run libraries, called require. Require searches for the file in two different path variables: package.path and package.cpath. These path used by require are a little different from typical paths. Most programs use paths as a list of directories wherein to search for a given file. However, ANSI C (the abstract platform where Lua runs) does not have the concept of directories. Therefore, the path used by require is a list of patterns, each of them specifying an alternative way to transform a virtual file name (the argument to require) into a real file name. More specifically, each component in the path is a file name containing optional interrogation marks. For each component, require replaces each '?' by the virtual file name and checks whether there is a file with that name; if not, it goes to the next component. The components in a path are separated by semicolons (a character seldom used for file names in most operating systems). For instance, if the path is
then the call require("lili") will try to open the following files:
The only things that require fixes is the semicolon (as the component separator) and the interrogation mark; everything else (such as directory separators or file extensions) is defined in the path.
package.path is responsible for loading lua files. package.cpath is responsible for loading C libraries in binaries.
To use mlpi4Lua in your Lua runtime environment you have to ensure that the runtime finds the library. Simply add the path to mlpi4Lua/bin/... to package.cpath variable.
For different Lua runtimes different mlpi libraries are provided:
| Lua Runtime | Lua Version | package.cpath | Build against |
|---|---|---|---|
| JNLua 32 Bit | 5.1 | "/mlpi4Lua/bin/win-any-x86/?51.dll" | lua51.dll |
| JNLua 32 Bit | 5.2 | "/mlpi4Lua/bin/win-any-x86/?52.dll" | lua52.dll |
| Lua 32 Bit | 5.3 | "/mlpi4Lua/bin/win-any-x86/?53.dll" | lua53.dll |
| JNLua 64 Bit | 5.1 | "/mlpi4Lua/bin/win-any-x64/?51.dll" | lua51.dll |
| JNLua 64 Bit | 5.2 | "/mlpi4Lua/bin/win-any-x64/?52.dll" | lua52.dll |
| Lua 64 Bit | 5.3 | "/mlpi4Lua/bin/win-any-x64/?53.dll" | lua53.dll |
| LuaDist | 5.1 | "/mlpi4Lua/bin/win_luadist-any-x86/luadist?51.dll" | liblua.dll |
| XLC/MLC | 5.3 | build in | build in |
On XLC/MLC target Lua runtime is provided as a firmware bundle. By default package.cpath includes all nessesary path information to find mlpi on target. So it is not necessary to modify package.cpath.
Every MLPI function call returns beside the return values of the function an integer which indicates if the function has succeeded(>=0) or not(<0) and a message representing human readable form of result. The return value is positive or zero if the call has succeeded and negative if the function call has failed. You may want to use either the mlpi.failed() or the mlpi.succeeded() function for quick evaluation of the return value.
In most cases, the return value not only holds information about success or failure, but also information about the cause of a failure. There is a list of definitions with some generic and most likely error codes.
| Define | Value | Description |
|---|---|---|
| MLPI_S_OK | 0x00360000 | Return code "everything okay". |
| MLPI_E_FAIL | 0xF0360001 | General error during function call. |
| MLPI_E_NOTSUPPORTED | 0xF0360002 | The given function is not supported yet. |
| MLPI_E_INVALIDARG | 0xF0360003 | Invalid argument given to method. |
| MLPI_E_OUTOFMEMORY | 0xF0360004 | Out of memory. |
| MLPI_E_TIMEOUT | 0xF0360005 | Timeout during function call. |
| MLPI_E_SERVEREXCEPTION | 0xF0360006 | System exception on control side. |
| MLPI_E_CONNECTFAILED | 0xF0360007 | Connection failed. |
| MLPI_E_CREATEERROR | 0xF0360008 | Error creating the resource. |
| MLPI_E_SYSTEMERROR | 0xF0360009 | System error during execution. |
| MLPI_E_BUFFERTOOSHORT | 0xF036000A | Given buffer is too short. |
| MLPI_E_INVALIDSIGNATURE | 0xF036000B | Invalid signature. |
| MLPI_E_STARTERROR | 0xF036000C | Error during start of functionality. |
| MLPI_E_WATCHDOGWARNING | 0xF036000D | Watchdog warning occurred. |
| MLPI_E_WATCHDOGERROR | 0xF536000E | Watchdog error occurred. |
| MLPI_E_UNIMPLEMENTED | 0xF036000F | The given function is not implemented on this specific device. |
| MLPI_E_LIMIT_MIN | 0xF0360010 | The minimum of a limitation is exceeded. |
| MLPI_E_LIMIT_MAX | 0xF0360011 | The maximum of a limitation is exceeded. |
| MLPI_E_VERSION | 0xF0360012 | Version conflict. |
| MLPI_E_DEPRECATED | 0xF0360013 | Deprecated. The lib or function is no longer supported. |
| MLPI_E_PERMISSION | 0xF0360014 | Request declined due to missing permission rights. |
| MLPI_E_TYPE_MISSMATCH | 0xF0360015 | Type mismatch, present type doesn't match requested type. |
| MLPI_E_SIZE_MISSMATCH | 0xF0360016 | Size mismatch, present size doesn't match requested size. |
| MLPI_E_INVALID_HANDLE | 0xF0360017 | Invalid handle argument or NULL pointer argument. |
| MLPI_E_NOCONNECTION | 0xF0360018 | The connection is not established, no longer established or has been quit by peer. |
| MLPI_E_RD_WR_PROTECTION | 0xF0360019 | Request declined due to read or write protection. |
| MLPI_E_INVALID_FLOATINGPOINT | 0xF036001A | Invalid floating point number given to method. |
| MLPI_E_NOTINITIALIZED | 0xF036001B | Object not initialized yet. |
| MLPI_E_STREAM_OUT_OF_SYNC | 0xF036001C | Send / Receive stream out of synchronization. |
| MLPI_E_INVALID_PRIVATEKEY_FILE | 0xF036001D | SThe given private key file is broken or not existing. |
| MLPI_E_INVALID_CERTIFICATE_FILE | 0xF036001E | The given certificate key file is broken or not existing. |
| MLPI_E_KEYPAIR_MISSMATCH | 0xF036001F | The given certificate does not match the given private key. |
| MLPI_E_TLS_HANDSHAKE_FAILED | 0xF0360020 | The TLS handshake was not successful. |
| MLPI_E_GENERAL_AC_ERROR | 0xF0360021 | There was a general access control error. |
| MLPI_E_POLICY_VIOLATION_AC | 0xF0360022 | A violation occurred in the user and/or policies. |
| MLPI_E_USER_ALREADY_EXISTS | 0xF0360023 | The given username is already in use. |
| MLPI_E_GROUP_ALREADY_EXISTS | 0xF0360024 | The given groupname is already in use. |
| MLPI_E_MEMBERSHIP_ALREADY_EXISTS | 0xF0360025 | The given user is already member of the given group. |
| MLPI_E_USER_NOT_EXISTING | 0xF0360026 | The given user does not exist on the control. |
| MLPI_E_GROUP_NOT_EXISTING | 0xF0360027 | The given group does not exist on the control. |
| MLPI_E_MEMBERSHIP_NOT_EXISTING | 0xF0360028 | The given user is not member of the given group. |
Please note that this is not a complete list of all possible return values a MLPI function might return. Besides these common error codes, there are also many device specific error codes. These error codes are specific to the facility (for example, Motion, Logic, sercos, drive...) of the connected device and not directly part of the MLPI. Still, all these error codes are unique and based on the idea that a failure message is a negative value (0xFxxxxxxx) and a success message is a positive value (0x0xxxxxxx). The difference to the errors listed above is that you won't find the description of the error code within this documentation, but within the documentation of the MLPI device you are connected to. For example, if you are connected to a XLC/MLC device, you will probably find more help on the error code by looking into the XLC/MLC diagnostics documentation which is not directly part of the MLPI SDK. In most cases, you will find the documentation included in an IndraWorks installation or you may want to download an up-to-date version from the http://www.boschrexroth.com homepage.
For the latest information, you should look at the BoschRexroth website. http://www.boschrexroth.com/oce